This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 Leopard board SD card boot file creation

   Has anyone tried the DM365 leopard board SD card boot method, as I am having missing file errors at step-4?

Steps>>>>>>>>
To prepare the SD card
1. insert a SD card ( SDHC is not supported) to a Linux PC
2. find out the device name of this SD card by looking at /dev/sd*
3. export PATH=$PATH:./bin.x86
4. make
5. sudo ./dm3xx_sd_boot format /dev/sdX (replace sdX with the SD device name)
6. remove the SD card, and plug it back in
7. make install
The log>>>>>>>>>>>>>>>>>>>>>>
[root@tools dm3xx_sd_boot-6_leopard]# export PATH=$PATH:./bin.x86

 [root@tools dm3xx_sd_boot-6_leopard]# make

 make -C sdcard_flash PLATFORM=DM36x all

 make[1]: Entering directory `/media/809A-4AF4/dm3xx_sd_boot-6_leopard/dm3xx_sd_boot-6_leopard/sdcard_flash'

 arm_v5t_le-gcc -DUBL_NAND=1 -Os -IDM36x -DDM36x -g -DANSI_COLORS --include sdc_debug.h -  I../flash_utils/Common/include -I../flash_utils/DM36x/Common/include -I../flash_utils/Common/arch/arm926ejs/include -I../flash_utils/Common/sft/include -I../flash_utils/Common/gnu/include -I../flash_utils/Common/drivers/include -I ../flash_utils/Common/ubl/include ../flash_utils/Common/arch/arm926ejs/src/boot.c -c -o DM36x/boot.o     

make[1]: arm_v5t_le-gcc: Command not found

make[1]: *** [DM36x/boot.o] Error 127

make[1]: Leaving directory `/media/809A-4AF4/dm3xx_sd_boot-6_leopard/dm3xx_sd_boot-6_leopard/sdcard_flash'

make: *** [all] Error 2

 [root@tools dm3xx_sd_boot-6_leopard]#

   Thank you

    Kumar