This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: Questions for UBS during in deepsleep

Part Number: AM623
Other Parts Discussed in Thread: SK-AM62, SK-AM62B, SK-AM62-LP, SK-AM62B-P1

Tool/software:

Hi,

My customer is considering below scenario using AM6232 and an external WLAN module.

- AM6232 and WLAN module is connected by USB. AM6232 is USB Host.
- When WLAN is waiting for data receive from WiFi, AM6232 is put in deep sleep for power saving.
- During above period, USB VBUS needs to be supplied to WLAN module.
- As soon as WLAN module receives data, WLAN module wakes up AM6232 by WoWLAN (Wake on Wireless LAN).

Questions:
Please answer if both AM623x hardware and TI Linux SDK support below functions.
Q1) Is 5V VBUS is kept provided while AM623x is in Deep Sleep?
Q2) Does AM623x USB support Type-C?
Q3) There are two USB channels. Each channel can work either Host and Device, correct?

Thanks and regards,
Koichiro Tashiro