Tool/software:
i have Maxlinear PHY GPY215C Ethernet chip,
i want to integrate in R5F2_0 and initialize the driver for IO packet.
i have the linux example for it , how to use that linux into R5F2_0?
I am attaching the linux example for your references
// SPDX-License-Identifier: GPL-2.0+ /* Copyright (C) 2021 Maxlinear Corporation * Copyright (C) 2020 Intel Corporation * * Drivers for Maxlinear Ethernet GPY * */ #include <linux/module.h> #include <linux/bitfield.h> #include <linux/hwmon.h> #include <linux/mutex.h> #include <linux/phy.h> #include <linux/polynomial.h> #include <linux/property.h> #include <linux/netdevice.h> /* PHY ID */ #define PHY_ID_GPYx15B_MASK 0xFFFFFFFC #define PHY_ID_GPY21xB_MASK 0xFFFFFFF9 #define PHY_ID_GPY2xx 0x67C9DC00 #define PHY_ID_GPY115B 0x67C9DF00 #define PHY_ID_GPY115C 0x67C9DF10 #define PHY_ID_GPY211B 0x67C9DE08 #define PHY_ID_GPY211C 0x67C9DE10 #define PHY_ID_GPY212B 0x67C9DE09 #define PHY_ID_GPY212C 0x67C9DE20 #define PHY_ID_GPY215B 0x67C9DF04 #define PHY_ID_GPY215C 0x67C9DF20 #define PHY_ID_GPY241B 0x67C9DE40 #define PHY_ID_GPY241BM 0x67C9DE80 #define PHY_ID_GPY245B 0x67C9DEC0 #define PHY_CTL1 0x13 #define PHY_CTL1_MDICD BIT(3) #define PHY_CTL1_MDIAB BIT(2) #define PHY_CTL1_AMDIX BIT(0) #define PHY_MIISTAT 0x18 /* MII state */ #define PHY_IMASK 0x19 /* interrupt mask */ #define PHY_ISTAT 0x1A /* interrupt status */ #define PHY_FWV 0x1E /* firmware version */ #define PHY_MIISTAT_SPD_MASK GENMASK(2, 0) #define PHY_MIISTAT_DPX BIT(3) #define PHY_MIISTAT_LS BIT(10) #define PHY_MIISTAT_SPD_10 0 #define PHY_MIISTAT_SPD_100 1 #define PHY_MIISTAT_SPD_1000 2 #define PHY_MIISTAT_SPD_2500 4 #define PHY_IMASK_WOL BIT(15) /* Wake-on-LAN */ #define PHY_IMASK_ANC BIT(10) /* Auto-Neg complete */ #define PHY_IMASK_ADSC BIT(5) /* Link auto-downspeed detect */ #define PHY_IMASK_DXMC BIT(2) /* Duplex mode change */ #define PHY_IMASK_LSPC BIT(1) /* Link speed change */ #define PHY_IMASK_LSTC BIT(0) /* Link state change */ #define PHY_IMASK_MASK (PHY_IMASK_LSTC | \ PHY_IMASK_LSPC | \ PHY_IMASK_DXMC | \ PHY_IMASK_ADSC | \ PHY_IMASK_ANC) #define PHY_FWV_REL_MASK BIT(15) #define PHY_FWV_MAJOR_MASK GENMASK(11, 8) #define PHY_FWV_MINOR_MASK GENMASK(7, 0) #define PHY_PMA_MGBT_POLARITY 0x82 #define PHY_MDI_MDI_X_MASK GENMASK(1, 0) #define PHY_MDI_MDI_X_NORMAL 0x3 #define PHY_MDI_MDI_X_AB 0x2 #define PHY_MDI_MDI_X_CD 0x1 #define PHY_MDI_MDI_X_CROSS 0x0 /* SGMII */ #define VSPEC1_SGMII_CTRL 0x08 #define VSPEC1_SGMII_CTRL_ANEN BIT(12) /* Aneg enable */ #define VSPEC1_SGMII_CTRL_ANRS BIT(9) /* Restart Aneg */ #define VSPEC1_SGMII_ANEN_ANRS (VSPEC1_SGMII_CTRL_ANEN | \ VSPEC1_SGMII_CTRL_ANRS) /* Temperature sensor */ #define VSPEC1_TEMP_STA 0x0E #define VSPEC1_TEMP_STA_DATA GENMASK(9, 0) /* Mailbox */ #define VSPEC1_MBOX_DATA 0x5 #define VSPEC1_MBOX_ADDRLO 0x6 #define VSPEC1_MBOX_CMD 0x7 #define VSPEC1_MBOX_CMD_ADDRHI GENMASK(7, 0) #define VSPEC1_MBOX_CMD_RD (0 << 8) #define VSPEC1_MBOX_CMD_READY BIT(15) /* WoL */ #define VPSPEC2_WOL_CTL 0x0E06 #define VPSPEC2_WOL_AD01 0x0E08 #define VPSPEC2_WOL_AD23 0x0E09 #define VPSPEC2_WOL_AD45 0x0E0A #define WOL_EN BIT(0) /* Internal registers, access via mbox */ #define REG_GPIO0_OUT 0xd3ce00 struct gpy_priv { /* serialize mailbox acesses */ struct mutex mbox_lock; u8 fw_major; u8 fw_minor; /* It takes 3 seconds to fully switch out of loopback mode before * it can safely re-enter loopback mode. Record the time when * loopback is disabled. Check and wait if necessary before loopback * is enabled. */ u64 lb_dis_to; }; static const struct { int major; int minor; } ver_need_sgmii_reaneg[] = { {7, 0x6D}, {8, 0x6D}, {9, 0x73}, }; #if IS_ENABLED(CONFIG_HWMON) /* The original translation formulae of the temperature (in degrees of Celsius) * are as follows: * * T = -2.5761e-11*(N^4) + 9.7332e-8*(N^3) + -1.9165e-4*(N^2) + * 3.0762e-1*(N^1) + -5.2156e1 * * where [-52.156, 137.961]C and N = [0, 1023]. * * They must be accordingly altered to be suitable for the integer arithmetics. * The technique is called 'factor redistribution', which just makes sure the * multiplications and divisions are made so to have a result of the operations * within the integer numbers limit. In addition we need to translate the * formulae to accept millidegrees of Celsius. Here what it looks like after * the alterations: * * T = -25761e-12*(N^4) + 97332e-9*(N^3) + -191650e-6*(N^2) + * 307620e-3*(N^1) + -52156 * * where T = [-52156, 137961]mC and N = [0, 1023]. */ static const struct polynomial poly_N_to_temp = { .terms = { {4, -25761, 1000, 1}, {3, 97332, 1000, 1}, {2, -191650, 1000, 1}, {1, 307620, 1000, 1}, {0, -52156, 1, 1} } }; static int gpy_hwmon_read(struct device *dev, enum hwmon_sensor_types type, u32 attr, int channel, long *value) { struct phy_device *phydev = dev_get_drvdata(dev); int ret; ret = phy_read_mmd(phydev, MDIO_MMD_VEND1, VSPEC1_TEMP_STA); if (ret < 0) return ret; if (!ret) return -ENODATA; *value = polynomial_calc(&poly_N_to_temp, FIELD_GET(VSPEC1_TEMP_STA_DATA, ret)); return 0; } static umode_t gpy_hwmon_is_visible(const void *data, enum hwmon_sensor_types type, u32 attr, int channel) { return 0444; } static const struct hwmon_channel_info * const gpy_hwmon_info[] = { HWMON_CHANNEL_INFO(temp, HWMON_T_INPUT), NULL }; static const struct hwmon_ops gpy_hwmon_hwmon_ops = { .is_visible = gpy_hwmon_is_visible, .read = gpy_hwmon_read, }; static const struct hwmon_chip_info gpy_hwmon_chip_info = { .ops = &gpy_hwmon_hwmon_ops, .info = gpy_hwmon_info, }; static int gpy_hwmon_register(struct phy_device *phydev) { struct device *dev = &phydev->mdio.dev; struct device *hwmon_dev; char *hwmon_name; hwmon_name = devm_hwmon_sanitize_name(dev, dev_name(dev)); if (IS_ERR(hwmon_name)) return PTR_ERR(hwmon_name); hwmon_dev = devm_hwmon_device_register_with_info(dev, hwmon_name, phydev, &gpy_hwmon_chip_info, NULL); return PTR_ERR_OR_ZERO(hwmon_dev); } #else static int gpy_hwmon_register(struct phy_device *phydev) { return 0; } #endif static int gpy_mbox_read(struct phy_device *phydev, u32 addr) { struct gpy_priv *priv = phydev->priv; int val, ret; u16 cmd; mutex_lock(&priv->mbox_lock); ret = phy_write_mmd(phydev, MDIO_MMD_VEND1, VSPEC1_MBOX_ADDRLO, addr); if (ret) goto out; cmd = VSPEC1_MBOX_CMD_RD; cmd |= FIELD_PREP(VSPEC1_MBOX_CMD_ADDRHI, addr >> 16); ret = phy_write_mmd(phydev, MDIO_MMD_VEND1, VSPEC1_MBOX_CMD, cmd); if (ret) goto out; /* The mbox read is used in the interrupt workaround. It was observed * that a read might take up to 2.5ms. This is also the time for which * the interrupt line is stuck low. To be on the safe side, poll the * ready bit for 10ms. */ ret = phy_read_mmd_poll_timeout(phydev, MDIO_MMD_VEND1, VSPEC1_MBOX_CMD, val, (val & VSPEC1_MBOX_CMD_READY), 500, 10000, false); if (ret) goto out; ret = phy_read_mmd(phydev, MDIO_MMD_VEND1, VSPEC1_MBOX_DATA); out: mutex_unlock(&priv->mbox_lock); return ret; } static int gpy_config_init(struct phy_device *phydev) { int ret; /* Mask all interrupts */ ret = phy_write(phydev, PHY_IMASK, 0); if (ret) return ret; /* Clear all pending interrupts */ ret = phy_read(phydev, PHY_ISTAT); return ret < 0 ? ret : 0; } static int gpy21x_config_init(struct phy_device *phydev) { __set_bit(PHY_INTERFACE_MODE_2500BASEX, phydev->possible_interfaces); __set_bit(PHY_INTERFACE_MODE_SGMII, phydev->possible_interfaces); return gpy_config_init(phydev); } static int gpy_probe(struct phy_device *phydev) { struct device *dev = &phydev->mdio.dev; struct gpy_priv *priv; int fw_version; int ret; if (!phydev->is_c45) { ret = phy_get_c45_ids(phydev); if (ret < 0) return ret; } priv = devm_kzalloc(dev, sizeof(*priv), GFP_KERNEL); if (!priv) return -ENOMEM; phydev->priv = priv; mutex_init(&priv->mbox_lock); if (!device_property_present(dev, "maxlinear,use-broken-interrupts")) phydev->dev_flags |= PHY_F_NO_IRQ; fw_version = phy_read(phydev, PHY_FWV); if (fw_version < 0) return fw_version; priv->fw_major = FIELD_GET(PHY_FWV_MAJOR_MASK, fw_version); priv->fw_minor = FIELD_GET(PHY_FWV_MINOR_MASK, fw_version); ret = gpy_hwmon_register(phydev); if (ret) return ret; /* Show GPY PHY FW version in dmesg */ phydev_info(phydev, "Firmware Version: %d.%d (0x%04X%s)\n", priv->fw_major, priv->fw_minor, fw_version, fw_version & PHY_FWV_REL_MASK ? "" : " test version"); return 0; } static bool gpy_sgmii_need_reaneg(struct phy_device *phydev) { struct gpy_priv *priv = phydev->priv; size_t i; for (i = 0; i < ARRAY_SIZE(ver_need_sgmii_reaneg); i++) { if (priv->fw_major != ver_need_sgmii_reaneg[i].major) continue; if (priv->fw_minor < ver_need_sgmii_reaneg[i].minor) return true; break; } return false; } static bool gpy_2500basex_chk(struct phy_device *phydev) { int ret; ret = phy_read(phydev, PHY_MIISTAT); if (ret < 0) { phydev_err(phydev, "Error: MDIO register access failed: %d\n", ret); return false; } if (!(ret & PHY_MIISTAT_LS) || FIELD_GET(PHY_MIISTAT_SPD_MASK, ret) != PHY_MIISTAT_SPD_2500) return false; phydev->speed = SPEED_2500; phydev->interface = PHY_INTERFACE_MODE_2500BASEX; phy_modify_mmd(phydev, MDIO_MMD_VEND1, VSPEC1_SGMII_CTRL, VSPEC1_SGMII_CTRL_ANEN, 0); return true; } static bool gpy_sgmii_aneg_en(struct phy_device *phydev) { int ret; ret = phy_read_mmd(phydev, MDIO_MMD_VEND1, VSPEC1_SGMII_CTRL); if (ret < 0) { phydev_err(phydev, "Error: MMD register access failed: %d\n", ret); return true; } return (ret & VSPEC1_SGMII_CTRL_ANEN) ? true : false; } static int gpy_config_mdix(struct phy_device *phydev, u8 ctrl) { int ret; u16 val; switch (ctrl) { case ETH_TP_MDI_AUTO: val = PHY_CTL1_AMDIX; break; case ETH_TP_MDI_X: val = (PHY_CTL1_MDIAB | PHY_CTL1_MDICD); break; case ETH_TP_MDI: val = 0; break; default: return 0; } ret = phy_modify(phydev, PHY_CTL1, PHY_CTL1_AMDIX | PHY_CTL1_MDIAB | PHY_CTL1_MDICD, val); if (ret < 0) return ret; return genphy_c45_restart_aneg(phydev); } static int gpy_config_aneg(struct phy_device *phydev) { bool changed = false; u32 adv; int ret; if (phydev->autoneg == AUTONEG_DISABLE) { /* Configure half duplex with genphy_setup_forced, * because genphy_c45_pma_setup_forced does not support. */ return phydev->duplex != DUPLEX_FULL ? genphy_setup_forced(phydev) : genphy_c45_pma_setup_forced(phydev); } ret = gpy_config_mdix(phydev, phydev->mdix_ctrl); if (ret < 0) return ret; ret = genphy_c45_an_config_aneg(phydev); if (ret < 0) return ret; if (ret > 0) changed = true; adv = linkmode_adv_to_mii_ctrl1000_t(phydev->advertising); ret = phy_modify_changed(phydev, MII_CTRL1000, ADVERTISE_1000FULL | ADVERTISE_1000HALF, adv); if (ret < 0) return ret; if (ret > 0) changed = true; ret = genphy_c45_check_and_restart_aneg(phydev, changed); if (ret < 0) return ret; if (phydev->interface == PHY_INTERFACE_MODE_USXGMII || phydev->interface == PHY_INTERFACE_MODE_INTERNAL) return 0; /* No need to trigger re-ANEG if link speed is 2.5G or SGMII ANEG is * disabled. */ if (!gpy_sgmii_need_reaneg(phydev) || gpy_2500basex_chk(phydev) || !gpy_sgmii_aneg_en(phydev)) return 0; /* There is a design constraint in GPY2xx device where SGMII AN is * only triggered when there is change of speed. If, PHY link * partner`s speed is still same even after PHY TPI is down and up * again, SGMII AN is not triggered and hence no new in-band message * from GPY to MAC side SGMII. * This could cause an issue during power up, when PHY is up prior to * MAC. At this condition, once MAC side SGMII is up, MAC side SGMII * wouldn`t receive new in-band message from GPY with correct link * status, speed and duplex info. * * 1) If PHY is already up and TPI link status is still down (such as * hard reboot), TPI link status is polled for 4 seconds before * retriggerring SGMII AN. * 2) If PHY is already up and TPI link status is also up (such as soft * reboot), polling of TPI link status is not needed and SGMII AN is * immediately retriggered. * 3) Other conditions such as PHY is down, speed change etc, skip * retriggering SGMII AN. Note: in case of speed change, GPY FW will * initiate SGMII AN. */ if (phydev->state != PHY_UP) return 0; ret = phy_read_poll_timeout(phydev, MII_BMSR, ret, ret & BMSR_LSTATUS, 20000, 4000000, false); if (ret == -ETIMEDOUT) return 0; else if (ret < 0) return ret; /* Trigger SGMII AN. */ return phy_modify_mmd(phydev, MDIO_MMD_VEND1, VSPEC1_SGMII_CTRL, VSPEC1_SGMII_CTRL_ANRS, VSPEC1_SGMII_CTRL_ANRS); } static int gpy_update_mdix(struct phy_device *phydev) { int ret; ret = phy_read(phydev, PHY_CTL1); if (ret < 0) return ret; if (ret & PHY_CTL1_AMDIX) phydev->mdix_ctrl = ETH_TP_MDI_AUTO; else if (ret & PHY_CTL1_MDICD || ret & PHY_CTL1_MDIAB) phydev->mdix_ctrl = ETH_TP_MDI_X; else phydev->mdix_ctrl = ETH_TP_MDI; ret = phy_read_mmd(phydev, MDIO_MMD_PMAPMD, PHY_PMA_MGBT_POLARITY); if (ret < 0) return ret; if ((ret & PHY_MDI_MDI_X_MASK) < PHY_MDI_MDI_X_NORMAL) phydev->mdix = ETH_TP_MDI_X; else phydev->mdix = ETH_TP_MDI; return 0; } static int gpy_update_interface(struct phy_device *phydev) { int ret; /* Interface mode is fixed for USXGMII and integrated PHY */ if (phydev->interface == PHY_INTERFACE_MODE_USXGMII || phydev->interface == PHY_INTERFACE_MODE_INTERNAL) return -EINVAL; /* Automatically switch SERDES interface between SGMII and 2500-BaseX * according to speed. Disable ANEG in 2500-BaseX mode. */ switch (phydev->speed) { case SPEED_2500: phydev->interface = PHY_INTERFACE_MODE_2500BASEX; ret = phy_modify_mmd(phydev, MDIO_MMD_VEND1, VSPEC1_SGMII_CTRL, VSPEC1_SGMII_CTRL_ANEN, 0); if (ret < 0) { phydev_err(phydev, "Error: Disable of SGMII ANEG failed: %d\n", ret); return ret; } break; case SPEED_1000: case SPEED_100: case SPEED_10: phydev->interface = PHY_INTERFACE_MODE_SGMII; if (gpy_sgmii_aneg_en(phydev)) break; /* Enable and restart SGMII ANEG for 10/100/1000Mbps link speed * if ANEG is disabled (in 2500-BaseX mode). */ ret = phy_modify_mmd(phydev, MDIO_MMD_VEND1, VSPEC1_SGMII_CTRL, VSPEC1_SGMII_ANEN_ANRS, VSPEC1_SGMII_ANEN_ANRS); if (ret < 0) { phydev_err(phydev, "Error: Enable of SGMII ANEG failed: %d\n", ret); return ret; } break; } if (phydev->speed == SPEED_2500 || phydev->speed == SPEED_1000) { ret = genphy_read_master_slave(phydev); if (ret < 0) return ret; } return gpy_update_mdix(phydev); } static int gpy_read_status(struct phy_device *phydev) { int ret; ret = genphy_update_link(phydev); if (ret) return ret; phydev->speed = SPEED_UNKNOWN; phydev->duplex = DUPLEX_UNKNOWN; phydev->pause = 0; phydev->asym_pause = 0; if (phydev->autoneg == AUTONEG_ENABLE && phydev->autoneg_complete) { ret = genphy_c45_read_lpa(phydev); if (ret < 0) return ret; /* Read the link partner's 1G advertisement */ ret = phy_read(phydev, MII_STAT1000); if (ret < 0) return ret; mii_stat1000_mod_linkmode_lpa_t(phydev->lp_advertising, ret); } else if (phydev->autoneg == AUTONEG_DISABLE) { linkmode_zero(phydev->lp_advertising); } ret = phy_read(phydev, PHY_MIISTAT); if (ret < 0) return ret; phydev->link = (ret & PHY_MIISTAT_LS) ? 1 : 0; phydev->duplex = (ret & PHY_MIISTAT_DPX) ? DUPLEX_FULL : DUPLEX_HALF; switch (FIELD_GET(PHY_MIISTAT_SPD_MASK, ret)) { case PHY_MIISTAT_SPD_10: phydev->speed = SPEED_10; break; case PHY_MIISTAT_SPD_100: phydev->speed = SPEED_100; break; case PHY_MIISTAT_SPD_1000: phydev->speed = SPEED_1000; break; case PHY_MIISTAT_SPD_2500: phydev->speed = SPEED_2500; break; } if (phydev->link) { ret = gpy_update_interface(phydev); if (ret < 0) return ret; } return 0; } static int gpy_config_intr(struct phy_device *phydev) { u16 mask = 0; if (phydev->interrupts == PHY_INTERRUPT_ENABLED) mask = PHY_IMASK_MASK; return phy_write(phydev, PHY_IMASK, mask); } static irqreturn_t gpy_handle_interrupt(struct phy_device *phydev) { int reg; reg = phy_read(phydev, PHY_ISTAT); if (reg < 0) { phy_error(phydev); return IRQ_NONE; } if (!(reg & PHY_IMASK_MASK)) return IRQ_NONE; /* The PHY might leave the interrupt line asserted even after PHY_ISTAT * is read. To avoid interrupt storms, delay the interrupt handling as * long as the PHY drives the interrupt line. An internal bus read will * stall as long as the interrupt line is asserted, thus just read a * random register here. * Because we cannot access the internal bus at all while the interrupt * is driven by the PHY, there is no way to make the interrupt line * unstuck (e.g. by changing the pinmux to GPIO input) during that time * frame. Therefore, polling is the best we can do and won't do any more * harm. * It was observed that this bug happens on link state and link speed * changes independent of the firmware version. */ if (reg & (PHY_IMASK_LSTC | PHY_IMASK_LSPC)) { reg = gpy_mbox_read(phydev, REG_GPIO0_OUT); if (reg < 0) { phy_error(phydev); return IRQ_NONE; } } phy_trigger_machine(phydev); return IRQ_HANDLED; } static int gpy_set_wol(struct phy_device *phydev, struct ethtool_wolinfo *wol) { struct net_device *attach_dev = phydev->attached_dev; int ret; if (wol->wolopts & WAKE_MAGIC) { /* MAC address - Byte0:Byte1:Byte2:Byte3:Byte4:Byte5 * VPSPEC2_WOL_AD45 = Byte0:Byte1 * VPSPEC2_WOL_AD23 = Byte2:Byte3 * VPSPEC2_WOL_AD01 = Byte4:Byte5 */ ret = phy_set_bits_mmd(phydev, MDIO_MMD_VEND2, VPSPEC2_WOL_AD45, ((attach_dev->dev_addr[0] << 8) | attach_dev->dev_addr[1])); if (ret < 0) return ret; ret = phy_set_bits_mmd(phydev, MDIO_MMD_VEND2, VPSPEC2_WOL_AD23, ((attach_dev->dev_addr[2] << 8) | attach_dev->dev_addr[3])); if (ret < 0) return ret; ret = phy_set_bits_mmd(phydev, MDIO_MMD_VEND2, VPSPEC2_WOL_AD01, ((attach_dev->dev_addr[4] << 8) | attach_dev->dev_addr[5])); if (ret < 0) return ret; /* Enable the WOL interrupt */ ret = phy_write(phydev, PHY_IMASK, PHY_IMASK_WOL); if (ret < 0) return ret; /* Enable magic packet matching */ ret = phy_set_bits_mmd(phydev, MDIO_MMD_VEND2, VPSPEC2_WOL_CTL, WOL_EN); if (ret < 0) return ret; /* Clear the interrupt status register. * Only WoL is enabled so clear all. */ ret = phy_read(phydev, PHY_ISTAT); if (ret < 0) return ret; } else { /* Disable magic packet matching */ ret = phy_clear_bits_mmd(phydev, MDIO_MMD_VEND2, VPSPEC2_WOL_CTL, WOL_EN); if (ret < 0) return ret; } if (wol->wolopts & WAKE_PHY) { /* Enable the link state change interrupt */ ret = phy_set_bits(phydev, PHY_IMASK, PHY_IMASK_LSTC); if (ret < 0) return ret; /* Clear the interrupt status register */ ret = phy_read(phydev, PHY_ISTAT); if (ret < 0) return ret; if (ret & (PHY_IMASK_MASK & ~PHY_IMASK_LSTC)) phy_trigger_machine(phydev); return 0; } /* Disable the link state change interrupt */ return phy_clear_bits(phydev, PHY_IMASK, PHY_IMASK_LSTC); } static void gpy_get_wol(struct phy_device *phydev, struct ethtool_wolinfo *wol) { int ret; wol->supported = WAKE_MAGIC | WAKE_PHY; wol->wolopts = 0; ret = phy_read_mmd(phydev, MDIO_MMD_VEND2, VPSPEC2_WOL_CTL); if (ret & WOL_EN) wol->wolopts |= WAKE_MAGIC; ret = phy_read(phydev, PHY_IMASK); if (ret & PHY_IMASK_LSTC) wol->wolopts |= WAKE_PHY; } static int gpy_loopback(struct phy_device *phydev, bool enable) { struct gpy_priv *priv = phydev->priv; u16 set = 0; int ret; if (enable) { u64 now = get_jiffies_64(); /* wait until 3 seconds from last disable */ if (time_before64(now, priv->lb_dis_to)) msleep(jiffies64_to_msecs(priv->lb_dis_to - now)); set = BMCR_LOOPBACK; } ret = phy_modify(phydev, MII_BMCR, BMCR_LOOPBACK, set); if (ret <= 0) return ret; if (enable) { /* It takes some time for PHY device to switch into * loopback mode. */ msleep(100); } else { priv->lb_dis_to = get_jiffies_64() + HZ * 3; } return 0; } static int gpy115_loopback(struct phy_device *phydev, bool enable) { struct gpy_priv *priv = phydev->priv; if (enable) return gpy_loopback(phydev, enable); if (priv->fw_minor > 0x76) return gpy_loopback(phydev, 0); return genphy_soft_reset(phydev); } static struct phy_driver gpy_drivers[] = { { PHY_ID_MATCH_MODEL(PHY_ID_GPY2xx), .name = "Maxlinear Ethernet GPY2xx", .get_features = genphy_c45_pma_read_abilities, .config_init = gpy_config_init, .probe = gpy_probe, .suspend = genphy_suspend, .resume = genphy_resume, .config_aneg = gpy_config_aneg, .aneg_done = genphy_c45_aneg_done, .read_status = gpy_read_status, .config_intr = gpy_config_intr, .handle_interrupt = gpy_handle_interrupt, .set_wol = gpy_set_wol, .get_wol = gpy_get_wol, .set_loopback = gpy_loopback, }, { .phy_id = PHY_ID_GPY115B, .phy_id_mask = PHY_ID_GPYx15B_MASK, .name = "Maxlinear Ethernet GPY115B", .get_features = genphy_c45_pma_read_abilities, .config_init = gpy_config_init, .probe = gpy_probe, .suspend = genphy_suspend, .resume = genphy_resume, .config_aneg = gpy_config_aneg, .aneg_done = genphy_c45_aneg_done, .read_status = gpy_read_status, .config_intr = gpy_config_intr, .handle_interrupt = gpy_handle_interrupt, .set_wol = gpy_set_wol, .get_wol = gpy_get_wol, .set_loopback = gpy115_loopback, }, { PHY_ID_MATCH_MODEL(PHY_ID_GPY115C), .name = "Maxlinear Ethernet GPY115C", .get_features = genphy_c45_pma_read_abilities, .config_init = gpy_config_init, .probe = gpy_probe, .suspend = genphy_suspend, .resume = genphy_resume, .config_aneg = gpy_config_aneg, .aneg_done = genphy_c45_aneg_done, .read_status = gpy_read_status, .config_intr = gpy_config_intr, .handle_interrupt = gpy_handle_interrupt, .set_wol = gpy_set_wol, .get_wol = gpy_get_wol, .set_loopback = gpy115_loopback, }, { .phy_id = PHY_ID_GPY211B, .phy_id_mask = PHY_ID_GPY21xB_MASK, .name = "Maxlinear Ethernet GPY211B", .get_features = genphy_c45_pma_read_abilities, .config_init = gpy21x_config_init, .probe = gpy_probe, .suspend = genphy_suspend, .resume = genphy_resume, .config_aneg = gpy_config_aneg, .aneg_done = genphy_c45_aneg_done, .read_status = gpy_read_status, .config_intr = gpy_config_intr, .handle_interrupt = gpy_handle_interrupt, .set_wol = gpy_set_wol, .get_wol = gpy_get_wol, .set_loopback = gpy_loopback, }, { PHY_ID_MATCH_MODEL(PHY_ID_GPY211C), .name = "Maxlinear Ethernet GPY211C", .get_features = genphy_c45_pma_read_abilities, .config_init = gpy21x_config_init, .probe = gpy_probe, .suspend = genphy_suspend, .resume = genphy_resume, .config_aneg = gpy_config_aneg, .aneg_done = genphy_c45_aneg_done, .read_status = gpy_read_status, .config_intr = gpy_config_intr, .handle_interrupt = gpy_handle_interrupt, .set_wol = gpy_set_wol, .get_wol = gpy_get_wol, .set_loopback = gpy_loopback, }, { .phy_id = PHY_ID_GPY212B, .phy_id_mask = PHY_ID_GPY21xB_MASK, .name = "Maxlinear Ethernet GPY212B", .get_features = genphy_c45_pma_read_abilities, .config_init = gpy21x_config_init, .probe = gpy_probe, .suspend = genphy_suspend, .resume = genphy_resume, .config_aneg = gpy_config_aneg, .aneg_done = genphy_c45_aneg_done, .read_status = gpy_read_status, .config_intr = gpy_config_intr, .handle_interrupt = gpy_handle_interrupt, .set_wol = gpy_set_wol, .get_wol = gpy_get_wol, .set_loopback = gpy_loopback, }, { PHY_ID_MATCH_MODEL(PHY_ID_GPY212C), .name = "Maxlinear Ethernet GPY212C", .get_features = genphy_c45_pma_read_abilities, .config_init = gpy21x_config_init, .probe = gpy_probe, .suspend = genphy_suspend, .resume = genphy_resume, .config_aneg = gpy_config_aneg, .aneg_done = genphy_c45_aneg_done, .read_status = gpy_read_status, .config_intr = gpy_config_intr, .handle_interrupt = gpy_handle_interrupt, .set_wol = gpy_set_wol, .get_wol = gpy_get_wol, .set_loopback = gpy_loopback, }, { .phy_id = PHY_ID_GPY215B, .phy_id_mask = PHY_ID_GPYx15B_MASK, .name = "Maxlinear Ethernet GPY215B", .get_features = genphy_c45_pma_read_abilities, .config_init = gpy21x_config_init, .probe = gpy_probe, .suspend = genphy_suspend, .resume = genphy_resume, .config_aneg = gpy_config_aneg, .aneg_done = genphy_c45_aneg_done, .read_status = gpy_read_status, .config_intr = gpy_config_intr, .handle_interrupt = gpy_handle_interrupt, .set_wol = gpy_set_wol, .get_wol = gpy_get_wol, .set_loopback = gpy_loopback, }, { PHY_ID_MATCH_MODEL(PHY_ID_GPY215C), .name = "Maxlinear Ethernet GPY215C", .get_features = genphy_c45_pma_read_abilities, .config_init = gpy21x_config_init, .probe = gpy_probe, .suspend = genphy_suspend, .resume = genphy_resume, .config_aneg = gpy_config_aneg, .aneg_done = genphy_c45_aneg_done, .read_status = gpy_read_status, .config_intr = gpy_config_intr, .handle_interrupt = gpy_handle_interrupt, .set_wol = gpy_set_wol, .get_wol = gpy_get_wol, .set_loopback = gpy_loopback, }, { PHY_ID_MATCH_MODEL(PHY_ID_GPY241B), .name = "Maxlinear Ethernet GPY241B", .get_features = genphy_c45_pma_read_abilities, .config_init = gpy_config_init, .probe = gpy_probe, .suspend = genphy_suspend, .resume = genphy_resume, .config_aneg = gpy_config_aneg, .aneg_done = genphy_c45_aneg_done, .read_status = gpy_read_status, .config_intr = gpy_config_intr, .handle_interrupt = gpy_handle_interrupt, .set_wol = gpy_set_wol, .get_wol = gpy_get_wol, .set_loopback = gpy_loopback, }, { PHY_ID_MATCH_MODEL(PHY_ID_GPY241BM), .name = "Maxlinear Ethernet GPY241BM", .get_features = genphy_c45_pma_read_abilities, .config_init = gpy_config_init, .probe = gpy_probe, .suspend = genphy_suspend, .resume = genphy_resume, .config_aneg = gpy_config_aneg, .aneg_done = genphy_c45_aneg_done, .read_status = gpy_read_status, .config_intr = gpy_config_intr, .handle_interrupt = gpy_handle_interrupt, .set_wol = gpy_set_wol, .get_wol = gpy_get_wol, .set_loopback = gpy_loopback, }, { PHY_ID_MATCH_MODEL(PHY_ID_GPY245B), .name = "Maxlinear Ethernet GPY245B", .get_features = genphy_c45_pma_read_abilities, .config_init = gpy_config_init, .probe = gpy_probe, .suspend = genphy_suspend, .resume = genphy_resume, .config_aneg = gpy_config_aneg, .aneg_done = genphy_c45_aneg_done, .read_status = gpy_read_status, .config_intr = gpy_config_intr, .handle_interrupt = gpy_handle_interrupt, .set_wol = gpy_set_wol, .get_wol = gpy_get_wol, .set_loopback = gpy_loopback, }, }; module_phy_driver(gpy_drivers); static struct mdio_device_id __maybe_unused gpy_tbl[] = { {PHY_ID_MATCH_MODEL(PHY_ID_GPY2xx)}, {PHY_ID_GPY115B, PHY_ID_GPYx15B_MASK}, {PHY_ID_MATCH_MODEL(PHY_ID_GPY115C)}, {PHY_ID_GPY211B, PHY_ID_GPY21xB_MASK}, {PHY_ID_MATCH_MODEL(PHY_ID_GPY211C)}, {PHY_ID_GPY212B, PHY_ID_GPY21xB_MASK}, {PHY_ID_MATCH_MODEL(PHY_ID_GPY212C)}, {PHY_ID_GPY215B, PHY_ID_GPYx15B_MASK}, {PHY_ID_MATCH_MODEL(PHY_ID_GPY215C)}, {PHY_ID_MATCH_MODEL(PHY_ID_GPY241B)}, {PHY_ID_MATCH_MODEL(PHY_ID_GPY241BM)}, {PHY_ID_MATCH_MODEL(PHY_ID_GPY245B)}, { } }; MODULE_DEVICE_TABLE(mdio, gpy_tbl); MODULE_DESCRIPTION("Maxlinear Ethernet GPY Driver"); MODULE_AUTHOR("Xu Liang"); MODULE_LICENSE("GPL");