Part Number: AM625
Tool/software:
Hi Ti,
1. We use SDK: 09_01_00_08 , Kernel Version: 6.1.46-rt13 in our custom board.
We use KIOXIA emmc sdhci0 boot on speed HS200 ,then to test Repeatedly power on and off.
When it run 311 times have error like follow log.
it mmc0: Timeout waiting for hardware interrupt.
[Thu Jun 13 17:58:15.952 2024] U-Boot SPL 2023.04-g576b2c98c0 (Mar 11 2024 - 07:42:03 +0000) [Thu Jun 13 17:58:15.983 2024] SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') [Thu Jun 13 17:58:16.030 2024] SPL initial stack usage: 13384 bytes [Thu Jun 13 17:58:16.046 2024] Trying to boot from MMC1 [Thu Jun 13 17:58:16.202 2024] Authentication passed [Thu Jun 13 17:58:16.202 2024] Authentication passed [Thu Jun 13 17:58:16.202 2024] Authentication passed [Thu Jun 13 17:58:16.249 2024] Authentication passed [Thu Jun 13 17:58:16.249 2024] Authentication passed [Thu Jun 13 17:58:16.249 2024] Starting ATF on ARM64 core... [Thu Jun 13 17:58:16.264 2024] [Thu Jun 13 17:58:16.264 2024] NOTICE: BL31: v2.9(release):v2.9.0-614-gd7a7135d32-dirty [Thu Jun 13 17:58:16.264 2024] NOTICE: BL31: Built : 09:34:15, Aug 24 2023 [Thu Jun 13 17:58:16.561 2024] [Thu Jun 13 17:58:16.561 2024] U-Boot SPL 2023.04-g576b2c98c0 (Mar 11 2024 - 07:42:03 +0000) [Thu Jun 13 17:58:16.577 2024] SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') [Thu Jun 13 17:58:16.608 2024] SPL initial stack usage: 1856 bytes [Thu Jun 13 17:58:16.624 2024] Error: could not access storage. [Thu Jun 13 17:58:16.624 2024] Trying to boot from MMC1 [Thu Jun 13 17:58:16.780 2024] Authentication passed [Thu Jun 13 17:58:16.780 2024] Authentication passed [Thu Jun 13 17:58:17.436 2024] [Thu Jun 13 17:58:17.436 2024] [Thu Jun 13 17:58:17.436 2024] U-Boot 2023.04-g576b2c98c0 (Mar 11 2024 - 07:42:03 +0000) [Thu Jun 13 17:58:17.436 2024] [Thu Jun 13 17:58:17.436 2024] SoC: AM62X SR1.0 HS-FS [Thu Jun 13 17:58:17.436 2024] Model: Texas Instruments AM625 SK [Thu Jun 13 17:58:17.436 2024] DRAM: 2 GiB [Thu Jun 13 17:58:17.686 2024] Core: 68 devices, 30 uclasses, devicetree: separate [Thu Jun 13 17:58:17.686 2024] MMC: mmc@fa10000: 0, mmc@fa00000: 1 [Thu Jun 13 17:58:17.702 2024] Loading Environment from MMC... OK [Thu Jun 13 17:58:17.890 2024] In: serial [Thu Jun 13 17:58:17.905 2024] Out: serial [Thu Jun 13 17:58:17.905 2024] Err: serial [Thu Jun 13 17:58:17.905 2024] [BSP] gd->boot_dev = 9 [Thu Jun 13 17:58:17.905 2024] Saving Environment to MMC... Writing to redundant MMC(0)... OK [Thu Jun 13 17:58:18.046 2024] switch to partitions #0, OK [Thu Jun 13 17:58:18.062 2024] mmc0(part 0) is current device [Thu Jun 13 17:58:18.187 2024] SD/MMC found on device 0 [Thu Jun 13 17:58:18.202 2024] Running eMMC boot ... [Thu Jun 13 17:58:18.218 2024] 574 bytes read in 14 ms (40 KiB/s) [Thu Jun 13 17:58:18.218 2024] EMMC Loaded env from uEnv.txt [Thu Jun 13 17:58:18.218 2024] Importing environment from mmc0 ... [Thu Jun 13 17:58:18.421 2024] 16908800 bytes read in 198 ms (81.4 MiB/s) [Thu Jun 13 17:58:18.452 2024] 63041 bytes read in 16 ms (3.8 MiB/s) [Thu Jun 13 17:58:18.452 2024] Working FDT set to 88000000 [Thu Jun 13 17:58:18.452 2024] ## Flattened Device Tree blob at 88000000 [Thu Jun 13 17:58:18.452 2024] Booting using the fdt blob at 0x88000000 [Thu Jun 13 17:58:18.468 2024] Working FDT set to 88000000 [Thu Jun 13 17:58:18.483 2024] ERROR: reserving fdt memory region failed (addr=ff700000 size=8ca000 flags=4) [Thu Jun 13 17:58:18.499 2024] Loading Device Tree to 000000008feed000, end 000000008fffffff ... OK [Thu Jun 13 17:58:18.499 2024] Working FDT set to 8feed000 [Thu Jun 13 17:58:18.515 2024] [Thu Jun 13 17:58:18.515 2024] Starting kernel ... [Thu Jun 13 17:58:18.515 2024] [Thu Jun 13 17:58:18.546 2024] [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [Thu Jun 13 17:58:18.561 2024] [ 0.000000] Linux version 6.1.46-rt13-BSP_12.4--g17da321871 (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT_RT Tue Apr 23 02:09:43 UTC 2024 [Thu Jun 13 17:58:18.577 2024] [ 0.000000] Machine model: Texas Instruments AM625 SK [Thu Jun 13 17:58:18.577 2024] [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [Thu Jun 13 17:58:18.671 2024] [ 0.000000] printk: bootconsole [ns16550a0] enabled [Thu Jun 13 17:58:18.671 2024] [ 0.000000] efi: UEFI not found. [Thu Jun 13 17:58:18.686 2024] [ 0.000000] Reserved memory: created CMA memory pool at 0x00000000f7600000, size 128 MiB [Thu Jun 13 17:58:18.686 2024] [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool [Thu Jun 13 17:58:18.702 2024] [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB [Thu Jun 13 17:58:18.702 2024] [ 0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool [Thu Jun 13 17:58:18.718 2024] [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB [Thu Jun 13 17:58:18.718 2024] [ 0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool [Thu Jun 13 17:58:18.733 2024] [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB [Thu Jun 13 17:58:18.733 2024] [ 0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool [Thu Jun 13 17:58:18.749 2024] [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB [Thu Jun 13 17:58:18.765 2024] [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool [Thu Jun 13 17:58:18.765 2024] [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB [Thu Jun 13 17:58:18.780 2024] [ 0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool [Thu Jun 13 17:58:18.780 2024] [ 0.000000] Zone ranges: [Thu Jun 13 17:58:18.780 2024] [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [Thu Jun 13 17:58:18.796 2024] [ 0.000000] DMA32 empty [Thu Jun 13 17:58:18.796 2024] [ 0.000000] Normal empty [Thu Jun 13 17:58:18.796 2024] [ 0.000000] Movable zone start for each node [Thu Jun 13 17:58:18.796 2024] [ 0.000000] Early memory node ranges [Thu Jun 13 17:58:18.811 2024] [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009c7fffff] [Thu Jun 13 17:58:18.811 2024] [ 0.000000] node 0: [mem 0x000000009c800000-0x000000009e6fffff] [Thu Jun 13 17:58:18.811 2024] [ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e77ffff] [Thu Jun 13 17:58:18.827 2024] [ 0.000000] node 0: [mem 0x000000009e780000-0x000000009fffffff] [Thu Jun 13 17:58:18.827 2024] [ 0.000000] node 0: [mem 0x00000000a0000000-0x00000000ff6fffff] [Thu Jun 13 17:58:18.843 2024] [ 0.000000] node 0: [mem 0x00000000ff700000-0x00000000fffc9fff] [Thu Jun 13 17:58:18.843 2024] [ 0.000000] node 0: [mem 0x00000000fffca000-0x00000000ffffffff] [Thu Jun 13 17:58:18.858 2024] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff] [Thu Jun 13 17:58:18.858 2024] [ 0.000000] psci: probing for conduit method from DT. [Thu Jun 13 17:58:18.858 2024] [ 0.000000] psci: PSCIv1.1 detected in firmware. [Thu Jun 13 17:58:18.874 2024] [ 0.000000] psci: Using standard PSCI v0.2 function IDs [Thu Jun 13 17:58:18.874 2024] [ 0.000000] psci: Trusted OS migration not required [Thu Jun 13 17:58:18.874 2024] [ 0.000000] psci: SMC Calling Convention v1.4 [Thu Jun 13 17:58:18.890 2024] [ 0.000000] percpu: Embedded 21 pages/cpu s45952 r8192 d31872 u86016 [Thu Jun 13 17:58:18.890 2024] [ 0.000000] pcpu-alloc: s45952 r8192 d31872 u86016 alloc=21*4096 [Thu Jun 13 17:58:18.890 2024] [ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3 [Thu Jun 13 17:58:18.905 2024] [ 0.000000] Detected VIPT I-cache on CPU0 [Thu Jun 13 17:58:18.905 2024] [ 0.000000] CPU features: detected: GIC system register CPU interface [Thu Jun 13 17:58:18.905 2024] [ 0.000000] CPU features: kernel page table isolation disabled by kernel configuration [Thu Jun 13 17:58:18.921 2024] [ 0.000000] CPU features: detected: ARM erratum 845719 [Thu Jun 13 17:58:18.921 2024] [ 0.000000] alternatives: applying boot alternatives [Thu Jun 13 17:58:18.936 2024] [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096 [Thu Jun 13 17:58:18.936 2024] [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),98048k@32m(ospi.rootfs),256k@130816k(ospi.phypattern);omap2-nand.0:2m(NAND.tiboot3),2m(NAND.tispl),2m(NAND.tiboot3.backup),4m(NAND.u-boot),256k(NAND.u-boot-env),256k(NAND.u-boot-env.backup),-(NAND.file-system) root=PARTUUID=580e0f6e-7c32-4f11-b947-84e486a51e62 rw rootfstype=ext4 rootwait systemd.show_status=no loglevel=8 syntec_extend= [Thu Jun 13 17:58:18.983 2024] [ 0.000000] Unknown kernel command line parameters "syntec_extend=", will be passed to user space. [Thu Jun 13 17:58:18.999 2024] [ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [Thu Jun 13 17:58:18.999 2024] [ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [Thu Jun 13 17:58:19.015 2024] [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [Thu Jun 13 17:58:19.015 2024] [ 0.000000] Memory: 1845668K/2097152K available (10752K kernel code, 1216K rwdata, 2600K rodata, 1856K init, 424K bss, 120412K reserved, 131072K cma-reserved) [Thu Jun 13 17:58:19.030 2024] [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [Thu Jun 13 17:58:19.030 2024] [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [Thu Jun 13 17:58:19.046 2024] [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4. [Thu Jun 13 17:58:19.046 2024] [ 0.000000] rcu: RCU_SOFTIRQ processing moved to rcuc kthreads. [Thu Jun 13 17:58:19.061 2024] [ 0.000000] No expedited grace period (rcu_normal_after_boot). [Thu Jun 13 17:58:19.061 2024] [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 100 jiffies. [Thu Jun 13 17:58:19.061 2024] [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [Thu Jun 13 17:58:19.077 2024] [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [Thu Jun 13 17:58:19.077 2024] [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [Thu Jun 13 17:58:19.093 2024] [ 0.000000] GICv3: 256 SPIs implemented [Thu Jun 13 17:58:19.093 2024] [ 0.000000] GICv3: 0 Extended SPIs implemented [Thu Jun 13 17:58:19.093 2024] [ 0.000000] Root IRQ handler: 0xffff800008412db0 [Thu Jun 13 17:58:19.093 2024] [ 0.000000] GICv3: GICv3 features: 16 PPIs [Thu Jun 13 17:58:19.108 2024] [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000 [Thu Jun 13 17:58:19.108 2024] [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [Thu Jun 13 17:58:19.108 2024] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [Thu Jun 13 17:58:19.124 2024] [ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19 [Thu Jun 13 17:58:19.124 2024] [ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0) [Thu Jun 13 17:58:19.140 2024] [ 0.000000] ITS: using cache flushing for cmd queue [Thu Jun 13 17:58:19.140 2024] [ 0.000000] GICv3: using LPI property table @0x0000000080020000 [Thu Jun 13 17:58:19.155 2024] [ 0.000000] GIC: using cache flushing for LPI property table [Thu Jun 13 17:58:19.155 2024] [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080030000 [Thu Jun 13 17:58:19.155 2024] [ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention. [Thu Jun 13 17:58:19.171 2024] [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [Thu Jun 13 17:58:19.171 2024] [ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [Thu Jun 13 17:58:19.186 2024] [ 0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [Thu Jun 13 17:58:19.202 2024] [ 0.000244] Console: colour dummy device 80x25 [Thu Jun 13 17:58:19.202 2024] [ 0.529230] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=200000) [Thu Jun 13 17:58:19.218 2024] [ 0.529241] pid_max: default: 32768 minimum: 301 [Thu Jun 13 17:58:19.218 2024] [ 0.529327] LSM: Security Framework initializing [Thu Jun 13 17:58:19.218 2024] [ 0.529453] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [Thu Jun 13 17:58:19.233 2024] [ 0.529476] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [Thu Jun 13 17:58:19.233 2024] [ 0.531205] rcu: Hierarchical SRCU implementation. [Thu Jun 13 17:58:19.249 2024] [ 0.531213] rcu: Max phase no-delay instances is 400. [Thu Jun 13 17:58:19.249 2024] [ 0.531257] printk: bootconsole [ns16550a0] printing thread started [Thu Jun 13 17:58:19.264 2024] [ 0.583703] Platform MSI: msi-controller@1820000 domain created [Thu Jun 13 17:58:19.264 2024] [ 0.583939] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created [Thu Jun 13 17:58:19.264 2024] [ 0.584029] EFI services will not be available. [Thu Jun 13 17:58:19.280 2024] [ 0.584266] smp: Bringing up secondary CPUs ... [Thu Jun 13 17:58:19.280 2024] [ 0.585033] Detected VIPT I-cache on CPU1 [Thu Jun 13 17:58:19.280 2024] [ 0.585150] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000 [Thu Jun 13 17:58:19.296 2024] [ 0.585167] GICv3: CPU1: using allocated LPI pending table @0x0000000080040000 [Thu Jun 13 17:58:19.296 2024] [ 0.585223] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [Thu Jun 13 17:58:19.311 2024] [ 0.635279] Detected VIPT I-cache on CPU2 [Thu Jun 13 17:58:19.311 2024] [ 0.635373] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000 [Thu Jun 13 17:58:19.311 2024] [ 0.635386] GICv3: CPU2: using allocated LPI pending table @0x0000000080050000 [Thu Jun 13 17:58:19.327 2024] [ 0.635420] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] [Thu Jun 13 17:58:19.327 2024] [ 0.661292] Detected VIPT I-cache on CPU3 [Thu Jun 13 17:58:19.343 2024] [ 0.661377] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000 [Thu Jun 13 17:58:19.343 2024] [ 0.661389] GICv3: CPU3: using allocated LPI pending table @0x0000000080060000 [Thu Jun 13 17:58:19.358 2024] [ 0.661420] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] [Thu Jun 13 17:58:19.358 2024] [ 0.661480] smp: Brought up 1 node, 4 CPUs [Thu Jun 13 17:58:19.358 2024] [ 0.661488] SMP: Total of 4 processors activated. [Thu Jun 13 17:58:19.374 2024] [ 0.695687] CPU features: detected: 32-bit EL0 Support [Thu Jun 13 17:58:19.374 2024] [ 0.695691] CPU features: detected: CRC32 instructions [Thu Jun 13 17:58:19.374 2024] [ 0.695736] CPU: All CPU(s) started at EL2 [Thu Jun 13 17:58:19.390 2024] [ 0.695739] alternatives: applying system-wide alternatives [Thu Jun 13 17:58:19.390 2024] [ 0.697256] devtmpfs: initialized [Thu Jun 13 17:58:19.390 2024] [ 0.709077] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 1911260446275000 ns [Thu Jun 13 17:58:19.405 2024] [ 0.709103] futex hash table entries: 1024 (order: 4, 65536 bytes, linear) [Thu Jun 13 17:58:19.405 2024] [ 0.714197] pinctrl core: initialized pinctrl subsystem [Thu Jun 13 17:58:19.421 2024] [ 0.714931] DMI not present or invalid. [Thu Jun 13 17:58:19.421 2024] [ 0.715466] NET: Registered PF_NETLINK/PF_ROUTE protocol family [Thu Jun 13 17:58:19.421 2024] [ 0.729158] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations [Thu Jun 13 17:58:19.436 2024] [ 0.729528] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [Thu Jun 13 17:58:19.436 2024] [ 0.729750] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [Thu Jun 13 17:58:19.452 2024] [ 0.729886] audit: initializing netlink subsys (disabled) [Thu Jun 13 17:58:19.452 2024] [ 0.730055] audit: type=2000 audit(0.728:1): state=initialized audit_enabled=0 res=1 [Thu Jun 13 17:58:19.468 2024] [ 0.730665] thermal_sys: Registered thermal governor 'step_wise' [Thu Jun 13 17:58:19.468 2024] [ 0.730670] thermal_sys: Registered thermal governor 'power_allocator' [Thu Jun 13 17:58:19.468 2024] [ 0.730892] ASID allocator initialised with 65536 entries [Thu Jun 13 17:58:19.483 2024] [ 0.745792] platform 30200000.dss: Fixed dependency cycle(s) with /display0 [Thu Jun 13 17:58:19.483 2024] [ 0.754786] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages [Thu Jun 13 17:58:19.499 2024] [ 0.754808] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page [Thu Jun 13 17:58:19.499 2024] [ 0.754814] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages [Thu Jun 13 17:58:19.514 2024] [ 0.754816] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page [Thu Jun 13 17:58:19.514 2024] [ 0.754820] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages [Thu Jun 13 17:58:19.514 2024] [ 0.754823] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page [Thu Jun 13 17:58:19.530 2024] [ 0.754827] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages [Thu Jun 13 17:58:19.530 2024] [ 0.754830] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page [Thu Jun 13 17:58:19.546 2024] [ 0.760145] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected [Thu Jun 13 17:58:19.546 2024] [ 0.762284] iommu: Default domain type: Translated [Thu Jun 13 17:58:19.561 2024] [ 0.762294] iommu: DMA domain TLB invalidation policy: strict mode [Thu Jun 13 17:58:19.561 2024] [ 0.762632] SCSI subsystem initialized [Thu Jun 13 17:58:19.561 2024] [ 0.762749] libata version 3.00 loaded. [Thu Jun 13 17:58:19.561 2024] [ 0.762994] usbcore: registered new interface driver usbfs [Thu Jun 13 17:58:19.577 2024] [ 0.763033] usbcore: registered new interface driver hub [Thu Jun 13 17:58:19.577 2024] [ 0.763062] usbcore: registered new device driver usb [Thu Jun 13 17:58:19.593 2024] [ 0.763410] pps_core: LinuxPPS API ver. 1 registered [Thu Jun 13 17:58:19.593 2024] [ 0.763413] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [Thu Jun 13 17:58:19.593 2024] [ 0.763428] PTP clock support registered [Thu Jun 13 17:58:19.608 2024] [ 0.763581] EDAC MC: Ver: 3.0.0 [Thu Jun 13 17:58:19.608 2024] [ 0.764448] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fc9100 [Thu Jun 13 17:58:19.608 2024] [ 0.764785] FPGA manager framework [Thu Jun 13 17:58:19.624 2024] [ 0.764909] Advanced Linux Sound Architecture Driver Initialized. [Thu Jun 13 17:58:19.624 2024] [ 0.765742] vgaarb: loaded [Thu Jun 13 17:58:19.624 2024] [ 0.765992] clocksource: Switched to clocksource arch_sys_counter [Thu Jun 13 17:58:19.639 2024] [ 0.766240] VFS: Disk quotas dquot_6.6.0 [Thu Jun 13 17:58:19.639 2024] [ 0.766277] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [Thu Jun 13 17:58:19.639 2024] [ 0.772577] NET: Registered PF_INET protocol family [Thu Jun 13 17:58:19.655 2024] [ 0.772848] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear) [Thu Jun 13 17:58:19.655 2024] [ 0.774594] tcp_listen_portaddr_hash hash table entries: 1024 (order: 3, 40960 bytes, linear) [Thu Jun 13 17:58:19.671 2024] [ 0.774715] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear) [Thu Jun 13 17:58:19.671 2024] [ 0.774733] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear) [Thu Jun 13 17:58:19.702 2024] [ 0.774952] TCP bind hash table entries: 16384 (order: 8, 1310720 bytes, linear) [Thu Jun 13 17:58:19.718 2024] [ 0.776692] TCP: Hash tables configured (established 16384 bind 16384) [Thu Jun 13 17:58:19.718 2024] [.776929] UDP hash table entries: 1024 (order: 4, 98304 bytes, linear) [Thu Jun 13 17:58:19.733 2024] [[ 1.055968] printk: console [ttyS2] printing thread started [Thu Jun 13 17:58:19.733 2024] 0.777138] UDP-Lite hash table entries: 1024 (order: 4, 98304 bytes, linear) [Thu Jun 13 17:58:19.749 2024] [ 1.056021] printk: console [ttyS2] enabled [Thu Jun 13 17:58:19.749 2024] [ 1.056025] printk: bootconsole [ns16550a0] disabled [Thu Jun 13 17:58:19.749 2024] [ 1.068862] printk: bootconsole [ns16550a0] printing thread stopped [Thu Jun 13 17:58:19.764 2024] [ 1.070160] 2810000.serial: ttyS1 at MMIO 0x2810000 (irq = 288, base_baud = 3000000) is a 8250 [Thu Jun 13 17:58:19.811 2024] [ 1.074000] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0 [Thu Jun 13 17:58:19.811 2024] [ 1.078270] Console: switching to colour dummy device 80x25 [Thu Jun 13 17:58:19.827 2024] [ 1.120582] Console: switching to colour frame buffer device 171x48 [Thu Jun 13 17:58:19.827 2024] [ 1.137208] tidss 30200000.dss: [drm] fb0: tidssdrmfb frame buffer device [Thu Jun 13 17:58:19.843 2024] [ 1.139140] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode [Thu Jun 13 17:58:19.843 2024] [ 1.173014] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [Thu Jun 13 17:58:19.858 2024] [ 1.173309] mdio_bus 8000f00.mdio: MDIO device at address 0 is missing. [Thu Jun 13 17:58:19.858 2024] [ 1.174943] davinci_mdio 8000f00.mdio: phy[3]: device 8000f00.mdio:03, driver TI DP83822 [Thu Jun 13 17:58:19.874 2024] [ 1.175023] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006 [Thu Jun 13 17:58:19.889 2024] [ 1.175313] am65-cpsw-nuss 8000000.ethernet: Use random MAC address [Thu Jun 13 17:58:19.889 2024] [ 1.175325] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5 [Thu Jun 13 17:58:19.889 2024] [ 1.175330] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512 [Thu Jun 13 17:58:19.905 2024] [ 1.176124] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0 [Thu Jun 13 17:58:19.905 2024] [ 1.196384] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19 [Thu Jun 13 17:58:19.921 2024] [ 1.201368] physmap-flash 50000000.fpgaBus: physmap platform flash device: [mem 0x50000000-0x50ffffff] [Thu Jun 13 17:58:19.921 2024] [ 1.202478] mmc1: CQHCI version 5.10 [Thu Jun 13 17:58:19.936 2024] [ 1.203563] mmc2: CQHCI version 5.10 [Thu Jun 13 17:58:19.936 2024] [ 1.203755] mmc0: CQHCI version 5.10 [Thu Jun 13 17:58:19.936 2024] [ 1.205492] physmap-flash 51000000.fpgaBus: physmap platform flash device: [mem 0x51000000-0x51ffffff] [Thu Jun 13 17:58:19.952 2024] [ 1.207995] physmap-flash 52000000.fpgaBus: physmap platform flash device: [mem 0x52000000-0x52ffffff] [Thu Jun 13 17:58:19.952 2024] [ 1.218167] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present! [Thu Jun 13 17:58:19.968 2024] [ 1.221028] debugfs: Directory 'pd:186' with parent 'pm_genpd' already present! [Thu Jun 13 17:58:19.968 2024] [ 1.233547] ALSA device list: [Thu Jun 13 17:58:19.968 2024] [ 1.233557] No soundcards found. [Thu Jun 13 17:58:19.968 2024] [ 1.239562] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit [Thu Jun 13 17:58:19.983 2024] [ 1.245077] mmc2: SDHCI controller on fa20000.mmc [fa20000.mmc] using ADMA 64-bit [Thu Jun 13 17:58:19.983 2024] [ 1.254327] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit [Thu Jun 13 17:58:19.999 2024] [ 1.254505] Waiting for root device PARTUUID=580e0f6e-7c32-4f11-b947-84e486a51e62... [Thu Jun 13 17:58:20.014 2024] [ 1.312639] [BSP] mmc0: Command Queue supported depth 32 [Thu Jun 13 17:58:20.014 2024] [ 1.318165] mmc0: new HS200 MMC card at address 0001 [Thu Jun 13 17:58:20.014 2024] [ 1.319007] mmcblk0: mmc0:0001 016GB0 14.7 GiB [Thu Jun 13 17:58:20.014 2024] [ 1.323257] mmcblk0: p1 p2 p3 p4 p5 [Thu Jun 13 17:58:20.030 2024] [ 1.324510] mmcblk0boot0: mmc0:0001 016GB0 4.00 MiB [Thu Jun 13 17:58:20.030 2024] [ 1.326266] mmcblk0boot1: mmc0:0001 016GB0 4.00 MiB [Thu Jun 13 17:58:20.030 2024] [ 1.327619] mmcblk0rpmb: mmc0:0001 016GB0 4.00 MiB, chardev (241:0) [Thu Jun 13 17:58:20.046 2024] [ 1.342994] mmc1: new MMC card at address 0001 [Thu Jun 13 17:58:20.046 2024] [ 1.344232] mmcblk1: mmc1:0001 004GA1 3.69 GiB [Thu Jun 13 17:58:20.046 2024] [ 1.346609] mmcblk1: p1 [Thu Jun 13 17:58:20.046 2024] [ 1.347376] mmcblk1boot0: mmc1:0001 004GA1 2.00 MiB [Thu Jun 13 17:58:20.061 2024] [ 1.349269] mmcblk1boot1: mmc1:0001 004GA1 2.00 MiB [Thu Jun 13 17:58:20.061 2024] [ 1.350712] mmcblk1rpmb: mmc1:0001 004GA1 512 KiB, chardev (241:1) [Thu Jun 13 17:58:20.061 2024] [ 1.358552] EXT4-fs (mmcblk0p4): recovery complete [Thu Jun 13 17:58:20.077 2024] [ 1.358969] EXT4-fs (mmcblk0p4): mounted filesystem with ordered data mode. Quota mode: none. [Thu Jun 13 17:58:20.077 2024] [ 1.359081] VFS: Mounted root (ext4 filesystem) on device 179:4. [Thu Jun 13 17:58:20.093 2024] [ 1.359295] devtmpfs: mounted [Thu Jun 13 17:58:20.093 2024] [ 1.360732] Freeing unused kernel memory: 1856K [Thu Jun 13 17:58:20.093 2024] [ 1.360867] Run /sbin/init as init process [Thu Jun 13 17:58:20.093 2024] [ 1.360871] with arguments: [Thu Jun 13 17:58:20.108 2024] [ 1.360873] /sbin/init [Thu Jun 13 17:58:20.108 2024] [ 1.360874] with environment: [Thu Jun 13 17:58:20.108 2024] [ 1.360876] HOME=/ [Thu Jun 13 17:58:20.108 2024] [ 1.360878] TERM=linux [Thu Jun 13 17:58:20.108 2024] [ 1.360880] syntec_extend= [Thu Jun 13 17:58:20.155 2024] [ 1.480918] systemd[1]: System time before build time, advancing clock. [Thu Jun 13 17:58:20.186 2024] [ 1.512395] NET: Registered PF_INET6 protocol family [Thu Jun 13 17:58:20.186 2024] [ 1.513636] Segment Routing with IPv6 [Thu Jun 13 17:58:20.202 2024] [ 1.513671] In-situ OAM (IOAM) with IPv6 [Thu Jun 13 17:58:20.202 2024] [ 1.526859] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid) [Thu Jun 13 17:58:20.233 2024] [ 1.527476] systemd[1]: Detected architecture arm64. [Thu Jun 13 17:58:20.233 2024] [ 1.530084] systemd[1]: Hostname set to <am62xx-evm>. [Thu Jun 13 17:58:20.311 2024] [ 1.642400] systemd-sysv-generator[184]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust. [Thu Jun 13 17:58:20.639 2024] [ 1.973403] systemd[1]: Configuration file /etc/systemd/system/syntec-rename-network.service is marked executable. Please remove executable permission bits. Proceeding anyway. [Thu Jun 13 17:58:20.655 2024] [ 1.976244] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether. [Thu Jun 13 17:58:20.718 2024] [ 2.038539] systemd[1]: Queued start job for default target Graphical Interface. [Thu Jun 13 17:58:20.718 2024] [ 2.042247] systemd[1]: Created slice Slice /system/modprobe. [Thu Jun 13 17:58:20.718 2024] [ 2.043841] systemd[1]: Created slice Slice /system/serial-getty. [Thu Jun 13 17:58:20.733 2024] [ 2.044413] systemd[1]: Created slice User and Session Slice. [Thu Jun 13 17:58:20.733 2024] [ 2.044769] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [Thu Jun 13 17:58:20.749 2024] [ 2.044971] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [Thu Jun 13 17:58:20.749 2024] [ 2.045359] systemd[1]: Reached target Path Units. [Thu Jun 13 17:58:20.749 2024] [ 2.045460] systemd[1]: Reached target Remote File Systems. [Thu Jun 13 17:58:20.764 2024] [ 2.045543] systemd[1]: Reached target Slice Units. [Thu Jun 13 17:58:20.764 2024] [ 2.045629] systemd[1]: Reached target Swaps. [Thu Jun 13 17:58:20.764 2024] [ 2.050195] systemd[1]: Listening on RPCbind Server Activation Socket. [Thu Jun 13 17:58:20.780 2024] [ 2.050379] systemd[1]: Reached target RPC Port Mapper. [Thu Jun 13 17:58:20.780 2024] [ 2.056568] systemd[1]: Listening on Process Core Dump Socket. [Thu Jun 13 17:58:20.796 2024] [ 2.057038] systemd[1]: Listening on initctl Compatibility Named Pipe. [Thu Jun 13 17:58:20.796 2024] [ 2.057869] systemd[1]: Listening on Journal Audit Socket. [Thu Jun 13 17:58:20.796 2024] [ 2.058516] systemd[1]: Listening on Journal Socket (/dev/log). [Thu Jun 13 17:58:20.811 2024] [ 2.059206] systemd[1]: Listening on Journal Socket. [Thu Jun 13 17:58:20.811 2024] [ 2.060070] systemd[1]: Listening on Network Service Netlink Socket. [Thu Jun 13 17:58:20.811 2024] [ 2.061940] systemd[1]: Listening on udev Control Socket. [Thu Jun 13 17:58:20.827 2024] [ 2.062501] systemd[1]: Listening on udev Kernel Socket. [Thu Jun 13 17:58:20.827 2024] [ 2.062956] systemd[1]: Listening on User Database Manager Socket. [Thu Jun 13 17:58:20.842 2024] [ 2.085786] systemd[1]: Mounting Huge Pages File System... [Thu Jun 13 17:58:20.842 2024] [ 2.090027] systemd[1]: Mounting POSIX Message Queue File System... [Thu Jun 13 17:58:20.842 2024] [ 2.094540] systemd[1]: Mounting Kernel Debug File System... [Thu Jun 13 17:58:20.858 2024] [ 2.095470] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing). [Thu Jun 13 17:58:20.889 2024] [ 2.096797] systemd[1]: tmp.mount: Directory /tmp to mount over is not empty, mounting anyway. [Thu Jun 13 17:58:20.889 2024] [ 2.100779] systemd[1]: Mounting Temporary Directory /tmp... [Thu Jun 13 17:58:20.905 2024] [ 2.106561] systemd[1]: Starting Create List of Static Device Nodes... [Thu Jun 13 17:58:20.905 2024] [ 2.112305] systemd[1]: Starting Load Kernel Module configfs... [Thu Jun 13 17:58:20.921 2024] [ 2.117665] systemd[1]: Starting Load Kernel Module drm... [Thu Jun 13 17:58:20.921 2024] [ 2.123297] systemd[1]: Starting Load Kernel Module fuse... [Thu Jun 13 17:58:20.921 2024] [ 2.129749] systemd[1]: Starting RPC Bind... [Thu Jun 13 17:58:20.936 2024] [ 2.130439] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/). [Thu Jun 13 17:58:20.936 2024] [ 2.131906] systemd[1]: systemd-journald.service: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling. [Thu Jun 13 17:58:20.952 2024] [ 2.131944] systemd[1]: (This warning is only shown for the first unit using IP firewalling.) [Thu Jun 13 17:58:20.967 2024] [ 2.135837] systemd[1]: Starting Journal Service... [Thu Jun 13 17:58:20.967 2024] [ 2.141298] fuse: init (API version 7.37) [Thu Jun 13 17:58:20.967 2024] [ 2.145428] systemd[1]: Starting Load Kernel Modules... [Thu Jun 13 17:58:20.983 2024] [ 2.150255] systemd[1]: Starting Generate network units from Kernel command line... [Thu Jun 13 17:58:20.983 2024] [ 2.155665] systemd[1]: Starting Remount Root and Kernel File Systems... [Thu Jun 13 17:58:20.983 2024] [ 2.160950] systemd[1]: Starting Coldplug All udev Devices... [Thu Jun 13 17:58:20.999 2024] [ 2.166238] systemd[1]: Starting Setup Virtual Console... [Thu Jun 13 17:58:20.999 2024] [ 2.178595] systemd[1]: Mounted Huge Pages File System. [Thu Jun 13 17:58:21.014 2024] [ 2.179551] systemd[1]: Mounted POSIX Message Queue File System. [Thu Jun 13 17:58:21.014 2024] [ 2.180339] systemd[1]: Mounted Kernel Debug File System. [Thu Jun 13 17:58:21.014 2024] [ 2.181115] systemd[1]: Mounted Temporary Directory /tmp. [Thu Jun 13 17:58:21.030 2024] [ 2.183403] systemd[1]: Finished Create List of Static Device Nodes. [Thu Jun 13 17:58:21.030 2024] [ 2.185338] systemd[1]: modprobe@configfs.service: Deactivated successfully. [Thu Jun 13 17:58:21.046 2024] [ 2.186200] systemd[1]: Finished Load Kernel Module configfs. [Thu Jun 13 17:58:21.046 2024] [ 2.187239] systemd[1]: Started RPC Bind. [Thu Jun 13 17:58:21.046 2024] [ 2.189863] systemd[1]: modprobe@drm.service: Deactivated successfully. [Thu Jun 13 17:58:21.061 2024] [ 2.190618] systemd[1]: Finished Load Kernel Module drm. [Thu Jun 13 17:58:21.061 2024] [ 2.192652] systemd[1]: modprobe@fuse.service: Deactivated successfully. [Thu Jun 13 17:58:21.061 2024] [ 2.193575] systemd[1]: Finished Load Kernel Module fuse. [Thu Jun 13 17:58:21.077 2024] [ 2.199528] systemd[1]: Mounting FUSE Control File System... [Thu Jun 13 17:58:21.077 2024] [ 2.204807] systemd[1]: Mounting Kernel Configuration File System... [Thu Jun 13 17:58:21.077 2024] [ 2.221316] cryptodev: loading out-of-tree module taints kernel. [Thu Jun 13 17:58:21.092 2024] [ 2.224740] EXT4-fs (mmcblk0p4): re-mounted. Quota mode: none. [Thu Jun 13 17:58:21.092 2024] [ 2.230234] systemd[1]: Finished Setup Virtual Console. [Thu Jun 13 17:58:21.108 2024] [ 2.234749] cryptodev: driver 1.12 loaded. [Thu Jun 13 17:58:21.108 2024] [ 2.250419] systemd[1]: Finished Load Kernel Modules. [Thu Jun 13 17:58:21.108 2024] [ 2.251731] systemd[1]: Finished Generate network units from Kernel command line. [Thu Jun 13 17:58:21.124 2024] [ 2.253204] systemd[1]: Finished Remount Root and Kernel File Systems. [Thu Jun 13 17:58:21.124 2024] [ 2.256153] systemd[1]: Mounted FUSE Control File System. [Thu Jun 13 17:58:21.124 2024] [ 2.256842] systemd[1]: Mounted Kernel Configuration File System. [Thu Jun 13 17:58:21.139 2024] [ 2.259885] systemd[1]: Rebuild Hardware Database was skipped because of a failed condition check (ConditionNeedsUpdate=/etc). [Thu Jun 13 17:58:21.155 2024] [ 2.260306] systemd[1]: Platform Persistent Storage Archival was skipped because of a failed condition check (ConditionDirectoryNotEmpty=/sys/fs/pstore). [Thu Jun 13 17:58:21.155 2024] [ 2.292503] systemd[1]: Starting Apply Kernel Variables... [Thu Jun 13 17:58:21.171 2024] [ 2.292948] systemd[1]: Create System Users was skipped because of a failed condition check (ConditionNeedsUpdate=/etc). [Thu Jun 13 17:58:21.171 2024] [ 2.297441] systemd[1]: Starting Create Static Device Nodes in /dev... [Thu Jun 13 17:58:21.186 2024] [ 2.299146] systemd[1]: Started Journal Service. [Thu Jun 13 17:58:21.186 2024] [ 2.347354] systemd-journald[197]: Received client request to flush runtime journal. [Thu Jun 13 17:58:21.530 2024] [ 2.852227] fram@0 enforce active low on chipselect handle [Thu Jun 13 17:58:21.530 2024] [ 2.861598] rtc-s35390a 1-0030: registered as rtc0 [Thu Jun 13 17:58:21.546 2024] [ 2.862687] rtc-s35390a 1-0030: setting system clock to 2024-06-13T18:02:36 UTC (1718301756) [Thu Jun 13 17:58:21.546 2024] [ 2.863040] systemd-journald[197]: Oldest entry in /run/log/journal/d31152b6b9414e1bb0002edccf0447b9/system.journal is older than the configured file retention duration (1month), suggesting rotation. [Thu Jun 13 17:58:21.593 2024] [ 2.863059] systemd-journald[197]: /run/log/journal/d31152b6b9414e1bb0002edccf0447b9/system.journal: Journal header limits reached or header out-of-date, rotating. [Thu Jun 13 17:58:21.640 2024] [ 2.866398] systemd-journald[197]: Oldest entry in /run/log/journal/d31152b6b9414e1bb0002edccf0447b9/system.journal is older than the configured file retention duration (1month), suggesting rotation. [Thu Jun 13 17:58:21.655 2024] [ 2.866431] systemd-journald[197]: /run/log/journal/d31152b6b9414e1bb0002edccf0447b9/system.journal: Journal header limits reached or header out-of-date, rotating. [Thu Jun 13 17:58:21.686 2024] [ 2.882778] mc: Linux media interface: v0.10 [Thu Jun 13 17:58:21.686 2024] [ 2.912534] videodev: Linux video capture interface: v2.00 [Thu Jun 13 17:58:21.702 2024] [ 3.020454] k3-m4-rproc 5000000.m4fss: assigned reserved memory node m4f-dma-memory@9cb00000 [Thu Jun 13 17:58:21.702 2024] [ 3.020654] k3-m4-rproc 5000000.m4fss: configured M4 for remoteproc mode [Thu Jun 13 17:58:21.718 2024] [ 3.020720] k3-m4-rproc 5000000.m4fss: local reset is deasserted for device [Thu Jun 13 17:58:21.718 2024] [ 3.021081] remoteproc remoteproc0: 5000000.m4fss is available [Thu Jun 13 17:58:21.733 2024] [ 3.022592] remoteproc remoteproc0: Direct firmware load for am62-mcu-m4f0_0-fw failed with error -2 [Thu Jun 13 17:58:21.733 2024] [ 3.022619] remoteproc remoteproc0: powering up 5000000.m4fss [Thu Jun 13 17:58:21.749 2024] [ 3.022660] remoteproc remoteproc0: Direct firmware load for am62-mcu-m4f0_0-fw failed with error -2 [Thu Jun 13 17:58:21.749 2024] [ 3.022669] remoteproc remoteproc0: request_firmware failed: -2 [Thu Jun 13 17:58:21.858 2024] [ 3.187168] rtc-ti-k3 2b1f0000.rtc: registered as rtc1 [Thu Jun 13 17:58:21.874 2024] [ 3.195865] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1) [Thu Jun 13 17:58:21.874 2024] [ 3.199204] platform 78000000.r5f: configured R5F for IPC-only mode [Thu Jun 13 17:58:21.890 2024] [ 3.199427] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@9da00000 [Thu Jun 13 17:58:21.890 2024] [ 3.201671] remoteproc remoteproc1: 78000000.r5f is available [Thu Jun 13 17:58:21.905 2024] [ 3.201755] remoteproc remoteproc1: attaching to 78000000.r5f [Thu Jun 13 17:58:21.905 2024] [ 3.213919] platform 31000000.usb: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/tps6598x@3f/connector [Thu Jun 13 17:58:21.921 2024] [ 3.216090] platform 78000000.r5f: R5F core initialized in IPC-only mode [Thu Jun 13 17:58:21.921 2024] [ 3.216125] rproc-virtio rproc-virtio.3.auto: assigned reserved memory node r5f-dma-memory@9da00000 [Thu Jun 13 17:58:21.936 2024] [ 3.221405] virtio_rpmsg_bus virtio0: rpmsg host is online [Thu Jun 13 17:58:21.936 2024] [ 3.221456] rproc-virtio rproc-virtio.3.auto: registered virtio0 (type 7) [Thu Jun 13 17:58:21.952 2024] [ 3.221466] remoteproc remoteproc1: remote processor 78000000.r5f is now attached [Thu Jun 13 17:58:21.952 2024] [ 3.221562] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd [Thu Jun 13 17:58:21.968 2024] [ 3.221751] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe [Thu Jun 13 17:58:22.046 2024] [ 3.368974] Init FPGA interrupt driver (1.0) [Thu Jun 13 17:58:22.046 2024] [ 3.377172] Get kick_gpio number= (418) [Thu Jun 13 17:58:22.327 2024] [ 3.659075] random: crng init done [Thu Jun 13 17:58:23.046 2024] [ 4.370663] fm25_syntec spi2.0: 32 KByte fm25 fram, pagesize 4096 [Thu Jun 13 17:58:23.124 2024] [ 4.448340] remoteproc remoteproc2: 30074000.pru is available [Thu Jun 13 17:58:23.124 2024] [ 4.449659] remoteproc remoteproc3: 30078000.pru is available [Thu Jun 13 17:58:23.296 2024] [ 4.620510] cdns-csi2rx: probe of 30101000.csi-bridge failed with error -22 [Thu Jun 13 17:58:23.296 2024] [ 4.630720] xhci-hcd xhci-hcd.4.auto: xHCI Host Controller [Thu Jun 13 17:58:23.312 2024] [ 4.630780] xhci-hcd xhci-hcd.4.auto: new USB bus registered, assigned bus number 1 [Thu Jun 13 17:58:23.327 2024] [ 4.631775] xhci-hcd xhci-hcd.4.auto: USB3 root hub has no ports [Thu Jun 13 17:58:23.327 2024] [ 4.631807] xhci-hcd xhci-hcd.4.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000000000010010 [Thu Jun 13 17:58:23.343 2024] [ 4.661629] xhci-hcd xhci-hcd.4.auto: irq 471, io mem 0x31100000 [Thu Jun 13 17:58:23.343 2024] [ 4.663108] hub 1-0:1.0: USB hub found [Thu Jun 13 17:58:23.358 2024] [ 4.663185] hub 1-0:1.0: 1 port detected [Thu Jun 13 17:58:23.577 2024] [ 4.901162] usb 1-1: new high-speed USB device number 2 using xhci-hcd [Thu Jun 13 17:58:23.749 2024] [ 5.078426] hub 1-1:1.0: USB hub found [Thu Jun 13 17:58:23.749 2024] [ 5.078670] hub 1-1:1.0: 4 ports detected [Thu Jun 13 17:58:23.780 2024] [ 5.110819] EXT4-fs (mmcblk0p2): recovery complete [Thu Jun 13 17:58:23.796 2024] [ 5.110861] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Quota mode: none. [Thu Jun 13 17:58:23.905 2024] [ 5.238885] EXT4-fs (mmcblk0p3): recovery complete [Thu Jun 13 17:58:23.921 2024] [ 5.238920] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Quota mode: none. [Thu Jun 13 17:58:24.093 2024] [ 5.427760] cfg80211: Loading compiled-in X.509 certificates for regulatory database [Thu Jun 13 17:58:24.108 2024] [ 5.443945] EXT4-fs (mmcblk0p1): recovery complete [Thu Jun 13 17:58:24.124 2024] [ 5.445094] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Quota mode: none. [Thu Jun 13 17:58:24.140 2024] [ 5.455248] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [Thu Jun 13 17:58:24.140 2024] [ 5.458343] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 [Thu Jun 13 17:58:24.155 2024] [ 5.458382] cfg80211: failed to load regulatory.db [Thu Jun 13 17:58:24.155 2024] [ 5.475274] EXT4-fs (mmcblk0p5): Using encoding defined by superblock: utf8-12.1.0 with flags 0x1 [Thu Jun 13 17:58:24.218 2024] [ 5.539136] usb 1-1.3: new low-speed USB device number 3 using xhci-hcd [Thu Jun 13 17:58:24.234 2024] [ 5.562240] EXT4-fs (mmcblk0p5): recovery complete [Thu Jun 13 17:58:24.234 2024] [ 5.562762] EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Quota mode: none. [Thu Jun 13 17:58:24.265 2024] [ 5.596126] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:03] driver [TI DP83822] (irq=POLL) [Thu Jun 13 17:58:24.280 2024] [ 5.596163] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rmii link mode [Thu Jun 13 17:58:24.421 2024] [ 5.754095] EXT4-fs (mmcblk1p1): Using encoding defined by superblock: utf8-12.1.0 with flags 0x1 [Thu Jun 13 17:58:24.499 2024] [ 5.825396] EXT4-fs (mmcblk1p1): recovery complete [Thu Jun 13 17:58:24.515 2024] [ 5.831028] EXT4-fs (mmcblk1p1): mounted filesystem with ordered data mode. Quota mode: none. [Thu Jun 13 17:58:24.515 2024] [ 5.849557] usbcore: registered new interface driver usbhid [Thu Jun 13 17:58:24.530 2024] [ 5.849577] usbhid: USB HID core driver [Thu Jun 13 17:58:24.546 2024] [ 5.867848] input: Wired USB Keyboard as /devices/platform/bus@f0000/f910000.dwc3-usb/31100000.usb/xhci-hcd.4.auto/usb1/1-1/1-1.3/1-1.3:1.0/0003:0461:4E6E.0001/input/input0 [Thu Jun 13 17:58:24.593 2024] [ 5.920539] hid-generic 0003:0461:4E6E.0001: input,hidraw0: USB HID v1.10 Keyboard [Wired USB Keyboard] on usb-xhci-hcd.4.auto-1.3/input0 [Thu Jun 13 17:58:24.608 2024] [ 5.922304] input: Wired USB Keyboard System Control as /devices/platform/bus@f0000/f910000.dwc3-usb/31100000.usb/xhci-hcd.4.auto/usb1/1-1/1-1.3/1-1.3:1.1/0003:0461:4E6E.0002/input/input1 [Thu Jun 13 17:58:24.655 2024] [ 5.974936] input: Wired USB Keyboard Consumer Control as /devices/platform/bus@f0000/f910000.dwc3-usb/31100000.usb/xhci-hcd.4.auto/usb1/1-1/1-1.3/1-1.3:1.1/0003:0461:4E6E.0002/input/input2 [Thu Jun 13 17:58:24.671 2024] [ 5.976667] hid-generic 0003:0461:4E6E.0002: input,hidraw1: USB HID v1.10 Device [Wired USB Keyboard] on usb-xhci-hcd.4.auto-1.3/input1 [Thu Jun 13 17:58:24.812 2024] [ 6.138786] am65-cpsw-nuss 8000000.ethernet lan1: renamed from eth0 [Thu Jun 13 17:58:24.859 2024] [ 6.182338] am65-cpsw-nuss 8000000.ethernet lan1: PHY [8000f00.mdio:03] driver [TI DP83822] (irq=POLL) [Thu Jun 13 17:58:24.859 2024] [ 6.182383] am65-cpsw-nuss 8000000.ethernet lan1: configuring for phy/rmii link mode [Thu Jun 13 17:58:25.509 2024] *************************************************************** [Thu Jun 13 17:58:25.509 2024] *************************************************************** [Thu Jun 13 17:58:25.525 2024] NOTICE: This file system contains the following GPL-3.0 packages: [Thu Jun 13 17:58:25.525 2024] adwaita-icon-theme-symbolic [Thu Jun 13 17:58:25.525 2024] bash [Thu Jun 13 17:58:25.525 2024] cifs-utils [Thu Jun 13 17:58:25.525 2024] dosfstools [Thu Jun 13 17:58:25.525 2024] grub-common [Thu Jun 13 17:58:25.525 2024] grub-editenv [Thu Jun 13 17:58:25.525 2024] grub-efi [Thu Jun 13 17:58:25.525 2024] less [Thu Jun 13 17:58:25.540 2024] lib32-libgcc1 [Thu Jun 13 17:58:25.540 2024] lib32-libstdc++6 [Thu Jun 13 17:58:25.540 2024] libdw1 [Thu Jun 13 17:58:25.540 2024] libelf1 [Thu Jun 13 17:58:25.540 2024] libgcc1 [Thu Jun 13 17:58:25.540 2024] libgdbm-compat4 [Thu Jun 13 17:58:25.540 2024] libgdbm6 [Thu Jun 13 17:58:25.540 2024] libgmp10 [Thu Jun 13 17:58:25.540 2024] libidn2-0 [Thu Jun 13 17:58:25.540 2024] libreadline8 [Thu Jun 13 17:58:25.540 2024] libstdc++6 [Thu Jun 13 17:58:25.540 2024] libunistring2 [Thu Jun 13 17:58:25.540 2024] libvte-2.91-0 [Thu Jun 13 17:58:25.540 2024] nettle [Thu Jun 13 17:58:25.556 2024] onboard [Thu Jun 13 17:58:25.556 2024] parted [Thu Jun 13 17:58:25.556 2024] rxvt-unicode [Thu Jun 13 17:58:25.556 2024] [Thu Jun 13 17:58:25.556 2024] If you do not wish to distribute GPL-3.0 components please remove [Thu Jun 13 17:58:25.556 2024] the above packages prior to distribution. This can be done using [Thu Jun 13 17:58:25.556 2024] the opkg remove command. i.e.: [Thu Jun 13 17:58:25.571 2024] opkg remove <package> [Thu Jun 13 17:58:25.571 2024] Where <package> is the name printed in the list above [Thu Jun 13 17:58:25.571 2024] [Thu Jun 13 17:58:25.571 2024] NOTE: If the package is a dependency of another package you [Thu Jun 13 17:58:25.571 2024] will be notified of the dependent packages. You should [Thu Jun 13 17:58:25.587 2024] use the --force-removal-of-dependent-packages option to [Thu Jun 13 17:58:25.587 2024] also remove the dependent packages as well [Thu Jun 13 17:58:25.587 2024] *************************************************************** [Thu Jun 13 17:58:25.603 2024] *************************************************************** [Thu Jun 13 17:58:30.874 2024] [Thu Jun 13 17:58:30.874 2024] _____ _____ _ _ [Thu Jun 13 17:58:30.874 2024] | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ [Thu Jun 13 17:58:30.890 2024] | | _| .'| . | . | | __| _| . | | | -_| _| _| [Thu Jun 13 17:58:30.890 2024] |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| [Thu Jun 13 17:58:30.890 2024] |___| |___| [Thu Jun 13 17:58:30.890 2024] [Thu Jun 13 17:58:30.890 2024] Arago Project am62xx-evm - [Thu Jun 13 17:58:30.906 2024] [Thu Jun 13 17:58:30.906 2024] Arago 2023.10 am62xx-evm - [Thu Jun 13 17:58:30.906 2024] [Thu Jun 13 17:58:30.906 2024] am62xx-evm login: WARNING: The runtime version supported by this application is unavailable. [Thu Jun 13 17:58:31.281 2024] Using default runtime: v4.0.30319 [Thu Jun 13 17:58:31.468 2024] WARNING: The runtime version supported by this application is unavailable. [Thu Jun 13 17:58:31.468 2024] Using default runtime: v4.0.30319 [Thu Jun 13 17:58:43.739 2024] [ 25.058989] mmc0: Timeout waiting for hardware interrupt. [Thu Jun 13 17:58:43.739 2024] [ 25.059009] mmc0: sdhci: ============ SDHCI REGISTER DUMP =========== [Thu Jun 13 17:58:43.739 2024] [ 25.059019] mmc0: sdhci: Sys addr: 0x00000100 | Version: 0x00001004 [Thu Jun 13 17:58:43.754 2024] [ 25.059028] mmc0: sdhci: Blk size: 0x00007200 | Blk cnt: 0x00000000 [Thu Jun 13 17:58:43.754 2024] [ 25.059032] mmc0: sdhci: Argument: 0x005c1a58 | Trn mode: 0x0000003b [Thu Jun 13 17:58:43.770 2024] [ 25.059036] mmc0: sdhci: Present: 0x011f0060 | Host ctl: 0x0000003d [Thu Jun 13 17:58:43.770 2024] [ 25.059040] mmc0: sdhci: Power: 0x0000000b | Blk gap: 0x00000080 [Thu Jun 13 17:58:43.770 2024] [ 25.059043] mmc0: sdhci: Wake-up: 0x00000000 | Clock: 0x00000107 [Thu Jun 13 17:58:43.785 2024] [ 25.059047] mmc0: sdhci: Timeout: 0x00000000 | Int stat: 0x00000003 [Thu Jun 13 17:58:43.785 2024] [ 25.059051] mmc0: sdhci: Int enab: 0x03ff000b | Sig enab: 0x03ff000b [Thu Jun 13 17:58:43.801 2024] [ 25.059055] mmc0: sdhci: ACmd stat: 0x00000000 | Slot int: 0x00000001 [Thu Jun 13 17:58:43.801 2024] [ 25.059059] mmc0: sdhci: Caps: 0x7decc801 | Caps_1: 0x18002407 [Thu Jun 13 17:58:43.801 2024] [ 25.059063] mmc0: sdhci: Cmd: 0x0000123a | Max curr: 0x00000000 [Thu Jun 13 17:58:43.816 2024] [ 25.059067] mmc0: sdhci: Resp[0]: 0x00000900 | Resp[1]: 0xffffffff [Thu Jun 13 17:58:43.816 2024] [ 25.059071] mmc0: sdhci: Resp[2]: 0x328f5903 | Resp[3]: 0x00000900 [Thu Jun 13 17:58:43.832 2024] [ 25.059074] mmc0: sdhci: Host ctl2: 0x0000000b [Thu Jun 13 17:58:43.832 2024] [ 25.059077] mmc0: sdhci: ADMA Err: 0x00000000 | ADMA Ptr: 0x0000000081320218 [Thu Jun 13 17:58:43.832 2024] [ 25.059082] mmc0: sdhci: ============================================
2. we see one post
we also have the same issue in HS200, on our some devices happen occasionally
* mmc0 read/write test fails in linux due to a blk_account_io_completion kernel page request fault.
* mmc0 read/write io error, triggering a "mmc0: running CQE recovery" message repeated agnosium.
But in that post SDK 9.1 and SDK 9.2 still have emmc problem, it not be fix.