This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sample Qt application is not running on TI/J4 EVM



Hi,

     I was tried to run sample Qt application [ from EZSDK 5.02 Release ]  on TI/J4 EVM but it's not run. It's thrown an error as 

$ ./basiclayouts -qws

Error opening framebuffer device /dev/fb0
QScreenLinuxFb::connect: No such file or directory
Error opening framebuffer device /dev/fb0
QScreenLinuxFb::connect: No such file or directory
Error opening framebuffer device /dev/fb0

....... it thrown an error continously

 

The steps which i used to compile Qt application in host for TI/J4

Step 1:  $ source $(SDK_HOME)/linux-devkit/environment-setup
               ( SDK_HOME = /u/users/Gowtham/ezsdk_57/)

After above statement bash prompt got changed

               [linux-devkit]:/u/users/Gowtham/ezsdk_57/

Step 2:  [linux-devkit]:  cd  /u/users/Gowtham/ezsdk_57/linux-devkit/arm-none-linux-gnueabi/usr/bin/qtopia/examples/layouts/basiclayouts

Step 3: [linux-devkit]: qmake basiclayouts.pro

Step 4: [linux-devkit]: make


After compilation, i copied "basiclayouts" binary into /users/gowtham/ in target path

I exported Qt libraries path before launch the application

$ export LD_LIBRARY_PATH=$LD_LIBRARY_PATH:/usr/local/Trolltech/qt-embedded-arm/lib

$ cd /users/gowtham/

$ ./basiclayouts -qws

 Error opening framebuffer device /dev/fb0
 QScreenLinuxFb::connect: No such file or directory
Error opening framebuffer device /dev/fb0
 QScreenLinuxFb::connect: No such file or directory
Error opening framebuffer device /dev/fb0
 QScreenLinuxFb::connect: No such file or directory
Error opening framebuffer device /dev/fb0
 QScreenLinuxFb::connect: No such file or directory
Error opening framebuffer device /dev/fb0
 QScreenLinuxFb::connect: No such file or directory
.....

Please help me to solve this issue.

Regards,
Gowthaman.P