Other Parts Discussed in Thread: AM1808, OMAP-L138, OMAPL138
I found that there is no screen show on the LCD upon power up (Switch 7 all in off position, WinCE SD card plugged in, as suggested by quick-start-guide). There is no serial port message coming out (set to correct baud rate already).
I think the board is totally blank, so I proceed to build WinCE OS and Eboot. But I failed to flash it into the board as suggested in the quick start guide (as attached, pg 6). When I execute “C:\TI\BSP_WINCE_ARM9_01_10_00\Demo TI_Default\AM1808>sfh_OMAP-L138.exe -erase -p
COM1“ I see message below:
TI Serial Flasher Host Program for OMAP-L138
(C) 2010, Texas Instruments, Inc.
Ver. 1.67
-----------------------------------------------------
[TYPE] Global erase
[TARGET] OMAPL138
[DEVICE] SPI_MEM
Attempting to connect to device COM1...
Press any key to end this program at any time.
(AIS Parse): Read magic word 0x41504954.
(AIS Parse): Waiting for BOOTME... (power on or reset target now)
(Serial Port): Read error! (The operation has timed out.)
(Serial Port): Read error! (The operation has timed out.)
Aborting program...
(Serial Port): Read error! (Thread was being aborted.)
Since I cannot flash the bootloader, I cannot proceed to download the OS and run the Demo. Do you have any idea what is going on? is there any steps I need to do before using it?
this is totally a new eval kit.
please help. thanks.