Other Parts Discussed in Thread: MIDAS, OMAP3530, SYSBIOS
Hi
I need to know the basic difference between MIDAS 2.0 and MIDAS 3.0.
When I just skimmed through the MIDAS2.0 and MIDAS 3.0 wiki pages, I understood that significant performance improvement is obtained by introducing a separate multicore DSP is introduced in MIDAS 3.0. I saw the functional blocks are same in both MIDAS 2.0 and MIDAS 3.0 except that only Scan conversion unit is implemented on OMAP3530 SOC and rest of the blocks implemented on multicore DSP in MIDAS3.0 and all the processing blocks are solely done on OMAP3530 SOC in MIDAS 2.0. Also in MIDAS3.0 wiki, I saw "The algorithm source code for BPU, DPU and SCU ultrasound processing modules will be made available soon. ".
I need to know if any additional feature improvement other than performance improvement is implemented in MIDAS 3.0 compared to MIDAS 2.0? I need to start MIDAS for an internal study purpose. For a newbie like me, which can be a better starting point - MIDAS 2.0 or MIDAS 3.0.
Thanks,
Honey S
Software Engineeer