Tool/software:
I need to define three CIO devices (using add_device), and by default there are three available (according to _NDEVICE in file.h).
Since there is a default host device added, I can not use all three but only two.
My question:
- is there a way to disable the default host device (which I assume is used for profiling, which I do not need anyways) or
- can I remove this existing device or
- can I increase the number of devices (besides patching file.h).