Part Number: SK-AM69
Tool/software:
Hi Experts,
I want to use a custom model in TensorflowLite with SK-AM69.
compile_options = {
'tidl_tools_path' : os.environ['TIDL_TOOLS_PATH'],
'artifacts_folder' : output_dir,
'tensor_bits' : num_bits,
'accuracy_level' : accuracy,
'debug_level' : 1,
'deny_list' : "1",
}
I compiled own tflite model, but it didn't generate allowedNode.txt after running. Could you please help me?
The following files are generated and I can do inference on ARM, but I can't use DSP.
149_tidl_io_1.bin
149_tidl_net.bin.layer_info.txt
149_tidl_net.bin_netLog.txt
149_tidl_net.bin
149_tidl_net.bin.svg
graphvizInfo.txt
*Environment
SK-AM69
SD boot (tisdk-edgeai-image-j784s4-evm.wic.xz)
Version: 09.02.00.05
----------------Inference log--------------------------------------------------
root@am69a-sk:~/tflite-test# python3 infer-test.py
******** WARNING ******* : Could not open /home/root/tflite-test/resnet//allowedNode.txt for reading... Entire model will run on ARM without any delegation to TIDL !
Number of subgraphs:1 , 0 nodes delegated out of 66 nodes
INFO: Created TensorFlow Lite XNNPACK delegate for CPU.
(680, 416)
infer time: 0.3435549736022949
{'ts:run_start': 15496595226687, 'ts:run_end': 15496938064560, 'ddr:read_start': 0, 'ddr:read_end': 18446744073709551615, 'ddr:write_start': 0, 'ddr:write_end': 0}
Best regards,
Rei