This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REGARDING GSTREAMER SUPPORT ON DM6446



Hi ,

I have some questions on ti gstreamer, we are working with the DM6446(DVSDK 2.2V, linux.2.18, DMAI.1.27) .

As for the study of gstreamer we tried all the commands on the host PC and run success . in the same way we downloaded gstreamer source code from the ti web site and done for our board also.

but some of that command are not working on our custom board.we noticed that that plugins are not installed.so,we are trying to download them and install forther.

Here i have some questions like:-

(i)  can i download the files like above i said and install or not ? if yes please suggest some web address from where to download them.

(ii) We have any programming books using gstreamer to create UI on the TV screen?

please let us know this information,

 

 

 

 

 

thanks and regards ,

Y.V.RAMAKRISHNA.