This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] : How to trigger DMA with the help of GPIO on AM64X/AM243 and AM62X devices ?

Part Number: AM6412


Tool/software:

Hello Users,

Many users are asking to trigger DMA with the help of GPIO on AM64X/AM243 and AM62X devices.

So, I have created an example of this solution on AM64X and the procedure is the same for all other devices.

  • In this example, I have taken the source address is PSRAM memory location and the destination memory is DDR.

    So, here users can  use source and destination memory as per user requirements and memory addresses may be MSRAM / DDR /OSPI or any other memory.

    Our devices can generate an DMA event from GPIO in both  input or output modes .

    The attached example below , I have used GPIO as an output and generating DMA event for every 1sec.

  • First go to the chapter below from TRM .

    And, to trigger DMA from GPIO we need to follow the procedure below.

    GPIO (Input/ Output) → RISING EDGE/ FALLING EDGE/ BOTH EDGES → GPIO MUX ROUTER → L2G (Local to Global Event) → DMSS / PDMA → IA → Destination core.

  • Steps : 

    1. Configuring GPIO Mux Router : 

     All GPIO interrupts should be routed to  GPIO Mux router on AM64X.

    As per AM64X, to trigger DMA,  on SOC total 10 router outputs are assigned.

    Those are from 16 to 17 and 30 to 37 Router outputs are used to trigger DMA.

    Please look at the image below .

    So, users can allocate any router output and there are no issues.

    In the current example, I need only one router output for triggering DMA .So, I have chosen to 16th Router output  and this router output should be configured in the sciclient_defaultBoardcfg_rm.file since currently, in the software, these routers are not configured.

    So, I have updated only the GPIO-16 router in the sciclient_defaultBoardcfg_rm.c file.

    Folder Path: C:timcu_plus_sdk_xx/source/drivers/sciclient/sciclient_default_boardcfgam64x_am243x

    To update sciclient_defaultBoardcfg_rm.c file , please follow the procedure from the link below  .

    https://software-dl.ti.com/mcu-plus-sdk/esd/AM64X/latest/exports/docs/api_guide_am64x/RESOURCE_ALLOCATION_GUIDE.html

    The sciclient_defaultBoardcfg_rm.c file is belongs to sysfw .So, user need to compile sciclient_defaultBoardcfg_rm.c file and after compilation it and sysfw should be flashed on SOC  .

    So, user should follow steps below .

    a. Compile the sciclient_defaultBoardcfg_rm.c file.

    b. Compile SBL and Flash SBL with updated board config file 

    2. As I mentioned above,  with the GPIO from either input or output configuration user can trigger DMA . In the attached example ,

    I have choosen GPIO1_44 pin as output .

    3. In the above steps , GPIO event  is routed to a GPIO MUX router and now we need to convert this local event to global event .

    As per AM64X, the Global events started from 50176 and local events should be converted to the form of 50176+X.

    https://software-dl.ti.com/tisci/esd/latest/5_soc_doc/am64x/interrupt_cfg.html#main-gpiomux-introuter0-interrupt-router-output-destinations

    Already in UDMA  driver there is an API to convert a global event from local event , so users can just send the local event number.

    4. Next, triggering DMA, here users need to configure below  settings based on user requirements.

    For example, users need to transfer from source to destination memory for less than 64KB then 

    If the data size is <  64KB, then  

    ICNT 0 = length and the trigger type is 

    pTr->flags |= CSL_FMK(UDMAP_TR_FLAGS_TRIGGER0, CSL_UDMAP_TR_FLAGS_TRIGGER_GLOBAL0);
    pTr->flags |= CSL_FMK(UDMAP_TR_FLAGS_TRIGGER0_TYPE, CSL_UDMAP_TR_FLAGS_TRIGGER_TYPE_ICNT1_DEC);

    If the data size is > 64KB, then  

    ICNT 0 and ICNT 1 should be configured accordingly to user length and the chosen trigger type is as below.

    pTr->flags |= CSL_FMK(UDMAP_TR_FLAGS_TRIGGER0, CSL_UDMAP_TR_FLAGS_TRIGGER_GLOBAL0);

    pTr->flags |= CSL_FMK(UDMAP_TR_FLAGS_TRIGGER0_TYPE, CSL_UDMAP_TR_FLAGS_TRIGGER_TYPE_ICNT2_DEC);

  • Example Code : 

    5023.gpmc_psram_io_am64x-evm_r5fss0-0_nortos_ti-arm-clang.zip

    /*
     * K3 System Firmware Resource Management Configuration Data
     * Auto generated from K3 Resource Partitioning tool
     *
     * Copyright (c) 2018-2023, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    /**
     *  \file sciclient_defaultBoardcfg_rm.c
     *
     *  \brief File containing the rm boardcfg default data structure to
     *      send TISCI_MSG_BOARD_CONFIG_RM message.
     *
     */
    /* ========================================================================== */
    /*                             Include Files                                  */
    /* ========================================================================== */
    
    #include <drivers/sciclient.h>
    #include <drivers/sciclient/include/tisci/am64x_am243x/tisci_hosts.h>
    #include <drivers/sciclient/include/tisci/am64x_am243x/tisci_boardcfg_constraints.h>
    #include <drivers/sciclient/include/tisci/am64x_am243x/tisci_devices.h>
    
    /* ========================================================================== */
    /*                            Global Variables                                */
    /* ========================================================================== */
    
    /* \brief Structure to hold the RM board configuration */
    struct tisci_local_rm_boardcfg {
        struct tisci_boardcfg_rm      rm_boardcfg;
        /**< Board configuration parameter */
        struct tisci_boardcfg_rm_resasg_entry resasg_entries[TISCI_RESASG_ENTRIES_MAX];
        /**< Resource assignment entries */
    };
    
    const struct tisci_local_rm_boardcfg gBoardConfigLow_rm
    __attribute__(( aligned(128), section(".boardcfg_data") )) =
    {
        .rm_boardcfg = {
            .rev = {
                .tisci_boardcfg_abi_maj = TISCI_BOARDCFG_RM_ABI_MAJ_VALUE,
                .tisci_boardcfg_abi_min = TISCI_BOARDCFG_RM_ABI_MIN_VALUE,
            },
            .host_cfg = {
                .subhdr = {
                    .magic = TISCI_BOARDCFG_RM_HOST_CFG_MAGIC_NUM,
                    .size = (uint16_t) sizeof(struct tisci_boardcfg_rm_host_cfg),
                },
                .host_cfg_entries = {
                    {
                        .host_id = TISCI_HOST_ID_A53_2,
                        .allowed_atype = 0b101010,
                        .allowed_qos   = 0xAAAA,
                        .allowed_orderid = 0xAAAAAAAA,
                        .allowed_priority = 0xAAAA,
                        .allowed_sched_priority = 0xAA
                    },
                    {
                        .host_id = TISCI_HOST_ID_M4_0,
                        .allowed_atype = 0b101010,
                        .allowed_qos   = 0xAAAA,
                        .allowed_orderid = 0xAAAAAAAA,
                        .allowed_priority = 0xAAAA,
                        .allowed_sched_priority = 0xAA
                    },
                    {
                        .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
                        .allowed_atype = 0b101010,
                        .allowed_qos   = 0xAAAA,
                        .allowed_orderid = 0xAAAAAAAA,
                        .allowed_priority = 0xAAAA,
                        .allowed_sched_priority = 0xAA
                    },
                    {
                        .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
                        .allowed_atype = 0b101010,
                        .allowed_qos   = 0xAAAA,
                        .allowed_orderid = 0xAAAAAAAA,
                        .allowed_priority = 0xAAAA,
                        .allowed_sched_priority = 0xAA
                    },
                    {
                        .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
                        .allowed_atype = 0b101010,
                        .allowed_qos   = 0xAAAA,
                        .allowed_orderid = 0xAAAAAAAA,
                        .allowed_priority = 0xAAAA,
                        .allowed_sched_priority = 0xAA
                    },
                    {
                        .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
                        .allowed_atype = 0b101010,
                        .allowed_qos   = 0xAAAA,
                        .allowed_orderid = 0xAAAAAAAA,
                        .allowed_priority = 0xAAAA,
                        .allowed_sched_priority = 0xAA
                    },
                },
            },
            .resasg = {
                .subhdr = {
                    .magic = TISCI_BOARDCFG_RM_RESASG_MAGIC_NUM,
                    .size = (uint16_t) sizeof(struct tisci_boardcfg_rm_resasg),
                },
                .resasg_entries_size = 182 * sizeof(struct tisci_boardcfg_rm_resasg_entry),
            },
        },
        .resasg_entries = {
            {
                .num_resource = 16,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_CMP_EVENT_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_CMP_EVENT_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 16,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_CMP_EVENT_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 16,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_CMP_EVENT_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 20,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_CMP_EVENT_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 24,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_CMP_EVENT_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 28,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_CMP_EVENT_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 32,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_MAIN_GPIOMUX_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_MAIN_GPIOMUX_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_MAIN_GPIOMUX_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 8,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_MAIN_GPIOMUX_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 12,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_MAIN_GPIOMUX_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 14,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_MAIN_GPIOMUX_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 16,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_MCU_MCU_GPIOMUX_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_MCU_MCU_GPIOMUX_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 4,
                .host_id = TISCI_HOST_ID_M4_0,
            },
            {
                .num_resource = 41,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_TIMESYNC_EVENT_INTROUTER0, TISCI_RESASG_SUBTYPE_IR_OUTPUT),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 136,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_GLOBAL_EVENT_TRIGGER),
                .start_resource = 50176,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_UDMAP_GLOBAL_CONFIG),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 12,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_BLOCK_COPY_CHAN),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_BLOCK_COPY_CHAN),
                .start_resource = 12,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_BLOCK_COPY_CHAN),
                .start_resource = 12,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_BLOCK_COPY_CHAN),
                .start_resource = 18,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_BLOCK_COPY_CHAN),
                .start_resource = 20,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_BLOCK_COPY_CHAN),
                .start_resource = 24,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_BLOCK_COPY_CHAN),
                .start_resource = 26,
                .host_id = TISCI_HOST_ID_M4_0,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_BLOCK_COPY_CHAN),
                .start_resource = 27,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_SPLIT_TR_RX_CHAN),
                .start_resource = 48,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_SPLIT_TR_RX_CHAN),
                .start_resource = 54,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_SPLIT_TR_RX_CHAN),
                .start_resource = 54,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_SPLIT_TR_RX_CHAN),
                .start_resource = 60,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_SPLIT_TR_RX_CHAN),
                .start_resource = 62,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_SPLIT_TR_RX_CHAN),
                .start_resource = 66,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_SPLIT_TR_TX_CHAN),
                .start_resource = 28,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_SPLIT_TR_TX_CHAN),
                .start_resource = 34,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_SPLIT_TR_TX_CHAN),
                .start_resource = 34,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_SPLIT_TR_TX_CHAN),
                .start_resource = 40,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_SPLIT_TR_TX_CHAN),
                .start_resource = 42,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_RING_SPLIT_TR_TX_CHAN),
                .start_resource = 46,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 12,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_BLOCK_COPY_CHAN),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_BLOCK_COPY_CHAN),
                .start_resource = 12,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_BLOCK_COPY_CHAN),
                .start_resource = 12,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_BLOCK_COPY_CHAN),
                .start_resource = 18,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_BLOCK_COPY_CHAN),
                .start_resource = 20,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_BLOCK_COPY_CHAN),
                .start_resource = 24,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_BLOCK_COPY_CHAN),
                .start_resource = 26,
                .host_id = TISCI_HOST_ID_M4_0,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_BLOCK_COPY_CHAN),
                .start_resource = 27,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_SPLIT_TR_RX_CHAN),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_SPLIT_TR_RX_CHAN),
                .start_resource = 6,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_SPLIT_TR_RX_CHAN),
                .start_resource = 6,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_SPLIT_TR_RX_CHAN),
                .start_resource = 12,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_SPLIT_TR_RX_CHAN),
                .start_resource = 14,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_SPLIT_TR_RX_CHAN),
                .start_resource = 18,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_SPLIT_TR_TX_CHAN),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_SPLIT_TR_TX_CHAN),
                .start_resource = 6,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 6,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_SPLIT_TR_TX_CHAN),
                .start_resource = 6,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_SPLIT_TR_TX_CHAN),
                .start_resource = 12,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_SPLIT_TR_TX_CHAN),
                .start_resource = 14,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_BCDMA_0, TISCI_RESASG_SUBTYPE_BCDMA_SPLIT_TR_TX_CHAN),
                .start_resource = 18,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 35,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_VINT),
                .start_resource = 5,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 14,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_VINT),
                .start_resource = 44,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 14,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_VINT),
                .start_resource = 44,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 14,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_VINT),
                .start_resource = 58,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 14,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_VINT),
                .start_resource = 92,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 14,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_VINT),
                .start_resource = 106,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 16,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_VINT),
                .start_resource = 168,
                .host_id = TISCI_HOST_ID_M4_0,
            },
            {
                .num_resource = 512,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_GLOBAL_EVENT_SEVT),
                .start_resource = 16,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 256,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_GLOBAL_EVENT_SEVT),
                .start_resource = 528,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 256,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_GLOBAL_EVENT_SEVT),
                .start_resource = 528,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 192,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_GLOBAL_EVENT_SEVT),
                .start_resource = 784,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 256,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_GLOBAL_EVENT_SEVT),
                .start_resource = 976,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 192,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_GLOBAL_EVENT_SEVT),
                .start_resource = 1232,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 96,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_GLOBAL_EVENT_SEVT),
                .start_resource = 1424,
                .host_id = TISCI_HOST_ID_M4_0,
            },
            {
                .num_resource = 16,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_GLOBAL_EVENT_SEVT),
                .start_resource = 1520,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 1024,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_TIMERMGR_EVT_OES),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 42,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_PKTDMA_TX_CHAN_ERROR_OES),
                .start_resource = 4096,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 112,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_PKTDMA_TX_FLOW_COMPLETION_OES),
                .start_resource = 4608,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 29,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_PKTDMA_RX_CHAN_ERROR_OES),
                .start_resource = 5120,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 176,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_PKTDMA_RX_FLOW_COMPLETION_OES),
                .start_resource = 5632,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 176,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_PKTDMA_RX_FLOW_STARVATION_OES),
                .start_resource = 6144,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 176,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_PKTDMA_RX_FLOW_FIREWALL_OES),
                .start_resource = 6656,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 28,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_BCDMA_CHAN_ERROR_OES),
                .start_resource = 8192,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 28,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_BCDMA_CHAN_DATA_COMPLETION_OES),
                .start_resource = 8704,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 28,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_BCDMA_CHAN_RING_COMPLETION_OES),
                .start_resource = 9216,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 20,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_BCDMA_TX_CHAN_ERROR_OES),
                .start_resource = 9728,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 20,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_BCDMA_TX_CHAN_DATA_COMPLETION_OES),
                .start_resource = 10240,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 20,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_BCDMA_TX_CHAN_RING_COMPLETION_OES),
                .start_resource = 10752,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 20,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_BCDMA_RX_CHAN_ERROR_OES),
                .start_resource = 11264,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 20,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_BCDMA_RX_CHAN_DATA_COMPLETION_OES),
                .start_resource = 11776,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 20,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_INTAGGR_0, TISCI_RESASG_SUBTYPE_IA_BCDMA_RX_CHAN_RING_COMPLETION_OES),
                .start_resource = 12288,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_UDMAP_GLOBAL_CONFIG),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_UNMAPPED_TX_CHAN),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 3,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_UNMAPPED_TX_CHAN),
                .start_resource = 4,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 3,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_UNMAPPED_TX_CHAN),
                .start_resource = 4,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_UNMAPPED_TX_CHAN),
                .start_resource = 7,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_UNMAPPED_TX_CHAN),
                .start_resource = 9,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_UNMAPPED_TX_CHAN),
                .start_resource = 13,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_UNMAPPED_TX_CHAN),
                .start_resource = 15,
                .host_id = TISCI_HOST_ID_M4_0,
            },
            {
                .num_resource = 64,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_CPSW_TX_CHAN),
                .start_resource = 16,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 64,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_CPSW_TX_CHAN),
                .start_resource = 16,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_SAUL_TX_1_CHAN),
                .start_resource = 88,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_SAUL_TX_1_CHAN),
                .start_resource = 88,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_ICSSG_0_TX_CHAN),
                .start_resource = 96,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_ICSSG_0_TX_CHAN),
                .start_resource = 96,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_ICSSG_1_TX_CHAN),
                .start_resource = 104,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_ICSSG_1_TX_CHAN),
                .start_resource = 104,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_UNMAPPED_RX_CHAN),
                .start_resource = 112,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 3,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_UNMAPPED_RX_CHAN),
                .start_resource = 116,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 3,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_UNMAPPED_RX_CHAN),
                .start_resource = 116,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_UNMAPPED_RX_CHAN),
                .start_resource = 119,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_UNMAPPED_RX_CHAN),
                .start_resource = 121,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_UNMAPPED_RX_CHAN),
                .start_resource = 125,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_UNMAPPED_RX_CHAN),
                .start_resource = 127,
                .host_id = TISCI_HOST_ID_M4_0,
            },
            {
                .num_resource = 16,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_CPSW_RX_CHAN),
                .start_resource = 128,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 16,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_CPSW_RX_CHAN),
                .start_resource = 128,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_SAUL_RX_1_CHAN),
                .start_resource = 144,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_SAUL_RX_2_CHAN),
                .start_resource = 152,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_SAUL_RX_2_CHAN),
                .start_resource = 152,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_SAUL_RX_3_CHAN),
                .start_resource = 152,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_SAUL_RX_3_CHAN),
                .start_resource = 152,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 64,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_ICSSG_0_RX_CHAN),
                .start_resource = 160,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 64,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_ICSSG_0_RX_CHAN),
                .start_resource = 160,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 64,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_ICSSG_1_RX_CHAN),
                .start_resource = 224,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 64,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_RING_ICSSG_1_RX_CHAN),
                .start_resource = 224,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_UNMAPPED_TX_CHAN),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 3,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_UNMAPPED_TX_CHAN),
                .start_resource = 4,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 3,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_UNMAPPED_TX_CHAN),
                .start_resource = 4,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_UNMAPPED_TX_CHAN),
                .start_resource = 7,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_UNMAPPED_TX_CHAN),
                .start_resource = 9,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_UNMAPPED_TX_CHAN),
                .start_resource = 13,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_UNMAPPED_TX_CHAN),
                .start_resource = 15,
                .host_id = TISCI_HOST_ID_M4_0,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_CPSW_TX_CHAN),
                .start_resource = 16,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_CPSW_TX_CHAN),
                .start_resource = 16,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_SAUL_TX_1_CHAN),
                .start_resource = 25,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_SAUL_TX_1_CHAN),
                .start_resource = 25,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_ICSSG_0_TX_CHAN),
                .start_resource = 26,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_ICSSG_0_TX_CHAN),
                .start_resource = 26,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_ICSSG_1_TX_CHAN),
                .start_resource = 34,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_ICSSG_1_TX_CHAN),
                .start_resource = 34,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_UNMAPPED_RX_CHAN),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 3,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_UNMAPPED_RX_CHAN),
                .start_resource = 4,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 3,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_UNMAPPED_RX_CHAN),
                .start_resource = 4,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_UNMAPPED_RX_CHAN),
                .start_resource = 7,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_UNMAPPED_RX_CHAN),
                .start_resource = 9,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_UNMAPPED_RX_CHAN),
                .start_resource = 13,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_UNMAPPED_RX_CHAN),
                .start_resource = 15,
                .host_id = TISCI_HOST_ID_M4_0,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_UNMAPPED_RX_CHAN),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 3,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_UNMAPPED_RX_CHAN),
                .start_resource = 4,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 3,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_UNMAPPED_RX_CHAN),
                .start_resource = 4,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_UNMAPPED_RX_CHAN),
                .start_resource = 7,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_UNMAPPED_RX_CHAN),
                .start_resource = 9,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_UNMAPPED_RX_CHAN),
                .start_resource = 13,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_UNMAPPED_RX_CHAN),
                .start_resource = 15,
                .host_id = TISCI_HOST_ID_M4_0,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_CPSW_RX_CHAN),
                .start_resource = 16,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_CPSW_RX_CHAN),
                .start_resource = 16,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 16,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_CPSW_RX_CHAN),
                .start_resource = 16,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 16,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_CPSW_RX_CHAN),
                .start_resource = 16,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_SAUL_RX_0_CHAN),
                .start_resource = 32,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_SAUL_RX_1_CHAN),
                .start_resource = 32,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_SAUL_RX_2_CHAN),
                .start_resource = 19,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_SAUL_RX_2_CHAN),
                .start_resource = 19,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_SAUL_RX_2_CHAN),
                .start_resource = 40,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_SAUL_RX_2_CHAN),
                .start_resource = 40,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_SAUL_RX_3_CHAN),
                .start_resource = 20,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_SAUL_RX_3_CHAN),
                .start_resource = 20,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_SAUL_RX_3_CHAN),
                .start_resource = 40,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 8,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_SAUL_RX_3_CHAN),
                .start_resource = 40,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_ICSSG_0_RX_CHAN),
                .start_resource = 21,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_ICSSG_0_RX_CHAN),
                .start_resource = 21,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 64,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_ICSSG_0_RX_CHAN),
                .start_resource = 48,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 64,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_ICSSG_0_RX_CHAN),
                .start_resource = 48,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_ICSSG_1_RX_CHAN),
                .start_resource = 25,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_ICSSG_1_RX_CHAN),
                .start_resource = 25,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 64,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_ICSSG_1_RX_CHAN),
                .start_resource = 112,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 64,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_PKTDMA_0, TISCI_RESASG_SUBTYPE_PKTDMA_FLOW_ICSSG_1_RX_CHAN),
                .start_resource = 112,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 1,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_RINGACC_0, TISCI_RESASG_SUBTYPE_RA_ERROR_OES),
                .start_resource = 0,
                .host_id = TISCI_HOST_ID_ALL,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_RINGACC_0, TISCI_RESASG_SUBTYPE_RA_VIRTID),
                .start_resource = 2,
                .host_id = TISCI_HOST_ID_A53_2,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_RINGACC_0, TISCI_RESASG_SUBTYPE_RA_GENERIC_IPC),
                .start_resource = 20,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_0,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_RINGACC_0, TISCI_RESASG_SUBTYPE_RA_GENERIC_IPC),
                .start_resource = 20,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_RINGACC_0, TISCI_RESASG_SUBTYPE_RA_GENERIC_IPC),
                .start_resource = 22,
                .host_id = TISCI_HOST_ID_MAIN_0_R5_3,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_RINGACC_0, TISCI_RESASG_SUBTYPE_RA_GENERIC_IPC),
                .start_resource = 24,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_1,
            },
            {
                .num_resource = 2,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_RINGACC_0, TISCI_RESASG_SUBTYPE_RA_GENERIC_IPC),
                .start_resource = 26,
                .host_id = TISCI_HOST_ID_MAIN_1_R5_3,
            },
            {
                .num_resource = 4,
                .type = TISCI_RESASG_UTYPE (TISCI_DEV_DMASS0_RINGACC_0, TISCI_RESASG_SUBTYPE_RA_GENERIC_IPC),
                .start_resource = 28,
                .host_id = TISCI_HOST_ID_ALL,
            },
        }
    };
    
    

    If users still need help on this topic please raise new threads .

    I have verified the basic functionality and not checked in all other Testcases .

    Please do Testing  while integrating these changes in your application .

  • As per TRM, routing GPIO interrupt to L2G is Level Type.

    For the level type, we need to set 1 in the L2G Register, but in the above example, I set the pulse type and configured to zero.

    Please change the API definition in the example with the change below.


    static void configure_intaggrL2G(uint32_t localEvent, uint32_t globalEvent)
    {
        uint64_t eventRegOffset = CSL_DMASS0_INTAGGR_L2G_BASE + (localEvent * 0x20U);
        CSL_REG64_WR(eventRegOffset, ( (1U << 31U) | (globalEvent & 0xFFFFU) ) ); /* Level event */
    }