This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM69: Can CSI support 4K 60fps YUV422 input

Part Number: AM69
Other Parts Discussed in Thread: TDA4VH,

Tool/software:

4K 60fps YUV422 data rate should be: 24-bit, 4K UHD @ 60 fps: 16bit × 3840 × 2160 × 60 = 8 Gbit/s.

One Lane data rate is 2.5Gbps,4 lane is 10Gbps. 

Is there over head of CSI interface? If yes, what is ratio?

Can AM69/TDA4VH system capability supports 2-ch 4K 60fps YUV422 input to do video encoding, then store it.