Hi, i am a Student of Electrical engineering and i m working on a project which involves harmonic analysis of current (50 Hz fundamental). Can anyone suggest me a cheap DSP processor for this purpose.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, i am a Student of Electrical engineering and i m working on a project which involves harmonic analysis of current (50 Hz fundamental). Can anyone suggest me a cheap DSP processor for this purpose.
Does the board need to interface to something? How will you get data in and out of the board? Or is this more of a simulation where you'll just define a test vector in memory and then process it?
we will be giving the inputs directly to ADC (in built ADC in the chip) via current sensor.
How many bits of resolution do you want/need in the ADC? What's the voltage range of the signal you're measuring? At what speed do you want/need to sample?
There's also question about what other peripherals you might need: USB, UART, SPI, I2C, etc.
How much memory do you need? Do you need to do floating point arithmetic or fixed point arithmetic? Any guess of how many MIPS/MHz? Do you have a cost target?
These are the things that need to be known in order to choose the right processor. Otherwise you'll likely end up with a processor that doesn't get the job done.
10 to 12 bits will be sufficient, the out put of the current sensor will be 5V (max), as i m working with 50 Hz fundamental so any reasonable sampling frequency will be okay.
at least one UART must be there as i am continuously displaying the harmonics (average of the samples within 0.5 second or so).
i need to implement FFT code on the input waveform using Fixed Point (Q number format), i don't know how much memory i will need. can you help me out here.
and thank you very much for your replies.
I think something like our F28335 eZdsp would be a good fit:
http://www.ti.com/tool/tmdsez28335
Our c2000 family of processors is geared toward things like motor control, digital power supplies, etc. There are libraries available for fixed FFTs and various control algorithms.
If you have follow-on questions related to this processor please start a new post in the c2000 forum. Please click "verify answer" on this post if this looks like a good fit for your application.
Best regards,
Brad
hey brad, that's great help
thank you so much for your responses. i read the datasheet and it is quite good for our purposes. i want to buy this processor (only processor, not the whole target board), so how can i buy it and how much it will cost? also how do i program it. is there a specific programmer?
gaurav
This info can be found in the product folder here:
http://www.ti.com/product/tms320f28335#pricingpackaging
Just click the "Sample or Buy" button. Make sure you choose the appropriate package. It looks like there's inventory available at multiple distributors.
Brad
Hello TI,
I have a question regarding TMS320F28335.
Context: Connecting 256kX16 SRAM to TMS320F28335.
Problem: There are two external write enable pins in TMS320F28335, XWE0 (pin137) and XWE1 (pin 151). I am confused in connecting them to an external SRAM as there is only one write enable pin in the SRAM.
Looking forward to your positive reply..