This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM64X: Bug in setup script for version 09.02.01.10 (solved)

Part Number: PROCESSOR-SDK-AM64X

Tool/software:

Hello,

there has been found an issue in the build process of the SDK, which could be traced back to

an error in bin/setup-targetfs-nfs.sh. I just wanna share that here, as others might be affected as well.

Thanks for Viktor Gotwig for locating the problem in the end!

When executing make linux_install normally, it is failing with the following error messages:

=======================================
Installing the Linux Kernel DTBs
=======================================
The extracted target filesystem directory doesn't exist.
Please run setup.sh in the SDK's root directory and then try again.
make: *** [makerules/Makefile_linux-dtbs:24: linux-dtbs_install] Error 1

Re-running setup.sh does not solve that problem, of course.

Apparently, the variable DESTDIR is not set up properly.

One work-around is to explicitely specify DESTDIR while calling make. I.e. by executing

DESTDIR=<Path to the SDK>/targetNFS make linux_install

The actual issue is in one of the setup scripts where some makefiles are being

created/edited - in particular bin/setup-targetfs-nfs.sh

There, in lines 153 and 156 are two calls of sed dealing with EXEC_DIR and DESTDIR.

In both cases these variables are trailed with a space (totally four times - at each occurence of

EXEC_DIR and DESTDIR), which is causing the troubles. Here is also a patch that is fixing the issue:

--- bin/setup-targetfs-nfs.sh    2024-06-20 16:14:54.505952679 +0000
+++ bin/setup-targetfs-nfs.new.sh    2024-06-20 16:16:27.710321122 +0000
@@ -150,10 +150,10 @@
 echo
 read -p "Press return to continue" REPLY
 
-sed -i "s=EXEC_DIR ?\=.*$=EXEC_DIR ?\=$dst/home/root/$platform=g" $cwd/../Rules.make
+sed -i "s=EXEC_DIR?\=.*$=EXEC_DIR?\=$dst/home/root/$platform=g" $cwd/../Rules.make
 check_status
 
-sed -i "s=DESTDIR ?\=.*$=DESTDIR ?\=$dst=g" $cwd/../Rules.make
+sed -i "s=DESTDIR?\=.*$=DESTDIR?\=$dst=g" $cwd/../Rules.make
 check_status
 
 echo "Rules.make edited successfully..

Mario