Part Number: TDA4VE-Q1
Tool/software:
Dear Sir,
I am working on OD single camera pipeline.
OS: RTOS+QNX
SDK : 9.2 (J721S2)
I am facing the below error;
Grapy verify SUCCESS! App Verify Graph Done! 1235.196788 s: ISS: Starting sensor [ISX016-UB913A_Q1] ... !!! [MCU2_0] 1235.452851 s: Error writing 0x1 to UB960 register 0x4c [MCU2_0] 1235.452906 s: UB960 Error: Reg Write Failed for regAddr 4c, cnt = 0 1235.494816 s: ISS: Starting sensor [ISX016-UB913A_Q1] ... Done !!! ========================================== Mando TIDL Demo - Camera and Testdata based Object Detection ========================================== p: Print performance statistics e: Export performance statistics 0: Show Object Detection Output 1: Show LDC Output x: Exit [MCU2_0] 1235.495190 s: VX_ZONE_ERROR:[tivxCaptureDequeueFrameFromDriver:885] CAPTURE: ERROR: Incomplete Frame for Ch0 !!!
What could be the possible reason of this, as the application freezes on display just after running.
Thanks and Regards,
Vyom Mishra