Part Number: OMAP-L138
Tool/software:
Hello,
I need to build DSPLINK module for L138 and toolchain specifies for Code Gen Tools version 6.1.15. Is there a link available to download the software?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OMAP-L138
Tool/software:
Hello,
I need to build DSPLINK module for L138 and toolchain specifies for Code Gen Tools version 6.1.15. Is there a link available to download the software?
I need to build DSPLINK module for L138 and toolchain specifies for Code Gen Tools version 6.1.15.
I can see the earliest version available for download being 7.3.0. Have you tried using this one, and see if you can build the DSPLINK module successfully?
https://www.ti.com/tool/download/C6000-CGT/7.3.0
Actually when I look at the OMAP-L138 SDK release note document, it references an even "newer" version of 7.3.1.
Where do you see 6.1.15 is required?
Regards, Andreas
Hi Yang,
where did you get the rest of the SDK? It is not on ti.com is it?
its build environment is limited to to 6.1.15.
I found this on an internal archive. Do you need the toolchain for Windows or Linux?
Regards, Andreas