Other Parts Discussed in Thread: TMS320C6455
Hello
I'm using a DSK6455 with 1 GHz CPU clock. I need to generate an integer frecuency for McBSP. In spru580, I read that I can use "internal clock source" for the "sample rate generator". The internal clock source is fCPU / 6. In sprs276 (PLL1 controller, page 135) there is an example with 1GHz of CPU clock and it is written that SYSCLK3 (/6) is 200 MHz.
I'm a little confused: how is the rounding in that divider?, and how is the rounding in the FPER and CLKGDV dividers of McBSP?
Best regards.