This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J784S4XEVM: Image flash in J784S4XEVM using Uniflash failing ! or Partial success sometimes

Part Number: J784S4XEVM
Other Parts Discussed in Thread: UNIFLASH

Tool/software:

For more details and examples, please refer to the UniFlash Quick Start guide.


----------------------------------------------------------------------------
ProcessorSDKSerialFlash CLI Tool
Copyright (C) 2017-2023 Texas Instruments Incorporated - http://www.ti.com/
Version 1.10.0.0
----------------------------------------------------------------------------
Downloading Flash Programmer..

Transferring File of size 386145 bytes
49% complete
Failure: Canceled by remote!!

Enabling System firmware transfer!!!
NAK: Transmit of header Failed