Part Number: AM620-Q1
Other Parts Discussed in Thread: AM620, DP83869
Tool/software:
If I enable eth1 in * uboot.dtsi, why can I not make it "active'?

How do I enable the second ethernet port? I'm assuming it's done using "k3-am62x-sk-common-u-boot.dtsi". I made a change here to see the above in u-boot shell but I think I'm missing some configuration info. Here's my "k3-am62x-sk-common-u-boot.dtsi" file:
// SPDX-License-Identifier: GPL-2.0
/*
* Common AM62x SK dts file for SPLs
* Copyright (C) 2021-2022 Texas Instruments Incorporated - https://www.ti.com/
*/
/ {
chosen {
stdout-path = "serial2:115200n8";
tick-timer = &timer1;
};
aliases {
mmc0 = &sdhci0;
mmc1 = &sdhci1;
};
memory@80000000 {
bootph-pre-ram;
};
};
&cbass_main{
bootph-pre-ram;
timer1: timer@2400000 {
clock-frequency = <25000000>;
bootph-pre-ram;
};
};
&dmss {
bootph-pre-ram;
};
&secure_proxy_main {
bootph-pre-ram;
};
&dmsc {
bootph-pre-ram;
k3_sysreset: sysreset-controller {
compatible = "ti,sci-sysreset";
bootph-pre-ram;
};
};
&k3_pds {
bootph-pre-ram;
};
&k3_clks {
bootph-pre-ram;
};
&k3_reset {
bootph-pre-ram;
};
&wkup_conf {
bootph-pre-ram;
};
&chipid {
bootph-pre-ram;
};
&main_pmx0 {
bootph-pre-ram;
};
&main_uart0 {
bootph-pre-ram;
};
&main_uart0_pins_default {
bootph-pre-ram;
};
&main_uart1 {
bootph-pre-ram;
};
&cbass_mcu {
bootph-pre-ram;
};
&cbass_wakeup {
bootph-pre-ram;
};
&mcu_pmx0 {
bootph-pre-ram;
};
&wkup_uart0 {
bootph-pre-ram;
};
&main_i2c0 {
bootph-pre-ram;
};
&main_i2c0_pins_default {
bootph-pre-ram;
};
&sdhci0 {
bootph-pre-ram;
};
&sdhci1 {
bootph-pre-ram;
};
&main_mmc1_pins_default {
bootph-pre-ram;
};
&usbss0 {
bootph-pre-ram;
};
&usb0 {
dr_mode = "peripheral";
/* Since role switching is not supported in U-Boot */
/delete-property/ extcon;
bootph-pre-ram;
};
&usbss1 {
bootph-pre-ram;
};
&usb1 {
bootph-pre-ram;
};
&main_usb1_pins_default {
bootph-pre-ram;
};
&cpsw3g {
reg = <0x0 0x8000000 0x0 0x200000>,
<0x0 0x43000200 0x0 0x8>;
reg-names = "cpsw_nuss", "mac_efuse";
/delete-property/ ranges;
/* This is WA because MDIO driver is not DM enabled */
pinctrl-0 = <&main_mdio1_pins_default &main_rgmii1_pins_default>;
bootph-pre-ram;
cpsw-phy-sel@04044 {
compatible = "ti,am64-phy-gmii-sel";
reg = <0x0 0x00104044 0x0 0x8>;
bootph-pre-ram;
};
};
//&cpsw_port2 {
// JM status = "disabled";
// bootph-pre-ram;
//};
&main_bcdma {
bootph-pre-ram;
reg = <0x00 0x485c0100 0x00 0x100>,
<0x00 0x4c000000 0x00 0x20000>,
<0x00 0x4a820000 0x00 0x20000>,
<0x00 0x4aa40000 0x00 0x20000>,
<0x00 0x4bc00000 0x00 0x100000>,
<0x00 0x48600000 0x00 0x8000>,
<0x00 0x484a4000 0x00 0x2000>,
<0x00 0x484c2000 0x00 0x2000>;
reg-names = "gcfg", "bchanrt", "rchanrt", "tchanrt",
"ringrt" , "cfg", "tchan", "rchan";
};
&main_pktdma {
bootph-pre-ram;
reg = <0x00 0x485c0000 0x00 0x100>,
<0x00 0x4a800000 0x00 0x20000>,
<0x00 0x4aa00000 0x00 0x20000>,
<0x00 0x4b800000 0x00 0x200000>,
<0x00 0x485e0000 0x00 0x10000>,
<0x00 0x484a0000 0x00 0x2000>,
<0x00 0x484c0000 0x00 0x2000>,
<0x00 0x48430000 0x00 0x1000>;
reg-names = "gcfg", "rchanrt", "tchanrt", "ringrt",
"cfg", "tchan", "rchan", "rflow";
};
&fss {
bootph-pre-ram;
};
&cpsw_port1 {
bootph-pre-ram;
};
// JM
&cpsw_port2 {
bootph-pre-ram;
};
// end
&main_rgmii1_pins_default {
bootph-pre-ram;
};
// JM
//&main_rgmii2_pins_default {
// bootph-pre-ram;
//};
// end
&main_mdio1_pins_default {
bootph-pre-ram;
};
&cpsw3g_phy0 {
bootph-pre-ram;
};
// JM
//&cpsw3g_phy1 {
// bootph-pre-ram;
//};
// end
&dmsc {
bootph-pre-ram;
k3_sysreset: sysreset-controller {
compatible = "ti,sci-sysreset";
bootph-pre-ram;
};
};
&main_gpio0 {
bootph-pre-ram;
};
&main_i2c1 {
bootph-pre-ram;
};
&main_i2c1_pins_default {
bootph-pre-ram;
};
&exp1 {
bootph-pre-ram;
};
&vdd_mmc1 {
bootph-pre-ram;
};
USB0 should be started by default, correct? We don't have a usbc device on USB0, just a standard USBA connection. Any changes required there in the file, as well?
Right now I get the following: