Tool/software:
How to solve this 'data abort'. With old FW (Uboot 2014) it works
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
How to solve this 'data abort'. With old FW (Uboot 2014) it works
I'm attaching u-boot JTAG debugging with T32 for your reference. where I used AM437x as an example, but the same flow is applicable to AM335x.
I think OpenOCD may work also, but I've not used it myself.
Best,
-Hong
/*
* Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
/dts-v1/;
#include "am33xx.dtsi"
#include <dt-bindings/interrupt-controller/irq.h>
/ {
model = "TI AM335x EVM";
compatible = "ti,am335x-evm", "ti,am33xx";
chosen {
stdout-path = &uart0;
tick-timer = &timer2;
};
cpus {
cpu@0 {
cpu0-supply = <&vdd1_reg>;
};
};
memory {
device_type = "memory";
reg = <0x80000000 0x10000000>; /* 256 MB */
};
vbat: fixedregulator@0 {
compatible = "regulator-fixed";
regulator-name = "vbat";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
regulator-boot-on;
};
lis3_reg: fixedregulator@1 {
compatible = "regulator-fixed";
regulator-name = "lis3_reg";
regulator-boot-on;
};
wlan_en_reg: fixedregulator@2 {
compatible = "regulator-fixed";
regulator-name = "wlan-en-regulator";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
/* WLAN_EN GPIO for this board - Bank1, pin16 */
gpio = <&gpio1 16 0>;
/* WLAN card specific delay */
startup-delay-us = <70000>;
enable-active-high;
};
matrix_keypad: matrix_keypad@0 {
compatible = "gpio-matrix-keypad";
debounce-delay-ms = <5>;
col-scan-delay-us = <2>;
row-gpios = <&gpio1 25 GPIO_ACTIVE_HIGH /* Bank1, pin25 */
&gpio1 26 GPIO_ACTIVE_HIGH /* Bank1, pin26 */
&gpio1 27 GPIO_ACTIVE_HIGH>; /* Bank1, pin27 */
col-gpios = <&gpio1 21 GPIO_ACTIVE_HIGH /* Bank1, pin21 */
&gpio1 22 GPIO_ACTIVE_HIGH>; /* Bank1, pin22 */
linux,keymap = <0x0000008b /* MENU */
0x0100009e /* BACK */
0x02000069 /* LEFT */
0x0001006a /* RIGHT */
0x0101001c /* ENTER */
0x0201006c>; /* DOWN */
};
gpio_keys: volume_keys@0 {
compatible = "gpio-keys";
autorepeat;
switch@9 {
label = "volume-up";
linux,code = <115>;
gpios = <&gpio0 2 GPIO_ACTIVE_LOW>;
gpio-key,wakeup;
};
switch@10 {
label = "volume-down";
linux,code = <114>;
gpios = <&gpio0 3 GPIO_ACTIVE_LOW>;
gpio-key,wakeup;
};
};
backlight {
compatible = "pwm-backlight";
pwms = <&ecap0 0 50000 0>;
brightness-levels = <0 51 53 56 62 75 101 152 255>;
default-brightness-level = <8>;
};
panel {
compatible = "ti,tilcdc,panel";
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&lcd_pins_s0>;
panel-info {
ac-bias = <255>;
ac-bias-intrpt = <0>;
dma-burst-sz = <16>;
bpp = <32>;
fdd = <0x80>;
sync-edge = <0>;
sync-ctrl = <1>;
raster-order = <0>;
fifo-th = <0>;
};
display-timings {
800x480p62 {
clock-frequency = <30000000>;
hactive = <800>;
vactive = <480>;
hfront-porch = <39>;
hback-porch = <39>;
hsync-len = <47>;
vback-porch = <29>;
vfront-porch = <13>;
vsync-len = <2>;
hsync-active = <1>;
vsync-active = <1>;
};
};
};
sound {
compatible = "ti,da830-evm-audio";
ti,model = "AM335x-EVM";
ti,audio-codec = <&tlv320aic3106>;
ti,mcasp-controller = <&mcasp1>;
ti,codec-clock-rate = <12000000>;
ti,audio-routing =
"Headphone Jack", "HPLOUT",
"Headphone Jack", "HPROUT",
"LINE1L", "Line In",
"LINE1R", "Line In";
};
};
&am33xx_pinmux {
pinctrl-names = "default";
pinctrl-0 = <&matrix_keypad_s0 &volume_keys_s0 &clkout2_pin>;
matrix_keypad_s0: matrix_keypad_s0 {
pinctrl-single,pins = <
0x54 (PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* gpmc_a5.gpio1_21 */
0x58 (PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* gpmc_a6.gpio1_22 */
0x64 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_a9.gpio1_25 */
0x68 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_a10.gpio1_26 */
0x6c (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_a11.gpio1_27 */
>;
};
volume_keys_s0: volume_keys_s0 {
pinctrl-single,pins = <
0x150 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* spi0_sclk.gpio0_2 */
0x154 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* spi0_d0.gpio0_3 */
>;
};
i2c0_pins: pinmux_i2c0_pins {
pinctrl-single,pins = <
0x188 (PIN_INPUT_PULLUP | MUX_MODE0) /* i2c0_sda.i2c0_sda */
0x18c (PIN_INPUT_PULLUP | MUX_MODE0) /* i2c0_scl.i2c0_scl */
>;
};
i2c1_pins: pinmux_i2c1_pins {
pinctrl-single,pins = <
0x158 (PIN_INPUT_PULLUP | MUX_MODE2) /* spi0_d1.i2c1_sda */
0x15c (PIN_INPUT_PULLUP | MUX_MODE2) /* spi0_cs0.i2c1_scl */
>;
};
uart0_pins: pinmux_uart0_pins {
pinctrl-single,pins = <
0x170 (PIN_INPUT_PULLUP | MUX_MODE0) /* uart0_rxd.uart0_rxd */
0x174 (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart0_txd.uart0_txd */
>;
};
uart1_pins: pinmux_uart1_pins {
pinctrl-single,pins = <
0x178 (PIN_INPUT | MUX_MODE0) /* uart1_ctsn.uart1_ctsn */
0x17C (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart1_rtsn.uart1_rtsn */
0x180 (PIN_INPUT_PULLUP | MUX_MODE0) /* uart1_rxd.uart1_rxd */
0x184 (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart1_txd.uart1_txd */
>;
};
clkout2_pin: pinmux_clkout2_pin {
pinctrl-single,pins = <
0x1b4 (PIN_OUTPUT_PULLDOWN | MUX_MODE3) /* xdma_event_intr1.clkout2 */
>;
};
nandflash_pins_s0: nandflash_pins_s0 {
pinctrl-single,pins = <
0x0 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad0.gpmc_ad0 */
0x4 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad1.gpmc_ad1 */
0x8 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad2.gpmc_ad2 */
0xc (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad3.gpmc_ad3 */
0x10 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad4.gpmc_ad4 */
0x14 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad5.gpmc_ad5 */
0x18 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad6.gpmc_ad6 */
0x1c (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad7.gpmc_ad7 */
0x70 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_wait0.gpmc_wait0 */
0x74 (PIN_INPUT_PULLUP | MUX_MODE7) /* gpmc_wpn.gpio0_30 */
0x7c (PIN_OUTPUT | MUX_MODE0) /* gpmc_csn0.gpmc_csn0 */
0x90 (PIN_OUTPUT | MUX_MODE0) /* gpmc_advn_ale.gpmc_advn_ale */
0x94 (PIN_OUTPUT | MUX_MODE0) /* gpmc_oen_ren.gpmc_oen_ren */
0x98 (PIN_OUTPUT | MUX_MODE0) /* gpmc_wen.gpmc_wen */
0x9c (PIN_OUTPUT | MUX_MODE0) /* gpmc_be0n_cle.gpmc_be0n_cle */
>;
};
ecap0_pins: backlight_pins {
pinctrl-single,pins = <
0x164 0x0 /* eCAP0_in_PWM0_out.eCAP0_in_PWM0_out MODE0 */
>;
};
cpsw_default: cpsw_default {
pinctrl-single,pins = <
/* Slave 1 */
0x114 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txen.rgmii1_tctl */
0x118 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxdv.rgmii1_rctl */
0x11c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd3.rgmii1_td3 */
0x120 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd2.rgmii1_td2 */
0x124 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd1.rgmii1_td1 */
0x128 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd0.rgmii1_td0 */
0x12c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txclk.rgmii1_tclk */
0x130 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxclk.rgmii1_rclk */
0x134 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd3.rgmii1_rd3 */
0x138 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd2.rgmii1_rd2 */
0x13c (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd1.rgmii1_rd1 */
0x140 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd0.rgmii1_rd0 */
>;
};
cpsw_sleep: cpsw_sleep {
pinctrl-single,pins = <
/* Slave 1 reset value */
0x114 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x118 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x11c (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x120 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x124 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x128 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x12c (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x130 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x134 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x138 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x13c (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x140 (PIN_INPUT_PULLDOWN | MUX_MODE7)
>;
};
davinci_mdio_default: davinci_mdio_default {
pinctrl-single,pins = <
/* MDIO */
0x148 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0) /* mdio_data.mdio_data */
0x14c (PIN_OUTPUT_PULLUP | MUX_MODE0) /* mdio_clk.mdio_clk */
>;
};
davinci_mdio_sleep: davinci_mdio_sleep {
pinctrl-single,pins = <
/* MDIO reset value */
0x148 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x14c (PIN_INPUT_PULLDOWN | MUX_MODE7)
>;
};
mmc1_pins: pinmux_mmc1_pins {
pinctrl-single,pins = <
0x160 (PIN_INPUT | MUX_MODE7) /* spi0_cs1.gpio0_6 */
>;
};
mmc3_pins: pinmux_mmc3_pins {
pinctrl-single,pins = <
0x44 (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_a1.mmc2_dat0, INPUT_PULLUP | MODE3 */
0x48 (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_a2.mmc2_dat1, INPUT_PULLUP | MODE3 */
0x4C (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_a3.mmc2_dat2, INPUT_PULLUP | MODE3 */
0x78 (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_ben1.mmc2_dat3, INPUT_PULLUP | MODE3 */
0x88 (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_csn3.mmc2_cmd, INPUT_PULLUP | MODE3 */
0x8C (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_clk.mmc2_clk, INPUT_PULLUP | MODE3 */
>;
};
wlan_pins: pinmux_wlan_pins {
pinctrl-single,pins = <
0x40 (PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* gpmc_a0.gpio1_16 */
0x19C (PIN_INPUT | MUX_MODE7) /* mcasp0_ahclkr.gpio3_17 */
0x1AC (PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* mcasp0_ahclkx.gpio3_21 */
>;
};
lcd_pins_s0: lcd_pins_s0 {
pinctrl-single,pins = <
0x20 (PIN_OUTPUT | MUX_MODE1) /* gpmc_ad8.lcd_data23 */
0x24 (PIN_OUTPUT | MUX_MODE1) /* gpmc_ad9.lcd_data22 */
0x28 (PIN_OUTPUT | MUX_MODE1) /* gpmc_ad10.lcd_data21 */
0x2c (PIN_OUTPUT | MUX_MODE1) /* gpmc_ad11.lcd_data20 */
0x30 (PIN_OUTPUT | MUX_MODE1) /* gpmc_ad12.lcd_data19 */
0x34 (PIN_OUTPUT | MUX_MODE1) /* gpmc_ad13.lcd_data18 */
0x38 (PIN_OUTPUT | MUX_MODE1) /* gpmc_ad14.lcd_data17 */
0x3c (PIN_OUTPUT | MUX_MODE1) /* gpmc_ad15.lcd_data16 */
0xa0 (PIN_OUTPUT | MUX_MODE0) /* lcd_data0.lcd_data0 */
0xa4 (PIN_OUTPUT | MUX_MODE0) /* lcd_data1.lcd_data1 */
0xa8 (PIN_OUTPUT | MUX_MODE0) /* lcd_data2.lcd_data2 */
0xac (PIN_OUTPUT | MUX_MODE0) /* lcd_data3.lcd_data3 */
0xb0 (PIN_OUTPUT | MUX_MODE0) /* lcd_data4.lcd_data4 */
0xb4 (PIN_OUTPUT | MUX_MODE0) /* lcd_data5.lcd_data5 */
0xb8 (PIN_OUTPUT | MUX_MODE0) /* lcd_data6.lcd_data6 */
0xbc (PIN_OUTPUT | MUX_MODE0) /* lcd_data7.lcd_data7 */
0xc0 (PIN_OUTPUT | MUX_MODE0) /* lcd_data8.lcd_data8 */
0xc4 (PIN_OUTPUT | MUX_MODE0) /* lcd_data9.lcd_data9 */
0xc8 (PIN_OUTPUT | MUX_MODE0) /* lcd_data10.lcd_data10 */
0xcc (PIN_OUTPUT | MUX_MODE0) /* lcd_data11.lcd_data11 */
0xd0 (PIN_OUTPUT | MUX_MODE0) /* lcd_data12.lcd_data12 */
0xd4 (PIN_OUTPUT | MUX_MODE0) /* lcd_data13.lcd_data13 */
0xd8 (PIN_OUTPUT | MUX_MODE0) /* lcd_data14.lcd_data14 */
0xdc (PIN_OUTPUT | MUX_MODE0) /* lcd_data15.lcd_data15 */
0xe0 (PIN_OUTPUT | MUX_MODE0) /* lcd_vsync.lcd_vsync */
0xe4 (PIN_OUTPUT | MUX_MODE0) /* lcd_hsync.lcd_hsync */
0xe8 (PIN_OUTPUT | MUX_MODE0) /* lcd_pclk.lcd_pclk */
0xec (PIN_OUTPUT | MUX_MODE0) /* lcd_ac_bias_en.lcd_ac_bias_en */
>;
};
am335x_evm_audio_pins: am335x_evm_audio_pins {
pinctrl-single,pins = <
0x10c (PIN_INPUT_PULLDOWN | MUX_MODE4) /* mii1_crs.mcasp1_aclkx */
0x110 (PIN_INPUT_PULLDOWN | MUX_MODE4) /* mii1_rxerr.mcasp1_fsx */
0x108 (PIN_OUTPUT_PULLDOWN | MUX_MODE4) /* mii1_col.mcasp1_axr2 */
0x144 (PIN_INPUT_PULLDOWN | MUX_MODE4) /* rmii1_ref_clk.mcasp1_axr3 */
>;
};
dcan1_pins_default: dcan1_pins_default {
pinctrl-single,pins = <
0x168 (PIN_OUTPUT | MUX_MODE2) /* uart0_ctsn.d_can1_tx */
0x16c (PIN_INPUT_PULLDOWN | MUX_MODE2) /* uart0_rtsn.d_can1_rx */
>;
};
};
&uart0 {
pinctrl-names = "default";
pinctrl-0 = <&uart0_pins>;
status = "okay";
};
&uart1 {
pinctrl-names = "default";
pinctrl-0 = <&uart1_pins>;
status = "okay";
};
&i2c0 {
pinctrl-names = "default";
pinctrl-0 = <&i2c0_pins>;
status = "okay";
clock-frequency = <400000>;
tps: tps@2d {
reg = <0x2d>;
};
};
&usb {
status = "okay";
};
&usb_ctrl_mod {
status = "okay";
};
&usb0_phy {
status = "okay";
};
&usb1_phy {
status = "okay";
};
&usb0 {
status = "okay";
};
&usb1 {
status = "okay";
dr_mode = "host";
};
&cppi41dma {
status = "okay";
};
&i2c1 {
pinctrl-names = "default";
pinctrl-0 = <&i2c1_pins>;
status = "okay";
clock-frequency = <100000>;
lis331dlh: lis331dlh@18 {
compatible = "st,lis331dlh", "st,lis3lv02d";
reg = <0x18>;
Vdd-supply = <&lis3_reg>;
Vdd_IO-supply = <&lis3_reg>;
st,click-single-x;
st,click-single-y;
st,click-single-z;
st,click-thresh-x = <10>;
st,click-thresh-y = <10>;
st,click-thresh-z = <10>;
st,irq1-click;
st,irq2-click;
st,wakeup-x-lo;
st,wakeup-x-hi;
st,wakeup-y-lo;
st,wakeup-y-hi;
st,wakeup-z-lo;
st,wakeup-z-hi;
st,min-limit-x = <120>;
st,min-limit-y = <120>;
st,min-limit-z = <140>;
st,max-limit-x = <550>;
st,max-limit-y = <550>;
st,max-limit-z = <750>;
};
tsl2550: tsl2550@39 {
compatible = "taos,tsl2550";
reg = <0x39>;
};
tmp275: tmp275@48 {
compatible = "ti,tmp275";
reg = <0x48>;
};
tlv320aic3106: tlv320aic3106@1b {
compatible = "ti,tlv320aic3106";
reg = <0x1b>;
status = "okay";
/* Regulators */
AVDD-supply = <&vaux2_reg>;
IOVDD-supply = <&vaux2_reg>;
DRVDD-supply = <&vaux2_reg>;
DVDD-supply = <&vbat>;
};
};
&lcdc {
status = "okay";
};
&elm {
status = "okay";
};
&epwmss0 {
status = "okay";
ecap0: ecap@100 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&ecap0_pins>;
};
};
&gpmc {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&nandflash_pins_s0>;
ranges = <0 0 0x08000000 0x1000000>; /* CS0: 16MB for NAND */
nand@0,0 {
reg = <0 0 4>; /* CS0, offset 0, IO size 4 */
ti,nand-ecc-opt = "bch8";
ti,elm-id = <&elm>;
nand-bus-width = <8>;
gpmc,device-width = <1>;
gpmc,sync-clk-ps = <0>;
gpmc,cs-on-ns = <0>;
gpmc,cs-rd-off-ns = <44>;
gpmc,cs-wr-off-ns = <44>;
gpmc,adv-on-ns = <6>;
gpmc,adv-rd-off-ns = <34>;
gpmc,adv-wr-off-ns = <44>;
gpmc,we-on-ns = <0>;
gpmc,we-off-ns = <40>;
gpmc,oe-on-ns = <0>;
gpmc,oe-off-ns = <54>;
gpmc,access-ns = <64>;
gpmc,rd-cycle-ns = <82>;
gpmc,wr-cycle-ns = <82>;
gpmc,wait-on-read = "true";
gpmc,wait-on-write = "true";
gpmc,bus-turnaround-ns = <0>;
gpmc,cycle2cycle-delay-ns = <0>;
gpmc,clk-activation-ns = <0>;
gpmc,wait-monitoring-ns = <0>;
gpmc,wr-access-ns = <40>;
gpmc,wr-data-mux-bus-ns = <0>;
/* MTD partition table */
/* All SPL-* partitions are sized to minimal length
* which can be independently programmable. For
* NAND flash this is equal to size of erase-block */
#address-cells = <1>;
#size-cells = <1>;
partition@0 {
label = "NAND.SPL";
reg = <0x00000000 0x000020000>;
};
partition@1 {
label = "NAND.SPL.backup1";
reg = <0x00020000 0x00020000>;
};
partition@2 {
label = "NAND.SPL.backup2";
reg = <0x00040000 0x00020000>;
};
partition@3 {
label = "NAND.SPL.backup3";
reg = <0x00060000 0x00020000>;
};
partition@4 {
label = "NAND.u-boot-spl-os";
reg = <0x00080000 0x00040000>;
};
partition@5 {
label = "NAND.u-boot";
reg = <0x000C0000 0x00100000>;
};
partition@6 {
label = "NAND.u-boot-env";
reg = <0x001C0000 0x00020000>;
};
partition@7 {
label = "NAND.u-boot-env.backup1";
reg = <0x001E0000 0x00020000>;
};
partition@8 {
label = "NAND.kernel";
reg = <0x00200000 0x00800000>;
};
partition@9 {
label = "NAND.file-system";
reg = <0x00A00000 0x0F600000>;
};
};
};
#include "tps65910.dtsi"
&mcasp1 {
pinctrl-names = "default";
pinctrl-0 = <&am335x_evm_audio_pins>;
status = "okay";
op-mode = <0>; /* MCASP_IIS_MODE */
tdm-slots = <2>;
/* 4 serializers */
serial-dir = < /* 0: INACTIVE, 1: TX, 2: RX */
0 0 1 2
>;
tx-num-evt = <32>;
rx-num-evt = <32>;
};
&tps {
vcc1-supply = <&vbat>;
vcc2-supply = <&vbat>;
vcc3-supply = <&vbat>;
vcc4-supply = <&vbat>;
vcc5-supply = <&vbat>;
vcc6-supply = <&vbat>;
vcc7-supply = <&vbat>;
vccio-supply = <&vbat>;
regulators {
vrtc_reg: regulator@0 {
regulator-always-on;
};
vio_reg: regulator@1 {
regulator-always-on;
};
vdd1_reg: regulator@2 {
/* VDD_MPU voltage limits 0.95V - 1.26V with +/-4% tolerance */
regulator-name = "vdd_mpu";
regulator-min-microvolt = <912500>;
regulator-max-microvolt = <1312500>;
regulator-boot-on;
regulator-always-on;
};
vdd2_reg: regulator@3 {
/* VDD_CORE voltage limits 0.95V - 1.1V with +/-4% tolerance */
regulator-name = "vdd_core";
regulator-min-microvolt = <912500>;
regulator-max-microvolt = <1150000>;
regulator-boot-on;
regulator-always-on;
};
vdd3_reg: regulator@4 {
regulator-always-on;
};
vdig1_reg: regulator@5 {
regulator-always-on;
};
vdig2_reg: regulator@6 {
regulator-always-on;
};
vpll_reg: regulator@7 {
regulator-always-on;
};
vdac_reg: regulator@8 {
regulator-always-on;
};
vaux1_reg: regulator@9 {
regulator-always-on;
};
vaux2_reg: regulator@10 {
regulator-always-on;
};
vaux33_reg: regulator@11 {
regulator-always-on;
};
vmmc_reg: regulator@12 {
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};
};
};
&mac {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
status = "okay";
slaves = <1>;
};
&davinci_mdio {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&davinci_mdio_default>;
pinctrl-1 = <&davinci_mdio_sleep>;
status = "okay";
ethphy0: ethernet-phy@0 {
reg = <0>;
};
};
&cpsw_emac0 {
phy-handle = <ðphy0>;
phy-mode = "rgmii-id";
};
&tscadc {
status = "okay";
tsc {
ti,wires = <4>;
ti,x-plate-resistance = <200>;
ti,coordinate-readouts = <5>;
ti,wire-config = <0x00 0x11 0x22 0x33>;
ti,charge-delay = <0x400>;
};
adc {
ti,adc-channels = <4 5 6 7>;
};
};
&mmc1 {
status = "okay";
vmmc-supply = <&vmmc_reg>;
bus-width = <4>;
pinctrl-names = "default";
pinctrl-0 = <&mmc1_pins>;
cd-gpios = <&gpio0 6 GPIO_ACTIVE_LOW>;
};
&mmc3 {
/* these are on the crossbar and are outlined in the
xbar-event-map element */
dmas = <&edma 12 0
&edma 13 0>;
dma-names = "tx", "rx";
status = "okay";
vmmc-supply = <&wlan_en_reg>;
bus-width = <4>;
pinctrl-names = "default";
pinctrl-0 = <&mmc3_pins &wlan_pins>;
ti,non-removable;
ti,needs-special-hs-handling;
cap-power-off-card;
keep-power-in-suspend;
#address-cells = <1>;
#size-cells = <0>;
wlcore: wlcore@0 {
compatible = "ti,wl1835";
reg = <2>;
interrupt-parent = <&gpio3>;
interrupts = <17 IRQ_TYPE_LEVEL_HIGH>;
};
};
&edma {
ti,edma-xbar-event-map = /bits/ 16 <1 12
2 13>;
};
&sham {
status = "okay";
};
&aes {
status = "okay";
};
&dcan1 {
status = "disabled"; /* Enable only if Profile 1 is selected */
pinctrl-names = "default";
pinctrl-0 = <&dcan1_pins_default>;
};
&rtc {
clocks = <&clk_32768_ck>, <&clk_24mhz_clkctrl AM3_CLK_24MHZ_CLKDIV32K_CLKCTRL 0>;
clock-names = "ext-clk", "int-clk";
};
In our device tree the
* NAND flash this is equal to size of erase-block */
#address-cells = <1>;
#size-cells = <1>;
partition@0 {
label = "NAND.SPL";
reg = <0x00000000 0x000020000>;
};
partition@1 {
label = "NAND.SPL.backup1";
reg = <0x00020000 0x00020000>;
};
partition@2 {
label = "NAND.SPL.backup2";
reg = <0x00040000 0x00020000>;
};
partition@3 {
label = "NAND.SPL.backup3";
reg = <0x00060000 0x00020000>;
};
partition@4 {
label = "NAND.u-boot-spl-os";
reg = <0x00080000 0x00040000>;
};
partition@5 {
label = "NAND.u-boot";
reg = <0x000C0000 0x00100000>;
};
partition@6 {
label = "NAND.u-boot-env";
reg = <0x001C0000 0x00020000>;
};
partition@7 {
label = "NAND.u-boot-env.backup1";
reg = <0x001E0000 0x00020000>;
};
partition@8 {
label = "NAND.kernel";
reg = <0x00200000 0x00800000>;
};
partition@9 {
label = "NAND.file-system";
reg = <0x00A00000 0x0F600000>;
};
};
is missing. Trying to boot with spl from sdcard. Is this section important?