This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

vc3 demo doesn't run with omtb

I am using ezsdk 5.02.01.59. and i am building m3 source as well as a8host source. When I build the vc3 demo and try to use it with the omtb test bench.

 

I execute the following:

     cd /usr/share/ti/ti-omtb
     ./omtb_dm816xbm_a8host.xv5T  decode_scale_display.oms

 

I get the following error:

        Error [0xffffffff] at Line no: 1091 in file /home/jwhit/projects/z3/netra-sdk-5.02/ezsdk/component-sources/syslink_2_00_02_80/packages/ti/syslink/utils/h
los/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/SharedRegion.c
Assertion at Line no: 430 in /home/jwhit/projects/z3/netra-sdk-5.02/ezsdk/component-sources/syslink_2_00_02_80/packages/ti/syslink/utils/hlos/knl/Linux/../../../
../../../ti/syslink/ipc/hlos/knl/Linux/SharedRegionDrv.c: (status >= 0) : failed
*** SharedRegion_setEntry: HeapMemMP_openByAddr failed!
        Error [0xffffffff] at Line no: 1091 in file /home/jwhit/projects/z3/netra-sdk-5.02/ezsdk/component-sources/syslink_2_00_02_80/packages/ti/syslink/utils/h
los/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/SharedRegion.c
Assertion at Line no: 430 in /home/jwhit/projects/z3/netra-sdk-5.02/ezsdk/component-sources/syslink_2_00_02_80/packages/ti/syslink/utils/hlos/knl/Linux/../../../
../../../ti/syslink/ipc/hlos/knl/Linux/SharedRegionDrv.c: (status >= 0) : failed

 

It works fine if I use the bm build

Does the vc3 work with the omtb?

 

Is it possible to build it so that it works with the test bench.

 

I am trying to port my app to the new ezsdk, and I get the same errors as soon as OMX_init runs on the a8host.

 

regards,

nb