Other Parts Discussed in Thread: OMAP-L137
I am using a custom board based on OMAP-L137 EVM Rev H from Spectrum Digital. The custom board does not use the EMAC, McASP and OHCI. Versions:
DVSDK 03.21.00.04/linux-2.6.37
DSPLink 1.65.00.03
helloDSP 1.10
BIOS 5.41.10.36
EDMA 01.11.02.05
PSP 01.30.01
XDCTools 03.22.01.21
CGT6.1.12
The kernel has been compiled without sound or network drivers. My application is based upon the helloDSP example with the addition of SPI data acquisition on the DSP side via BIOSPSP. On my custom board, I am getting kernel panics immediately or after a few seconds of data acquiistion. Attached are the some kernel panic texts. On the EVM, kernel panics do not appear to happen. Any comments would be appreciated.