Hi,
I just want to know what the following messages mean that appear during the VC application run time.
decodeFrameNumber[Port0]: 44400
frameNumber[Port0]: 45000
(1) - 30 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
(0) - 30 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
And, what if the number '30' is changed to some lower value? Say,
(1) - 29 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
(0) - 30 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
Thanks!