Other Parts Discussed in Thread: AM4378
Tool/software:
Hi,
As mentioned in the related question, I am considering USB boot. If the boot sequence is set to USB_MS, what data should be written to the USB memory?
I tried to insert the USB into the evaluation board (AM437xEVM) and boot it using the following procedure, but it did not work.
- Insert the USB memory into a Windows PC and copy the following data to the root directory.
1. MLO
2. U-boot.img
3. U-boot-spl.bin
4. zImage
5. am4378.ccxml
6. tisdk-base-image-am437x-evm.ubi
7. debrick.scr
8. am437x-gp-evm-hdmi.dtb
- Insert the above USB into J13 (USB1) of the evaluation board.
- Turn on the power switch of SW12 of the evaluation board with the settings 1: ON-2: ON-3: ON-4: OFF-5: OFF.
I tried to boot it using the above procedure, but it did not work.
Can you give me some advice?
Thanks,
Conor