Other Parts Discussed in Thread: SYSBIOS
hi all,
I try to use c64plus-imglib and install c64plus-imglib_2_02_00_00.
and try \test_drivers\drivers\IMG_sobel_3x3_8 example to test imglib can work or not.
I created an c6000 SYS/BIOS CCS example project in CCS5.1.
then copy the IMG_sobel_3x3_8_d.c in c64plus-imglib_2_02_00_00\test_drivers\drivers\IMG_sobel_3x3_8.
then add the IMG_sobel_3x3_8_idat.c and IMG_sobel_3x3_8_odat.c into the project.
it can run but had problem when execute the following code.
/* run the testcase */
t1 = clock();
IMG_sobel_3x3_8 (src_ptr, output_ptr, cols, rows);
t2 = clock();
the t1, t2 return 0;
and IMG_sobel_3x3_8 function can't work.
Is it an linking problem?
the following code is the test code source.
/* ======================================================================== */
/* TEXAS INSTRUMENTS, INC. */
/* */
/* IMGLIB-2 DSP Image/Video Processing Library */
/* */
/* Release: Revision 2.0.1 */
/* Snapshot date: 6-May-2008 */
/* */
/* This library contains proprietary intellectual property of Texas */
/* Instruments, Inc. The library and its source code are protected by */
/* various copyrights, and portions may also be protected by patents or */
/* other legal protections. */
/* */
/* This software is licensed for use with Texas Instruments TMS320 */
/* family DSPs. This license was provided to you prior to installing */
/* the software. You may review this license by consulting the file */
/* TI_license.PDF which accompanies the files in this library. */
/* ------------------------------------------------------------------------ */
/* Copyright (C) 2008 Texas Instruments, Incorporated. */
/* All Rights Reserved. */
/* ======================================================================== */
/* Copyright 2008, Texas Instruments, Inc. All rights reserved. */
#include <stdio.h>
#include <time.h>
#include "mem_cpy.h"
#include "support.h"
#include "IMG_sobel_3x3_8.h"
#include "IMG_sobel_3x3_8_c.h"
#define N 96
#define PAD 64
#define SIZE (N + 2*PAD)
typedef unsigned char D_type;
D_type input[SIZE];
D_type output[SIZE], ref_output[SIZE];
/* Declare the golden input and output data buffers created in Matlab. */
extern int in_data[]; /* Standard input data array. */
extern D_type out_data[]; /* Standard output data array. */
extern int testcases; /* number of test-cases */
main()
{
clock_t t_start, t_stop, t_overhead, t1, t2, t_c, t_cn;
int count;
int in_size, out_size;
int cols, rows;
short align_in, align_out;
D_type *src_ptr;
D_type *output_ptr, *ref_output_ptr;
int *inp = &in_data[0];
D_type *outp = &out_data[0];
/* Compute the overhead of calling clock twice to get timing info. */
t_start = clock();
t_stop = clock();
t_overhead = t_stop - t_start;
/* Read test parameters. */
align_in = *inp++;
align_out = *inp++;
src_ptr = (D_type *)( (unsigned int)&input[PAD] + align_in );
output_ptr = (D_type *)( (unsigned int)&output[PAD] + align_out);
ref_output_ptr = (D_type *)( (unsigned int)&ref_output[PAD] + align_out);
for(count = 1; count <= testcases; count++)
{
/* Read test-case params. */
cols = *inp++;
rows = *inp++;
in_size = *inp++;
out_size = *inp++; // input and output size is the same.
/* Checking sanity of generated driver. */
if( N < in_size )
{
printf("source or dst array size is less than test-case (ID %d) size\n", count);
return(0);
}
/* Prepare output arrays */
memset(input, 0, sizeof(input));
memset(output, 0, sizeof(output[0]) * SIZE);
memset(ref_output, 0, sizeof(ref_output[0]) * SIZE);
/* Copy input and ref output to respective buffers */
copy_int_to_uchar(src_ptr, inp, in_size); // copy input
inp += in_size;
memcpy(ref_output_ptr + 1, outp, out_size * sizeof(outp[0]));
outp += out_size;
/* run the testcase */
t1 = clock();
IMG_sobel_3x3_8 (src_ptr, output_ptr, cols, rows);
t2 = clock();
t_c = t2 - t1 - t_overhead;
if( memcmp(output, ref_output, SIZE * sizeof(ref_output[0])) )
{
printf("Result failure: output - intrinsics: case # %d\n", count);
return(0);
}
memset(output, 0, sizeof(output[0]) * SIZE);
t1 = clock();
IMG_sobel_3x3_8_cn (src_ptr, output_ptr, cols, rows);
t2 = clock();
t_cn = t2 - t1 - t_overhead;
if( memcmp(output, ref_output, SIZE * sizeof(ref_output[0])) )
{
printf("Result failure: output - natural c: case # %d\n", count);
return(0);
}
printf("%2d : C = %4d, natC = %4d\n", count, t_c, t_cn);
} /* for */
printf("Success. Test suite (%d cases) passed.\n", testcases);
return(0);
}
regards,
Yi-LIn