Hello!
We are using the OMAP-L138. for indoor navigation. I'm trying to catch a Transfer Completion Interrupt from EDMA on the DSP side of OMAP-L138.
I'm using channel 10 for my DMA transfer,
In the SPRUGP9B document page 42 it is mentioned that the EDMA3_0_CC0_INT (EDMA3 Transfer Completion Interrupts) event number is 8
I use HWI_eventMap command to map event 8 to a physical interrupt without success but when I use the event 11 it is work
Whould you like to explain me why?
Regards
PF