This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J721E: change the path of gcc toolchain within the Linux SDK

Part Number: PROCESSOR-SDK-J721E

Tool/software:

hi Ti

I download the sdk of ti-processor-sdk-linux-adas-j721e-evm-09_01_00_06,and run the SDK Installer.I want to change the path of gcc toolchain about linux-devkit/ directory and k3r5-devkit/ directory.I move two directorys to other path, but now i can not build the sdk.

I have other problem of the sdk.I build the uboot but failed before move two directorys.I run the 'make u-boot' in ubuntu 22.04,and I can build ti-processor-sdk-rtos-j784s4-evm-09_01_00_06 succeed.