This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: Error in the AM62x Academy

Part Number: AM625

Tool/software:

There is not USB ID pin On AM6x device, but it still tells user to use USB ID Pin.

https://dev.ti.com/tirex/explore/node?node=A__ARuO9NQ7pbUhENsPI2RGDQ__AM62-ACADEMY__uiYMDcq__LATEST&placeholder=true

“otg”

Specifies the USB module to work in dual-role mode, in which the mode is determined by the USB_ID pin status. The USB module works in host mode when USB_ID pin is grounded, or in device mode when USB_ID pin is float.

When dr_mode = “otg”, the USB_ID pin should be routed to the ID pin of the USB receptacle. That allows the inserted USB cable to control the status of the USB_ID pin.