Part Number: AM6411
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hello,
I am modifying the uniflash and bootloader applications to support my custom board which mounts a quad-spi flash (S25HS512TFAMHI01).
I managed to successfully flash the bootloader at 0x00 and the application at 0x80000, but when the bootloader starts after reset the system hangs on this function call:
status = Bootloader_parseMultiCoreAppImage(bootHandle, &bootImageInfo);.
By single-stepping through the code I found out that the code hangs and end up in
HwiP_data_abort_handlerwhen executing the following statements in file bootloader.c line 384:
if ((*x509_cert_ptr == seq_oid[0]) &&
(*(x509_cert_ptr + 2) == seq_oid[2]) &&
(*(x509_cert_ptr - 2) == 0x30))
The same application instead runs smoothly if I load it using for example uart bootloader so I exclude it is a certificate problem.
Some notes:
- I am using mcu_plus_sdk_am64x_09_01_00_41
- I used sbl_ospi application as a starting point.
- I need to reset the flash before calling
status = Board_driversOpen();
otherwise the system reads wrong manufacturer id and device id.
Looking forward to hearing from you
Paolo