Other Parts Discussed in Thread: 4430
Hi
I am trying to write an accelerometer driver in android froyo on the pandaboard.
The problem I encounter is that pandaboard has an accelerometer (VTI) which android choose to work with him.
Internal accelerometer gets /dev/input/event2, while we get /dev/input/event7, so Android ignores us,
It’s seems android support only one device (accelerometer) for each device,
My question is what is the name of the driver, or configuration parameter in the kernel so I can disable it.
I am using Froyo Kernel2-6.35 configuration file android_4430_defconfig.
See below event file Description
There is an internal sensor in
Input driver version is 1.0.0
Input device ID: bus 0x0 vendor 0x0 product 0x0 version 0x0
Input device name: "sensors"
Supported events:
Event type 0 (Sync)
Event type 3 (Absolute)
Event code 0 (X)
Value 0
Min -8000
Max 8000
Event code 1 (Y)
Value 0
Min -8000
Max 8000
Event code 2 (Z)
Value 0
Min -8000
Max 8000
Event code 10 (Brake)
Value 0
Min -8000
Max 8000
Event code 16 (Hat0X)
Value 0
Min -8000
Max 8000
Event code 17 (Hat0Y)
Value 0
Min -8000
Max 8000
Event code 24 (Pressure)
Value 0
Min -8000
Max 8000
Event code 25 (Distance)
Value 0
Min -8000
Max 8000
Event code 40 (Misc)
Value 0
Min -8000
Max 8000
Event type 17 (LED)
Event code 8 (Misc)