Part Number: TDA4VL-Q1
Tool/software:
Hi, experts ,
Currently we are porting 0902sdk kernel and related drivers to sdk0806, we are using 0902sdk kernel source code ti-processor-sdk-linux-adas-j721s2-evm-09_02_00_05/board-support/ti-linux-kernel- 6.1.80+gitAUTOINC+2e423244f8-ti, but the toolchain uses the 0806sdk ti-processor-sdk-linux-j721s2-evm-08_06_01_02/linux-devkit/sysroots/x86_64-arago- linux/. This way we basically don't have to change the application and filesystem.
Now the kernel is up and running, the GPU driver (source code ti-img-rogue-driver-23.3.6512818) can be loaded normally, but when calling the gpu dynamic library in the application layer, we found that the version of glibc does not correspond to the 0806sdk, the glibc of the 0902 is 2.33, and the version of the 2.30.
Because the gpu dynamic library source code is not open source, so our gpu dynamic library can only be obtained from this link graphics/ti-img-rogue-umlibs - Graphics related projects on TI platforms - Graphics libraries for Imagination Rogue GPU on Texas Instruments SoC., can not be adapted to our current use of the situation, so can we ask you to provide:
Use 0806's compilation toolchain to compile version 23.3.6512818 of the gpu dynamic library to us, thanks~!
Best Regards,
Bing