Hi,
I am working with a custom board with DM365. The codec IC is connected in I2S mode to the DM365.
I have given the dai_link parameters as below.
static struct snd_soc_dai_link custom_dai = {
.name = "TLV320AIC3X",
.stream_name = "AIC3X",
.cpu_dai = &davinci_i2s_dai,
.codec_dai = &aic3x_dai,
.init = custom_aic3x_init,
.ops = &custom_ops,
};
But for me the davinci_i2s_probe function is not called and cpu dai is not registering and sound card is not detecting.
Could you please tell me why davinci_i2s_probe function is not getting invoked. I am working with 2.6.32 kernel
Thank you, Sreedhar