If I'm running with the sys clock at 26MHz, what are the settings I should use to get the fastest clocks for my peripherals?
The Logic PD code isn't making sense. They reference a 52MHz clock that doesn't exist. Since DPLL4 is either DPLL3/2 or DPLL3/1 and they're stating that they've set DPLL3 to 166 Mhz, the 52MHz clock is not there.
Thanks,
Matt