This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDVPSS interface on DM8168

Hi,

When using the video in bus on the DM8168, if only VIN[1]A_D(0:23) is going to be used are both clocks (VIN[1]A_CLK and VIN[1]B_CLK ) required to be fed with a clock signal or only VIN[1]A_CLK?

Regards.

  • Hi Ivan,

    I just wanted to clarify that VIN[1] only supports 16 bit capture.  If you need 24-bit capture then use VIN[0].  In either case, you only need the B_CLK if you are splitting the port into 2 separate 8-bit capture ports.  If you are doing 16/24-bit capture you only need A_CLK.

    Regards,
    Marc