This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: LSC Calibration ISP DCC Tuning Tool - AM62A3

Part Number: SK-AM62A-LP

Tool/software:

Hello,

We are working on LSC for the IMX219. When we generated the default BIN file from the DCC tools, we encountered lines on the screen.


 

I have attached the Files below,

<?xml version="1.0" encoding="utf-8"?>
<RAWFE_cfg_lsc_xml xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance" xmlns:xsd="http://www.w3.org/2001/XMLSchema">
  <!--this is a comment-->
    <dcc_name>rawfe_cfg_lsc</dcc_name>
    <dcc_header>
        <camera_module_id>     219 </camera_module_id>
        <dcc_descriptor_id>    7 </dcc_descriptor_id>
        <algorithm_vendor_id>  1 </algorithm_vendor_id>
        <tunning_tool_version> 0 </tunning_tool_version>
    </dcc_header>
    <!--=======================================================================-->
    <typedef>
        <cfg_rawfe_lsc type="struct">
            <!--==================cfg lsc=====================================================-->
            <lsc_cfg_enable type="uint32"> </lsc_cfg_enable>
            <lsc_cfg_gain_mode_m type="uint32"> </lsc_cfg_gain_mode_m>
            <lsc_cfg_gain_mode_n type="uint32"> </lsc_cfg_gain_mode_n>
            <lsc_cfg_gain_format type="uint32"> </lsc_cfg_gain_format>
            <lsc_cfg_lut_size    type="uint32"> </lsc_cfg_lut_size>
            <lsc_lut type="uint8*"> </lsc_lut>
        </cfg_rawfe_lsc>
    </typedef>
    <!--=======================================================================-->
    <use_case val="65535">
        <n-space>
            <region0 class="0">
				<gain             val="0" min="0" max="1000000">  </gain>
				<exposure         val="1" min="0" max="1000000">  </exposure>
				<colortemperature val="2" min="0" max="1000000">  </colortemperature>
            </region0>
        </n-space>

        <parameter_package>
            <rawfe_lsc_dcc type="cfg_rawfe_lsc">
            {
                <!--===============================cfg lsc dcc=======================================-->

                1           // lsc_cfg_enable         0:disable, 1: enable
                5           // lsc_cfg_gain_mode_m    3:8x, 4:16x, 5: 32x, 6: 64x, 7: 128x
                5           // lsc_cfg_gain_mode_n    3:8x, 4:16x, 5: 32x, 6: 64x, 7: 128x
                1           // lsc_cfg_gain_format    0:Q8, 1:Q8+1, 2:Q7, 3:Q7+1, 4:Q6, 5:Q6+1, 6:Q5, 7:Q5+1
                8480           // lsc_cfg_lut_size       in bytes
                {
178 178 178 178 170 170 170 170 163 163 163 163 151 151 151 151 144 144 144 144 133 133 133 133 127 127 127 127 119 119 119 119 114 114 114 114 106 106 106 106 102 102 102 102  95  95  95  95  88  88  88  88  86  86  86  86  80  80  80  80  76  76  76  76  73  73  73  73  69  69  69  69  67  67  67  67  66  66  66  66  62  62  62  62  61  61  61  61  59  59  59  59  57  57  57  57  57  57  57  57  57  57  57  57  57  57  57  57  57  57  57  57  57  57  57  57  59  59  59  59  61  61  61  61  62  62  62  62  64  64  64  64  67  67  67  67  69  69  69  69  73  73  73  73  76  76  76  76  79  79  79  79  84  84  84  84  88  88  88  88  93  93  93  93  99  99  99  99 104 104 104 104 111 111 111 111 117 117 117 117 125 125 125 125 133 133 133 133 142 142 142 142 149 149 149 149 159 159 159 159 166 166 166 166 178 178 178 178 186 186 186 186
170 170 170 170 163 163 163 163 152 152 152 152 146 146 146 146 136 136 136 136 127 127 127 127 119 119 119 119 114 114 114 114 106 106 106 106  99  99  99  99  93  93  93  93  88  88  88  88  82  82  82  82  78  78  78  78  75  75  75  75  69  69  69  69  67  67  67  67  64  64  64  64  61  61  61  61  57  57  57  57  56  56  56  56  54  54  54  54  53  53  53  53  51  51  51  51  51  51  51  51  51  51  51  51  51  51  51  51  51  51  51  51  51  51  51  51  53  53  53  53  54  54  54  54  56  56  56  56  57  57  57  57  59  59  59  59  62  62  62  62  67  67  67  67  69  69  69  69  73  73  73  73  78  78  78  78  82  82  82  82  86  86  86  86  93  93  93  93  99  99  99  99 104 104 104 104 111 111 111 111 117 117 117 117 125 125 125 125 133 133 133 133 142 142 142 142 149 149 149 149 161 161 161 161 170 170 170 170 179 179 179 179
166 166 166 166 156 156 156 156 146 146 146 146 136 136 136 136 127 127 127 127 122 122 122 122 114 114 114 114 106 106 106 106  99  99  99  99  93  93  93  93  86  86  86  86  82  82  82  82  76  76  76  76  73  73  73  73  67  67  67  67  64  64  64  64  61  61  61  61  57  57  57  57  54  54  54  54  53  53  53  53  50  50  50  50  49  49  49  49  47  47  47  47  47  47  47  47  45  45  45  45  45  45  45  45  45  45  45  45  45  45  45  45  46  46  46  46  47  47  47  47  48  48  48  48  50  50  50  50  51  51  51  51  54  54  54  54  57  57  57  57  59  59  59  59  64  64  64  64  67  67  67  67  71  71  71  71  76  76  76  76  80  80  80  80  86  86  86  86  91  91  91  91  99  99  99  99 104 104 104 104 111 111 111 111 119 119 119 119 127 127 127 127 136 136 136 136 146 146 146 146 152 152 152 152 163 163 163 163 172 172 172 172
159 159 159 159 149 149 149 149 139 139 139 139 130 130 130 130 122 122 122 122 114 114 114 114 106 106 106 106  99  99  99  99  93  93  93  93  86  86  86  86  80  80  80  80  76  76  76  76  71  71  71  71  67  67  67  67  62  62  62  62  57  57  57  57  55  55  55  55  51  51  51  51  50  50  50  50  47  47  47  47  44  44  44  44  44  44  44  44  43  43  43  43  41  41  41  41  40  40  40  40  40  40  40  40  40  40  40  40  40  40  40  40  41  41  41  41  43  43  43  43  43  43  43  43  44  44  44  44  47  47  47  47  48  48  48  48  51  51  51  51  54  54  54  54  57  57  57  57  61  61  61  61  66  66  66  66  69  69  69  69  75  75  75  75  80  80  80  80  86  86  86  86  91  91  91  91  99  99  99  99 104 104 104 104 114 114 114 114 120 120 120 120 127 127 127 127 136 136 136 136 146 146 146 146 156 156 156 156 166 166 166 166
152 152 152 152 145 145 145 145 133 133 133 133 125 125 125 125 117 117 117 117 109 109 109 109 102 102 102 102  95  95  95  95  86  86  86  86  80  80  80  80  76  76  76  76  69  69  69  69  66  66  66  66  61  61  61  61  57  57  57  57  53  53  53  53  50  50  50  50  47  47  47  47  44  44  44  44  43  43  43  43  40  40  40  40  38  38  38  38  37  37  37  37  36  36  36  36  36  36  36  36  35  35  35  35  35  35  35  35  36  36  36  36  36  36  36  36  36  36  36  36  37  37  37  37  40  40  40  40  41  41  41  41  44  44  44  44  45  45  45  45  50  50  50  50  52  52  52  52  56  56  56  56  59  59  59  59  64  64  64  64  69  69  69  69  75  75  75  75  80  80  80  80  86  86  86  86  93  93  93  93  99  99  99  99 106 106 106 106 114 114 114 114 123 123 123 123 130 130 130 130 142 142 142 142 149 149 149 149 162 162 162 162
146 146 146 146 136 136 136 136 127 127 127 127 119 119 119 119 111 111 111 111 102 102 102 102  95  95  95  95  88  88  88  88  82  82  82  82  76  76  76  76  70  70  70  70  66  66  66  66  60  60  60  60  56  56  56  56  51  51  51  51  48  48  48  48  44  44  44  44  43  43  43  43  40  40  40  40  37  37  37  37  36  36  36  36  33  33  33  33  32  32  32  32  31  31  31  31  30  30  30  30  30  30  30  30  30  30  30  30  30  30  30  30  31  31  31  31  32  32  32  32  33  33  33  33  35  35  35  35  36  36  36  36  38  38  38  38  41  41  41  41  44  44  44  44  47  47  47  47  51  51  51  51  54  54  54  54  59  59  59  59  64  64  64  64  69  69  69  69  75  75  75  75  80  80  80  80  86  86  86  86  94  94  94  94 102 102 102 102 109 109 109 109 117 117 117 117 127 127 127 127 135 135 135 135 146 146 146 146 156 156 156 156
142 142 142 142 130 130 130 130 124 124 124 124 114 114 114 114 106 106 106 106  99  99  99  99  91  91  91  91  84  84  84  84  78  78  78  78  71  71  71  71  66  66  66  66  61  61  61  61  56  56  56  56  51  51  51  51  47  47  47  47  44  44  44  44  41  41  41  41  37  37  37  37  35  35  35  35  32  32  32  32  30  30  30  30  28  28  28  28  28  28  28  28  27  27  27  27  26  26  26  26  26  26  26  26  26  26  26  26  26  26  26  26  27  27  27  27  27  27  27  27  28  28  28  28  30  30  30  30  32  32  32  32  35  35  35  35  37  37  37  37  40  40  40  40  43  43  43  43  47  47  47  47  50  50  50  50  54  54  54  54  59  59  59  59  65  65  65  65  69  69  69  69  76  76  76  76  82  82  82  82  88  88  88  88  97  97  97  97 104 104 104 104 114 114 114 114 121 121 121 121 130 130 130 130 139 139 139 139 149 149 149 149
136 136 136 136 127 127 127 127 117 117 117 117 109 109 109 109 102 102 102 102  93  93  93  93  86  86  86  86  78  78  78  78  73  73  73  73  67  67  67  67  61  61  61  61  56  56  56  56  51  51  51  51  47  47  47  47  44  44  44  44  40  40  40  40  36  36  36  36  33  33  33  33  31  31  31  31  28  28  28  28  27  27  27  27  25  25  25  25  24  24  24  24  24  24  24  24  23  23  23  23  23  23  23  23  23  23  23  23  23  23  23  23  23  23  23  23  24  24  24  24  25  25  25  25  26  26  26  26  28  28  28  28  30  30  30  30  33  33  33  33  36  36  36  36  38  38  38  38  43  43  43  43  46  46  46  46  50  50  50  50  55  55  55  55  59  59  59  59  66  66  66  66  71  71  71  71  78  78  78  78  84  84  84  84  91  91  91  91  99  99  99  99 106 106 106 106 117 117 117 117 125 125 125 125 133 133 133 133 146 146 146 146
130 130 130 130 123 123 123 123 114 114 114 114 104 104 104 104  97  97  97  97  88  88  88  88  82  82  82  82  76  76  76  76  69  69  69  69  62  62  62  62  57  57  57  57  52  52  52  52  48  48  48  48  44  44  44  44  40  40  40  40  36  36  36  36  32  32  32  32  30  30  30  30  27  27  27  27  25  25  25  25  24  24  24  24  22  22  22  22  20  20  20  20  19  19  19  19  19  19  19  19  18  18  18  18  18  18  18  18  18  18  18  18  19  19  19  19  20  20  20  20  22  22  22  22  23  23  23  23  25  25  25  25  27  27  27  27  28  28  28  28  32  32  32  32  36  36  36  36  38  38  38  38  43  43  43  43  47  47  47  47  51  51  51  51  56  56  56  56  61  61  61  61  67  67  67  67  74  74  74  74  80  80  80  80  86  86  86  86  95  95  95  95 102 102 102 102 111 111 111 111 119 119 119 119 130 130 130 130 139 139 139 139
127 127 127 127 119 119 119 119 109 109 109 109 102 102 102 102  93  93  93  93  86  86  86  86  78  78  78  78  71  71  71  71  66  66  66  66  59  59  59  59  54  54  54  54  49  49  49  49  44  44  44  44  40  40  40  40  36  36  36  36  32  32  32  32  28  28  28  28  26  26  26  26  24  24  24  24  22  22  22  22  20  20  20  20  18  18  18  18  18  18  18  18  17  17  17  17  16  16  16  16  16  16  16  16  16  16  16  16  16  16  16  16  16  16  16  16  17  17  17  17  18  18  18  18  19  19  19  19  22  22  22  22  24  24  24  24  26  26  26  26  28  28  28  28  31  31  31  31  36  36  36  36  38  38  38  38  43  43  43  43  48  48  48  48  53  53  53  53  57  57  57  57  64  64  64  64  69  69  69  69  76  76  76  76  84  84  84  84  91  91  91  91  99  99  99  99 106 106 106 106 117 117 117 117 127 127 127 127 136 136 136 136
125 125 125 125 114 114 114 114 106 106 106 106  98  98  98  98  88  88  88  88  82  82  82  82  75  75  75  75  67  67  67  67  62  62  62  62  56  56  56  56  50  50  50  50  45  45  45  45  41  41  41  41  36  36  36  36  33  33  33  33  29  29  29  29  26  26  26  26  24  24  24  24  22  22  22  22  19  19  19  19  17  17  17  17  16  16  16  16  15  15  15  15  14  14  14  14  13  13  13  13  13  13  13  13  13  13  13  13  13  13  13  13  13  13  13  13  14  14  14  14  16  16  16  16  17  17  17  17  18  18  18  18  20  20  20  20  23  23  23  23  25  25  25  25  28  28  28  28  32  32  32  32  36  36  36  36  40  40  40  40  44  44  44  44  50  50  50  50  54  54  54  54  59  59  59  59  67  67  67  67  73  73  73  73  80  80  80  80  86  86  86  86  95  95  95  95 104 104 104 104 114 114 114 114 122 122 122 122 130 130 130 130
122 122 122 122 112 112 112 112 102 102 102 102  95  95  95  95  86  86  86  86  78  78  78  78  71  71  71  71  66  66  66  66  59  59  59  59  53  53  53  53  48  48  48  48  43  43  43  43  38  38  38  38  35  35  35  35  30  30  30  30  27  27  27  27  24  24  24  24  20  20  20  20  18  18  18  18  17  17  17  17  15  15  15  15  13  13  13  13  12  12  12  12  12  12  12  12  11  11  11  11  11  11  11  11  11  11  11  11  11  11  11  11  11  11  11  11  12  12  12  12  13  13  13  13  14  14  14  14  16  16  16  16  18  18  18  18  20  20  20  20  23  23  23  23  26  26  26  26  28  28  28  28  33  33  33  33  37  37  37  37  42  42  42  42  47  47  47  47  51  51  51  51  57  57  57  57  64  64  64  64  69  69  69  69  76  76  76  76  84  84  84  84  93  93  93  93 102 102 102 102 109 109 109 109 119 119 119 119 127 127 127 127
117 117 117 117 109 109 109 109  99  99  99  99  91  91  91  91  84  84  84  84  76  76  76  76  69  69  69  69  62  62  62  62  56  56  56  56  50  50  50  50  45  45  45  45  40  40  40  40  36  36  36  36  31  31  31  31  28  28  28  28  24  24  24  24  22  22  22  22  18  18  18  18  16  16  16  16  14  14  14  14  13  13  13  13  11  11  11  11  10  10  10  10   9   9   9   9   9   9   9   9   8   8   8   8   8   8   8   8   9   9   9   9   9   9   9   9  10  10  10  10  11  11  11  11  12  12  12  12  14  14  14  14  16  16  16  16  18  18  18  18  20  20  20  20  24  24  24  24  27  27  27  27  30  30  30  30  35  35  35  35  38  38  38  38  44  44  44  44  50  50  50  50  54  54  54  54  61  61  61  61  67  67  67  67  75  75  75  75  81  81  81  81  88  88  88  88  99  99  99  99 106 106 106 106 117 117 117 117 125 125 125 125
117 117 117 117 106 106 106 106  97  97  97  97  88  88  88  88  80  80  80  80  74  74  74  74  67  67  67  67  59  59  59  59  54  54  54  54  48  48  48  48  43  43  43  43  37  37  37  37  33  33  33  33  29  29  29  29  25  25  25  25  23  23  23  23  19  19  19  19  17  17  17  17  14  14  14  14  12  12  12  12  11  11  11  11   9   9   9   9   8   8   8   8   8   8   8   8   7   7   7   7   7   7   7   7   7   7   7   7   7   7   7   7   8   8   8   8   8   8   8   8   9   9   9   9  11  11  11  11  12  12  12  12  14  14  14  14  16  16  16  16  18  18  18  18  22  22  22  22  25  25  25  25  28  28  28  28  32  32  32  32  37  37  37  37  43  43  43  43  47  47  47  47  53  53  53  53  57  57  57  57  66  66  66  66  71  71  71  71  78  78  78  78  86  86  86  86  95  95  95  95 104 104 104 104 114 114 114 114 125 125 125 125
114 114 114 114 104 104 104 104  95  95  95  95  86  86  86  86  78  78  78  78  71  71  71  71  66  66  66  66  57  57  57  57  51  51  51  51  47  47  47  47  41  41  41  41  36  36  36  36  31  31  31  31  27  27  27  27  24  24  24  24  20  20  20  20  18  18  18  18  15  15  15  15  13  13  13  13  11  11  11  11   9   9   9   9   8   8   8   8   7   7   7   7   6   6   6   6   5   5   5   5   5   5   5   5   5   5   5   5   5   5   5   5   6   6   6   6   7   7   7   7   8   8   8   8   9   9   9   9  11  11  11  11  12  12  12  12  14  14  14  14  17  17  17  17  19  19  19  19  24  24  24  24  26  26  26  26  30  30  30  30  36  36  36  36  40  40  40  40  44  44  44  44  50  50  50  50  56  56  56  56  62  62  62  62  69  69  69  69  77  77  77  77  85  85  85  85  93  93  93  93 102 102 102 102 111 111 111 111 122 122 122 122
112 112 112 112 102 102 102 102  93  93  93  93  86  86  86  86  78  78  78  78  69  69  69  69  62  62  62  62  56  56  56  56  50  50  50  50  44  44  44  44  40  40  40  40  35  35  35  35  30  30  30  30  26  26  26  26  23  23  23  23  19  19  19  19  16  16  16  16  14  14  14  14  12  12  12  12  10  10  10  10   8   8   8   8   7   7   7   7   5   5   5   5   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   5   5   5   5   6   6   6   6   8   8   8   8   9   9   9   9  11  11  11  11  13  13  13  13  16  16  16  16  18  18  18  18  22  22  22  22  25  25  25  25  28  28  28  28  33  33  33  33  38  38  38  38  44  44  44  44  50  50  50  50  54  54  54  54  61  61  61  61  67  67  67  67  76  76  76  76  82  82  82  82  91  91  91  91  99  99  99  99 109 109 109 109 119 119 119 119
111 111 111 111 102 102 102 102  93  93  93  93  84  84  84  84  76  76  76  76  69  69  69  69  62  62  62  62  56  56  56  56  50  50  50  50  44  44  44  44  38  38  38  38  33  33  33  33  28  28  28  28  25  25  25  25  22  22  22  22  18  18  18  18  15  15  15  15  13  13  13  13  11  11  11  11   9   9   9   9   7   7   7   7   5   5   5   5   4   4   4   4   4   4   4   4   4   4   4   4   3   3   3   3   3   3   3   3   3   3   3   3   4   4   4   4   4   4   4   4   5   5   5   5   7   7   7   7   8   8   8   8  10  10  10  10  12  12  12  12  15  15  15  15  18  18  18  18  20  20  20  20  24  24  24  24  28  28  28  28  32  32  32  32  37  37  37  37  43  43  43  43  48  48  48  48  53  53  53  53  59  59  59  59  67  67  67  67  75  75  75  75  82  82  82  82  89  89  89  89  99  99  99  99 109 109 109 109 117 117 117 117
109 109 109 109  99  99  99  99  91  91  91  91  82  82  82  82  76  76  76  76  67  67  67  67  61  61  61  61  54  54  54  54  48  48  48  48  43  43  43  43  37  37  37  37  32  32  32  32  28  28  28  28  24  24  24  24  20  20  20  20  18  18  18  18  14  14  14  14  12  12  12  12  10  10  10  10   8   8   8   8   6   6   6   6   4   4   4   4   4   4   4   4   3   3   3   3   2   2   2   2   2   2   2   2   2   2   2   2   2   2   2   2   3   3   3   3   4   4   4   4   4   4   4   4   6   6   6   6   8   8   8   8   9   9   9   9  12  12  12  12  14  14  14  14  17  17  17  17  19  19  19  19  24  24  24  24  27  27  27  27  31  31  31  31  36  36  36  36  41  41  41  41  47  47  47  47  53  53  53  53  59  59  59  59  66  66  66  66  73  73  73  73  80  80  80  80  88  88  88  88  99  99  99  99 106 106 106 106 117 117 117 117
109 109 109 109  99  99  99  99  91  91  91  91  82  82  82  82  75  75  75  75  67  67  67  67  59  59  59  59  53  53  53  53  48  48  48  48  43  43  43  43  37  37  37  37  32  32  32  32  27  27  27  27  24  24  24  24  20  20  20  20  17  17  17  17  14  14  14  14  12  12  12  12   9   9   9   9   8   8   8   8   6   6   6   6   4   4   4   4   4   4   4   4   3   3   3   3   2   2   2   2   1   1   1   1   1   1   1   1   1   1   1   1   2   2   2   2   4   4   4   4   4   4   4   4   5   5   5   5   7   7   7   7   9   9   9   9  11  11  11  11  13  13  13  13  16  16  16  16  19  19  19  19  23  23  23  23  26  26  26  26  31  31  31  31  36  36  36  36  41  41  41  41  46  46  46  46  51  51  51  51  57  57  57  57  66  66  66  66  73  73  73  73  80  80  80  80  88  88  88  88  97  97  97  97 106 106 106 106 117 117 117 117
109 109 109 109  99  99  99  99  91  91  91  91  82  82  82  82  75  75  75  75  67  67  67  67  59  59  59  59  53  53  53  53  47  47  47  47  43  43  43  43  36  36  36  36  32  32  32  32  27  27  27  27  24  24  24  24  19  19  19  19  17  17  17  17  14  14  14  14  12  12  12  12   9   9   9   9   7   7   7   7   5   5   5   5   4   4   4   4   4   4   4   4   2   2   2   2   1   1   1   1   0   0   0   0   0   0   0   0   1   1   1   1   2   2   2   2   3   3   3   3   4   4   4   4   5   5   5   5   7   7   7   7   9   9   9   9  11  11  11  11  13  13  13  13  16  16  16  16  19  19  19  19  23  23  23  23  26  26  26  26  30  30  30  30  36  36  36  36  41  41  41  41  45  45  45  45  51  51  51  51  57  57  57  57  66  66  66  66  73  73  73  73  80  80  80  80  88  88  88  88  97  97  97  97 106 106 106 106 117 117 117 117
109 109 109 109  99  99  99  99  91  91  91  91  82  82  82  82  75  75  75  75  67  67  67  67  59  59  59  59  53  53  53  53  48  48  48  48  43  43  43  43  36  36  36  36  32  32  32  32  27  27  27  27  24  24  24  24  19  19  19  19  17  17  17  17  14  14  14  14  12  12  12  12   9   9   9   9   8   8   8   8   5   5   5   5   4   4   4   4   4   4   4   4   2   2   2   2   1   1   1   1   1   1   1   1   0   0   0   0   1   1   1   1   2   2   2   2   3   3   3   3   4   4   4   4   5   5   5   5   7   7   7   7   9   9   9   9  11  11  11  11  13  13  13  13  16  16  16  16  19  19  19  19  23  23  23  23  26  26  26  26  30  30  30  30  36  36  36  36  41  41  41  41  45  45  45  45  51  51  51  51  57  57  57  57  66  66  66  66  73  73  73  73  80  80  80  80  88  88  88  88  97  97  97  97 106 106 106 106 117 117 117 117
109 109 109 109  99  99  99  99  91  91  91  91  82  82  82  82  75  75  75  75  67  67  67  67  60  60  60  60  54  54  54  54  48  48  48  48  43  43  43  43  37  37  37  37  32  32  32  32  28  28  28  28  24  24  24  24  20  20  20  20  17  17  17  17  14  14  14  14  12  12  12  12   9   9   9   9   8   8   8   8   6   6   6   6   4   4   4   4   4   4   4   4   3   3   3   3   2   2   2   2   1   1   1   1   1   1   1   1   2   2   2   2   3   3   3   3   4   4   4   4   4   4   4   4   5   5   5   5   7   7   7   7   9   9   9   9  11  11  11  11  13  13  13  13  16  16  16  16  19  19  19  19  23  23  23  23  27  27  27  27  31  31  31  31  36  36  36  36  41  41  41  41  47  47  47  47  52  52  52  52  58  58  58  58  66  66  66  66  73  73  73  73  80  80  80  80  88  88  88  88  97  97  97  97 106 106 106 106 117 117 117 117
111 111 111 111 101 101 101 101  91  91  91  91  83  83  83  83  76  76  76  76  67  67  67  67  61  61  61  61  54  54  54  54  48  48  48  48  43  43  43  43  37  37  37  37  33  33  33  33  28  28  28  28  24  24  24  24  21  21  21  21  18  18  18  18  15  15  15  15  12  12  12  12  10  10  10  10   8   8   8   8   7   7   7   7   5   5   5   5   4   4   4   4   4   4   4   4   3   3   3   3   3   3   3   3   2   2   2   2   3   3   3   3   4   4   4   4   4   4   4   4   4   4   4   4   6   6   6   6   8   8   8   8  10  10  10  10  12  12  12  12  14  14  14  14  17  17  17  17  20  20  20  20  24  24  24  24  27  27  27  27  32  32  32  32  36  36  36  36  43  43  43  43  47  47  47  47  53  53  53  53  59  59  59  59  67  67  67  67  74  74  74  74  80  80  80  80  88  88  88  88  99  99  99  99 106 106 106 106 117 117 117 117
111 111 111 111 102 102 102 102  93  93  93  93  84  84  84  84  76  76  76  76  69  69  69  69  62  62  62  62  56  56  56  56  50  50  50  50  44  44  44  44  38  38  38  38  35  35  35  35  30  30  30  30  25  25  25  25  22  22  22  22  18  18  18  18  16  16  16  16  13  13  13  13  11  11  11  11   9   9   9   9   8   8   8   8   6   6   6   6   5   5   5   5   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   6   6   6   6   7   7   7   7   9   9   9   9  11  11  11  11  13  13  13  13  15  15  15  15  18  18  18  18  22  22  22  22  25  25  25  25  28  28  28  28  33  33  33  33  37  37  37  37  43  43  43  43  48  48  48  48  54  54  54  54  61  61  61  61  67  67  67  67  75  75  75  75  82  82  82  82  91  91  91  91  99  99  99  99 109 109 109 109 118 118 118 118
114 114 114 114 102 102 102 102  95  95  95  95  86  86  86  86  78  78  78  78  71  71  71  71  64  64  64  64  57  57  57  57  51  51  51  51  45  45  45  45  40  40  40  40  36  36  36  36  31  31  31  31  27  27  27  27  24  24  24  24  19  19  19  19  17  17  17  17  14  14  14  14  12  12  12  12  10  10  10  10   9   9   9   9   7   7   7   7   6   6   6   6   5   5   5   5   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   4   5   5   5   5   6   6   6   6   7   7   7   7   8   8   8   8  10  10  10  10  12  12  12  12  14  14  14  14  16  16  16  16  19  19  19  19  23  23  23  23  26  26  26  26  30  30  30  30  35  35  35  35  38  38  38  38  44  44  44  44  50  50  50  50  56  56  56  56  62  62  62  62  69  69  69  69  76  76  76  76  84  84  84  84  93  93  93  93 102 102 102 102 111 111 111 111 119 119 119 119
114 114 114 114 104 104 104 104  97  97  97  97  88  88  88  88  80  80  80  80  73  73  73  73  66  66  66  66  59  59  59  59  53  53  53  53  47  47  47  47  43  43  43  43  37  37  37  37  32  32  32  32  28  28  28  28  25  25  25  25  22  22  22  22  18  18  18  18  16  16  16  16  13  13  13  13  12  12  12  12  10  10  10  10   9   9   9   9   8   8   8   8   7   7   7   7   6   6   6   6   6   6   6   6   6   6   6   6   6   6   6   6   7   7   7   7   8   8   8   8   8   8   8   8  10  10  10  10  11  11  11  11  13  13  13  13  15  15  15  15  18  18  18  18  20  20  20  20  24  24  24  24  27  27  27  27  31  31  31  31  36  36  36  36  41  41  41  41  45  45  45  45  51  51  51  51  57  57  57  57  64  64  64  64  71  71  71  71  78  78  78  78  86  86  86  86  95  95  95  95 102 102 102 102 114 114 114 114 122 122 122 122
117 117 117 117 107 107 107 107  99  99  99  99  90  90  90  90  82  82  82  82  75  75  75  75  67  67  67  67  61  61  61  61  54  54  54  54  50  50  50  50  44  44  44  44  38  38  38  38  35  35  35  35  30  30  30  30  26  26  26  26  24  24  24  24  20  20  20  20  18  18  18  18  15  15  15  15  13  13  13  13  12  12  12  12  10  10  10  10   9   9   9   9   8   8   8   8   8   8   8   8   8   8   8   8   8   8   8   8   8   8   8   8   8   8   8   8   9   9   9   9  10  10  10  10  12  12  12  12  13  13  13  13  15  15  15  15  17  17  17  17  19  19  19  19  23  23  23  23  26  26  26  26  30  30  30  30  33  33  33  33  37  37  37  37  43  43  43  43  48  48  48  48  53  53  53  53  59  59  59  59  67  67  67  67  73  73  73  73  80  80  80  80  88  88  88  88  97  97  97  97 104 104 104 104 114 114 114 114 125 125 125 125
119 119 119 119 111 111 111 111 102 102 102 102  93  93  93  93  85  85  85  85  78  78  78  78  69  69  69  69  64  64  64  64  57  57  57  57  51  51  51  51  47  47  47  47  41  41  41  41  37  37  37  37  32  32  32  32  28  28  28  28  25  25  25  25  23  23  23  23  19  19  19  19  18  18  18  18  15  15  15  15  13  13  13  13  12  12  12  12  11  11  11  11  10  10  10  10  10  10  10  10   9   9   9   9   9   9   9   9  10  10  10  10  10  10  10  10  11  11  11  11  12  12  12  12  13  13  13  13  15  15  15  15  17  17  17  17  19  19  19  19  22  22  22  22  25  25  25  25  28  28  28  28  31  31  31  31  36  36  36  36  40  40  40  40  45  45  45  45  50  50  50  50  56  56  56  56  62  62  62  62  69  69  69  69  76  76  76  76  82  82  82  82  91  91  91  91  99  99  99  99 109 109 109 109 117 117 117 117 127 127 127 127
123 123 123 123 114 114 114 114 104 104 104 104  95  95  95  95  87  87  87  87  80  80  80  80  73  73  73  73  67  67  67  67  59  59  59  59  54  54  54  54  50  50  50  50  44  44  44  44  40  40  40  40  36  36  36  36  31  31  31  31  28  28  28  28  25  25  25  25  23  23  23  23  19  19  19  19  18  18  18  18  16  16  16  16  14  14  14  14  13  13  13  13  12  12  12  12  12  12  12  12  12  12  12  12  12  12  12  12  12  12  12  12  12  12  12  12  13  13  13  13  14  14  14  14  16  16  16  16  17  17  17  17  19  19  19  19  22  22  22  22  24  24  24  24  27  27  27  27  30  30  30  30  35  35  35  35  38  38  38  38  43  43  43  43  48  48  48  48  53  53  53  53  58  58  58  58  66  66  66  66  71  71  71  71  78  78  78  78  86  86  86  86  93  93  93  93 102 102 102 102 111 111 111 111 119 119 119 119 130 130 130 130
127 127 127 127 117 117 117 117 109 109 109 109  99  99  99  99  91  91  91  91  84  84  84  84  76  76  76  76  69  69  69  69  64  64  64  64  57  57  57  57  51  51  51  51  47  47  47  47  43  43  43  43  38  38  38  38  35  35  35  35  31  31  31  31  28  28  28  28  25  25  25  25  23  23  23  23  20  20  20  20  18  18  18  18  17  17  17  17  16  16  16  16  15  15  15  15  14  14  14  14  14  14  14  14  14  14  14  14  14  14  14  14  15  15  15  15  16  16  16  16  17  17  17  17  18  18  18  18  19  19  19  19  23  23  23  23  24  24  24  24  27  27  27  27  30  30  30  30  33  33  33  33  37  37  37  37  41  41  41  41  45  45  45  45  51  51  51  51  56  56  56  56  62  62  62  62  67  67  67  67  75  75  75  75  82  82  82  82  88  88  88  88  97  97  97  97 105 105 105 105 114 114 114 114 125 125 125 125 133 133 133 133
130 130 130 130 121 121 121 121 111 111 111 111 102 102 102 102  95  95  95  95  86  86  86  86  80  80  80  80  73  73  73  73  67  67  67  67  61  61  61  61  56  56  56  56  50  50  50  50  45  45  45  45  42  42  42  42  37  37  37  37  35  35  35  35  31  31  31  31  28  28  28  28  25  25  25  25  24  24  24  24  22  22  22  22  20  20  20  20  18  18  18  18  18  18  18  18  18  18  18  18  17  17  17  17  17  17  17  17  17  17  17  17  18  18  18  18  18  18  18  18  19  19  19  19  22  22  22  22  23  23  23  23  25  25  25  25  27  27  27  27  30  30  30  30  33  33  33  33  36  36  36  36  41  41  41  41  44  44  44  44  50  50  50  50  54  54  54  54  59  59  59  59  66  66  66  66  71  71  71  71  78  78  78  78  86  86  86  86  93  93  93  93 102 102 102 102 109 109 109 109 118 118 118 118 127 127 127 127 137 137 137 137
133 133 133 133 125 125 125 125 117 117 117 117 106 106 106 106  99  99  99  99  91  91  91  91  84  84  84  84  78  78  78  78  71  71  71  71  66  66  66  66  59  59  59  59  54  54  54  54  50  50  50  50  45  45  45  45  41  41  41  41  37  37  37  37  35  35  35  35  31  31  31  31  28  28  28  28  27  27  27  27  25  25  25  25  24  24  24  24  23  23  23  23  22  22  22  22  20  20  20  20  20  20  20  20  20  20  20  20  20  20  20  20  22  22  22  22  23  23  23  23  24  24  24  24  24  24  24  24  26  26  26  26  28  28  28  28  31  31  31  31  33  33  33  33  37  37  37  37  40  40  40  40  44  44  44  44  48  48  48  48  53  53  53  53  57  57  57  57  64  64  64  64  69  69  69  69  76  76  76  76  82  82  82  82  88  88  88  88  97  97  97  97 104 104 104 104 114 114 114 114 122 122 122 122 130 130 130 130 142 142 142 142
139 139 139 139 128 128 128 128 119 119 119 119 112 112 112 112 102 102 102 102  95  95  95  95  88  88  88  88  81  81  81  81  76  76  76  76  69  69  69  69  64  64  64  64  57  57  57  57  53  53  53  53  50  50  50  50  45  45  45  45  43  43  43  43  38  38  38  38  36  36  36  36  33  33  33  33  30  30  30  30  28  28  28  28  27  27  27  27  26  26  26  26  25  25  25  25  24  24  24  24  24  24  24  24  24  24  24  24  24  24  24  24  25  25  25  25  25  25  25  25  27  27  27  27  28  28  28  28  30  30  30  30  32  32  32  32  35  35  35  35  37  37  37  37  41  41  41  41  44  44  44  44  48  48  48  48  53  53  53  53  57  57  57  57  62  62  62  62  67  67  67  67  74  74  74  74  80  80  80  80  86  86  86  86  93  93  93  93 102 102 102 102 109 109 109 109 117 117 117 117 127 127 127 127 136 136 136 136 146 146 146 146
146 146 146 146 133 133 133 133 125 125 125 125 117 117 117 117 109 109 109 109 102 102 102 102  93  93  93  93  86  86  86  86  79  79  79  79  75  75  75  75  67  67  67  67  62  62  62  62  57  57  57  57  53  53  53  53  50  50  50  50  45  45  45  45  43  43  43  43  40  40  40  40  37  37  37  37  35  35  35  35  33  33  33  33  31  31  31  31  30  30  30  30  28  28  28  28  28  28  28  28  28  28  28  28  28  28  28  28  28  28  28  28  28  28  28  28  30  30  30  30  31  31  31  31  32  32  32  32  35  35  35  35  36  36  36  36  38  38  38  38  43  43  43  43  45  45  45  45  48  48  48  48  53  53  53  53  57  57  57  57  62  62  62  62  67  67  67  67  73  73  73  73  78  78  78  78  84  84  84  84  91  91  91  91  99  99  99  99 106 106 106 106 114 114 114 114 125 125 125 125 130 130 130 130 142 142 142 142 152 152 152 152
149 149 149 149 139 139 139 139 130 130 130 130 122 122 122 122 114 114 114 114 106 106 106 106  99  99  99  99  91  91  91  91  85  85  85  85  78  78  78  78  73  73  73  73  67  67  67  67  62  62  62  62  57  57  57  57  54  54  54  54  51  51  51  51  47  47  47  47  44  44  44  44  43  43  43  43  40  40  40  40  37  37  37  37  36  36  36  36  35  35  35  35  33  33  33  33  33  33  33  33  32  32  32  32  32  32  32  32  32  32  32  32  33  33  33  33  35  35  35  35  36  36  36  36  37  37  37  37  38  38  38  38  41  41  41  41  44  44  44  44  47  47  47  47  50  50  50  50  53  53  53  53  57  57  57  57  62  62  62  62  67  67  67  67  71  71  71  71  78  78  78  78  83  83  83  83  88  88  88  88  97  97  97  97 104 104 104 104 112 112 112 112 119 119 119 119 127 127 127 127 138 138 138 138 149 149 149 149 159 159 159 159
156 156 156 156 146 146 146 146 136 136 136 136 127 127 127 127 119 119 119 119 111 111 111 111 104 104 104 104  97  97  97  97  91  91  91  91  84  84  84  84  78  78  78  78  73  73  73  73  68  68  68  68  64  64  64  64  59  59  59  59  56  56  56  56  52  52  52  52  50  50  50  50  47  47  47  47  44  44  44  44  43  43  43  43  41  41  41  41  40  40  40  40  38  38  38  38  37  37  37  37  37  37  37  37  37  37  37  37  37  37  37  37  38  38  38  38  38  38  38  38  40  40  40  40  43  43  43  43  44  44  44  44  45  45  45  45  48  48  48  48  51  51  51  51  54  54  54  54  57  57  57  57  62  62  62  62  67  67  67  67  72  72  72  72  77  77  77  77  82  82  82  82  88  88  88  88  95  95  95  95 102 102 102 102 109 109 109 109 117 117 117 117 126 126 126 126 133 133 133 133 146 146 146 146 152 152 152 152 163 163 163 163
163 163 163 163 152 152 152 152 145 145 145 145 133 133 133 133 125 125 125 125 117 117 117 117 111 111 111 111 102 102 102 102  97  97  97  97  89  89  89  89  84  84  84  84  78  78  78  78  75  75  75  75  69  69  69  69  66  66  66  66  61  61  61  61  57  57  57  57  54  54  54  54  51  51  51  51  50  50  50  50  48  48  48  48  45  45  45  45  44  44  44  44  44  44  44  44  43  43  43  43  43  43  43  43  43  43  43  43  43  43  43  43  44  44  44  44  44  44  44  44  45  45  45  45  47  47  47  47  50  50  50  50  51  51  51  51  54  54  54  54  57  57  57  57  60  60  60  60  64  64  64  64  68  68  68  68  73  73  73  73  78  78  78  78  82  82  82  82  88  88  88  88  95  95  95  95 102 102 102 102 109 109 109 109 117 117 117 117 125 125 125 125 130 130 130 130 142 142 142 142 149 149 149 149 159 159 159 159 170 170 170 170
170 170 170 170 159 159 159 159 149 149 149 149 142 142 142 142 130 130 130 130 125 125 125 125 117 117 117 117 109 109 109 109 102 102 102 102  97  97  97  97  91  91  91  91  86  86  86  86  80  80  80  80  76  76  76  76  71  71  71  71  67  67  67  67  64  64  64  64  61  61  61  61  57  57  57  57  56  56  56  56  53  53  53  53  51  51  51  51  50  50  50  50  50  50  50  50  48  48  48  48  48  48  48  48  48  48  48  48  48  48  48  48  50  50  50  50  50  50  50  50  51  51  51  51  53  53  53  53  54  54  54  54  57  57  57  57  59  59  59  59  62  62  62  62  67  67  67  67  69  69  69  69  75  75  75  75  78  78  78  78  84  84  84  84  88  88  88  88  95  95  95  95 102 102 102 102 108 108 108 108 114 114 114 114 122 122 122 122 130 130 130 130 139 139 139 139 149 149 149 149 156 156 156 156 166 166 166 166 175 175 175 175
174 174 174 174 166 166 166 166 156 156 156 156 149 149 149 149 139 139 139 139 130 130 130 130 125 125 125 125 117 117 117 117 109 109 109 109 102 102 102 102  97  97  97  97  91  91  91  91  86  86  86  86  82  82  82  82  78  78  78  78  74  74  74  74  69  69  69  69  67  67  67  67  64  64  64  64  61  61  61  61  59  59  59  59  57  57  57  57  56  56  56  56  56  56  56  56  54  54  54  54  54  54  54  54  54  54  54  54  54  54  54  54  55  55  55  55  56  56  56  56  57  57  57  57  59  59  59  59  61  61  61  61  64  64  64  64  67  67  67  67  69  69  69  69  73  73  73  73  76  76  76  76  80  80  80  80  86  86  86  86  91  91  91  91  95  95  95  95 102 102 102 102 109 109 109 109 114 114 114 114 122 122 122 122 127 127 127 127 136 136 136 136 146 146 146 146 155 155 155 155 166 166 166 166 174 174 174 174 182 182 182 182
182 182 182 182 174 174 174 174 166 166 166 166 156 156 156 156 146 146 146 146 139 139 139 139 130 130 130 130 125 125 125 125 117 117 117 117 111 111 111 111 104 104 104 104  99  99  99  99  93  93  93  93  88  88  88  88  84  84  84  84  80  80  80  80  76  76  76  76  74  74  74  74  71  71  71  71  68  68  68  68  67  67  67  67  64  64  64  64  62  62  62  62  62  62  62  62  61  61  61  61  61  61  61  61  61  61  61  61  61  61  61  61  62  62  62  62  62  62  62  62  64  64  64  64  66  66  66  66  67  67  67  67  69  69  69  69  73  73  73  73  76  76  76  76  78  78  78  78  83  83  83  83  86  86  86  86  93  93  93  93  97  97  97  97 102 102 102 102 109 109 109 109 114 114 114 114 122 122 122 122 127 127 127 127 136 136 136 136 146 146 146 146 152 152 152 152 163 163 163 163 170 170 170 170 182 182 182 182 190 190 190 190

                }
            }
            </rawfe_lsc_dcc>
        </parameter_package>
    </use_case>
    <!--=====================================================================-->
</RAWFE_cfg_lsc_xml>
<?xml version="1.0" encoding="utf-8"?>
<RAWFE_cfg_lsc_ext_xml xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance" xmlns:xsd="http://www.w3.org/2001/XMLSchema">
  <!--this is a comment-->
    <dcc_name>rawfe_cfg_lsc_extension</dcc_name>
    <dcc_header>
		<camera_module_id> 219 </camera_module_id>
	    <dcc_descriptor_id> 37 </dcc_descriptor_id>
	    <algorithm_vendor_id>  1 </algorithm_vendor_id>
	    <tunning_tool_version> 0 </tunning_tool_version>
    </dcc_header>
  <!--=======================================================================-->
    <typedef>
		<cfg_rawfe_lsc_ext type="struct">
			<lsc_cfg_mode type="uint32"> </lsc_cfg_mode>
			<lsc_ch2lut_map type="uint8[16]"> </lsc_ch2lut_map>
        </cfg_rawfe_lsc_ext>
    </typedef>

<!--=======================================================================-->
    
    <use_case val="1023">
        <n-space>
		
            <region0 class="0">
				<colortemperature val="2" min="0" max="20000">  </colortemperature>
				<exposure val="1" min="0" max="10000000">  </exposure>
				<gain val="0" min="0" max="1024">  </gain>
			</region0>
		
		</n-space>
		

    <parameter_package>
        <rawfe_lsc_ext_dcc type="cfg_rawfe_lsc_ext">
        {
            0,           // lsc_cfg_mode
            {             // lsc_ch2lut_map
                0, 1, 2, 1,
                1, 3, 1, 3,
                2, 1, 0, 1,
                1, 3, 1, 3,
            }
        }
        </rawfe_lsc_ext_dcc>
    </parameter_package>
    
</use_case>

<!--=====================================================================-->
</RAWFE_cfg_lsc_ext_xml>
0.00112	1
0.00224	1
0.00336	1
0.00448	1
0.0056	1
0.00672	1
0.00784	1
0.00896	1
0.01008	1
0.0112	1
0.01232	1
0.01344	1
0.01456	1
0.01568	1
0.0168	1
0.01792	1
0.01904	1
0.02016	1
0.02128	1
0.0224	1
0.02352	1
0.02464	1
0.02576	1
0.02688	1
0.028	1
0.02912	1
0.03024	1
0.03136	1
0.03248	0.993975903614458
0.0336	0.993975903614458
0.03472	0.993975903614458
0.03584	0.993975903614458
0.03696	0.993975903614458
0.03808	0.993975903614458
0.0392	0.993975903614458
0.04032	0.993975903614458
0.04144	0.993975903614458
0.04256	0.993975903614458
0.04368	0.993975903614458
0.0448	0.993975903614458
0.04592	0.993975903614458
0.04704	0.993975903614458
0.04816	0.993975903614458
0.04928	0.993975903614458
0.0504	0.993975903614458
0.05152	0.993975903614458
0.05264	0.993975903614458
0.05376	0.993975903614458
0.05488	0.993975903614458
0.056	0.993975903614458
0.05712	0.993975903614458
0.05824	0.993975903614458
0.05936	0.993975903614458
0.06048	0.993975903614458
0.0616	0.993975903614458
0.06272	0.993975903614458
0.06384	0.993975903614458
0.06496	0.993975903614458
0.06608	0.993975903614458
0.0672	0.993975903614458
0.06832	0.993975903614458
0.06944	0.993975903614458
0.07056	0.993975903614458
0.07168	0.987951807228916
0.0728	0.987951807228916
0.07392	0.987951807228916
0.07504	0.987951807228916
0.07616	0.987951807228916
0.07728	0.987951807228916
0.0784	0.987951807228916
0.07952	0.987951807228916
0.08064	0.987951807228916
0.08176	0.987951807228916
0.08288	0.987951807228916
0.084	0.987951807228916
0.08512	0.987951807228916
0.08624	0.987951807228916
0.08736	0.987951807228916
0.08848	0.987951807228916
0.0896	0.987951807228916
0.09072	0.987951807228916
0.09184	0.987951807228916
0.09296	0.987951807228916
0.09408	0.987951807228916
0.0952	0.987951807228916
0.09632	0.987951807228916
0.09744	0.987951807228916
0.09856	0.987951807228916
0.09968	0.987951807228916
0.1008	0.981927710843374
0.10192	0.981927710843374
0.10304	0.981927710843374
0.10416	0.981927710843374
0.10528	0.981927710843374
0.1064	0.981927710843374
0.10752	0.981927710843374
0.10864	0.981927710843374
0.10976	0.981927710843374
0.11088	0.981927710843374
0.112	0.981927710843374
0.11312	0.981927710843374
0.11424	0.981927710843374
0.11536	0.981927710843374
0.11648	0.981927710843374
0.1176	0.981927710843374
0.11872	0.981927710843374
0.11984	0.981927710843374
0.12096	0.981927710843374
0.12208	0.981927710843374
0.1232	0.981927710843374
0.12432	0.981927710843374
0.12544	0.981927710843374
0.12656	0.975903614457831
0.12768	0.975903614457831
0.1288	0.975903614457831
0.12992	0.975903614457831
0.13104	0.975903614457831
0.13216	0.975903614457831
0.13328	0.975903614457831
0.1344	0.975903614457831
0.13552	0.975903614457831
0.13664	0.975903614457831
0.13776	0.975903614457831
0.13888	0.975903614457831
0.14	0.975903614457831
0.14112	0.975903614457831
0.14224	0.975903614457831
0.14336	0.975903614457831
0.14448	0.975903614457831
0.1456	0.975903614457831
0.14672	0.975903614457831
0.14784	0.975903614457831
0.14896	0.975903614457831
0.15008	0.975903614457831
0.1512	0.975903614457831
0.15232	0.975903614457831
0.15344	0.975903614457831
0.15456	0.975903614457831
0.15568	0.969879518072289
0.1568	0.969879518072289
0.15792	0.969879518072289
0.15904	0.969879518072289
0.16016	0.969879518072289
0.16128	0.969879518072289
0.1624	0.969879518072289
0.16352	0.969879518072289
0.16464	0.969879518072289
0.16576	0.969879518072289
0.16688	0.969879518072289
0.168	0.969879518072289
0.16912	0.969879518072289
0.17024	0.969879518072289
0.17136	0.969879518072289
0.17248	0.969879518072289
0.1736	0.969879518072289
0.17472	0.969879518072289
0.17584	0.969879518072289
0.17696	0.969879518072289
0.17808	0.969879518072289
0.1792	0.969879518072289
0.18032	0.969879518072289
0.18144	0.969879518072289
0.18256	0.969879518072289
0.18368	0.969879518072289
0.1848	0.969879518072289
0.18592	0.969879518072289
0.18704	0.963855421686747
0.18816	0.963855421686747
0.18928	0.963855421686747
0.1904	0.963855421686747
0.19152	0.963855421686747
0.19264	0.963855421686747
0.19376	0.963855421686747
0.19488	0.963855421686747
0.196	0.963855421686747
0.19712	0.963855421686747
0.19824	0.963855421686747
0.19936	0.963855421686747
0.20048	0.963855421686747
0.2016	0.963855421686747
0.20272	0.963855421686747
0.20384	0.963855421686747
0.20496	0.957831325301205
0.20608	0.957831325301205
0.2072	0.957831325301205
0.20832	0.957831325301205
0.20944	0.957831325301205
0.21056	0.957831325301205
0.21168	0.957831325301205
0.2128	0.957831325301205
0.21392	0.957831325301205
0.21504	0.957831325301205
0.21616	0.957831325301205
0.21728	0.957831325301205
0.2184	0.957831325301205
0.21952	0.957831325301205
0.22064	0.957831325301205
0.22176	0.951807228915663
0.22288	0.951807228915663
0.224	0.951807228915663
0.22512	0.951807228915663
0.22624	0.951807228915663
0.22736	0.951807228915663
0.22848	0.951807228915663
0.2296	0.951807228915663
0.23072	0.951807228915663
0.23184	0.951807228915663
0.23296	0.951807228915663
0.23408	0.951807228915663
0.2352	0.951807228915663
0.23632	0.951807228915663
0.23744	0.951807228915663
0.23856	0.951807228915663
0.23968	0.94578313253012
0.2408	0.94578313253012
0.24192	0.94578313253012
0.24304	0.94578313253012
0.24416	0.94578313253012
0.24528	0.94578313253012
0.2464	0.94578313253012
0.24752	0.94578313253012
0.24864	0.94578313253012
0.24976	0.94578313253012
0.25088	0.94578313253012
0.252	0.94578313253012
0.25312	0.94578313253012
0.25424	0.94578313253012
0.25536	0.94578313253012
0.25648	0.94578313253012
0.2576	0.94578313253012
0.25872	0.94578313253012
0.25984	0.94578313253012
0.26096	0.94578313253012
0.26208	0.94578313253012
0.2632	0.94578313253012
0.26432	0.939759036144578
0.26544	0.939759036144578
0.26656	0.939759036144578
0.26768	0.939759036144578
0.2688	0.939759036144578
0.26992	0.939759036144578
0.27104	0.939759036144578
0.27216	0.939759036144578
0.27328	0.939759036144578
0.2744	0.939759036144578
0.27552	0.939759036144578
0.27664	0.939759036144578
0.27776	0.939759036144578
0.27888	0.939759036144578
0.28	0.939759036144578
0.28112	0.933734939759036
0.28224	0.933734939759036
0.28336	0.933734939759036
0.28448	0.933734939759036
0.2856	0.933734939759036
0.28672	0.933734939759036
0.28784	0.933734939759036
0.28896	0.933734939759036
0.29008	0.933734939759036
0.2912	0.933734939759036
0.29232	0.933734939759036
0.29344	0.933734939759036
0.29456	0.927710843373494
0.29568	0.927710843373494
0.2968	0.927710843373494
0.29792	0.927710843373494
0.29904	0.927710843373494
0.30016	0.927710843373494
0.30128	0.927710843373494
0.3024	0.927710843373494
0.30352	0.927710843373494
0.30464	0.927710843373494
0.30576	0.927710843373494
0.30688	0.927710843373494
0.308	0.927710843373494
0.30912	0.921686746987952
0.31024	0.921686746987952
0.31136	0.921686746987952
0.31248	0.921686746987952
0.3136	0.921686746987952
0.31472	0.921686746987952
0.31584	0.921686746987952
0.31696	0.921686746987952
0.31808	0.921686746987952
0.3192	0.921686746987952
0.32032	0.921686746987952
0.32144	0.921686746987952
0.32256	0.921686746987952
0.32368	0.921686746987952
0.3248	0.921686746987952
0.32592	0.921686746987952
0.32704	0.921686746987952
0.32816	0.921686746987952
0.32928	0.91566265060241
0.3304	0.91566265060241
0.33152	0.91566265060241
0.33264	0.91566265060241
0.33376	0.91566265060241
0.33488	0.91566265060241
0.336	0.91566265060241
0.33712	0.91566265060241
0.33824	0.91566265060241
0.33936	0.91566265060241
0.34048	0.91566265060241
0.3416	0.91566265060241
0.34272	0.91566265060241
0.34384	0.91566265060241
0.34496	0.909638554216868
0.34608	0.909638554216868
0.3472	0.909638554216868
0.34832	0.909638554216868
0.34944	0.909638554216868
0.35056	0.909638554216868
0.35168	0.909638554216868
0.3528	0.909638554216868
0.35392	0.909638554216868
0.35504	0.909638554216868
0.35616	0.903614457831325
0.35728	0.903614457831325
0.3584	0.903614457831325
0.35952	0.903614457831325
0.36064	0.903614457831325
0.36176	0.903614457831325
0.36288	0.903614457831325
0.364	0.903614457831325
0.36512	0.903614457831325
0.36624	0.903614457831325
0.36736	0.897590361445783
0.36848	0.897590361445783
0.3696	0.897590361445783
0.37072	0.897590361445783
0.37184	0.897590361445783
0.37296	0.897590361445783
0.37408	0.897590361445783
0.3752	0.897590361445783
0.37632	0.897590361445783
0.37744	0.897590361445783
0.37856	0.891566265060241
0.37968	0.891566265060241
0.3808	0.891566265060241
0.38192	0.891566265060241
0.38304	0.891566265060241
0.38416	0.891566265060241
0.38528	0.891566265060241
0.3864	0.891566265060241
0.38752	0.891566265060241
0.38864	0.891566265060241
0.38976	0.885542168674699
0.39088	0.885542168674699
0.392	0.885542168674699
0.39312	0.885542168674699
0.39424	0.885542168674699
0.39536	0.885542168674699
0.39648	0.885542168674699
0.3976	0.885542168674699
0.39872	0.885542168674699
0.39984	0.885542168674699
0.40096	0.885542168674699
0.40208	0.885542168674699
0.4032	0.885542168674699
0.40432	0.885542168674699
0.40544	0.885542168674699
0.40656	0.885542168674699
0.40768	0.879518072289157
0.4088	0.879518072289157
0.40992	0.879518072289157
0.41104	0.879518072289157
0.41216	0.879518072289157
0.41328	0.879518072289157
0.4144	0.879518072289157
0.41552	0.879518072289157
0.41664	0.879518072289157
0.41776	0.879518072289157
0.41888	0.873493975903614
0.42	0.873493975903614
0.42112	0.873493975903614
0.42224	0.873493975903614
0.42336	0.873493975903614
0.42448	0.873493975903614
0.4256	0.873493975903614
0.42672	0.873493975903614
0.42784	0.873493975903614
0.42896	0.867469879518072
0.43008	0.867469879518072
0.4312	0.867469879518072
0.43232	0.867469879518072
0.43344	0.867469879518072
0.43456	0.867469879518072
0.43568	0.867469879518072
0.4368	0.867469879518072
0.43792	0.86144578313253
0.43904	0.86144578313253
0.44016	0.86144578313253
0.44128	0.86144578313253
0.4424	0.86144578313253
0.44352	0.86144578313253
0.44464	0.86144578313253
0.44576	0.86144578313253
0.44688	0.86144578313253
0.448	0.86144578313253
0.44912	0.855421686746988
0.45024	0.855421686746988
0.45136	0.855421686746988
0.45248	0.855421686746988
0.4536	0.855421686746988
0.45472	0.855421686746988
0.45584	0.855421686746988
0.45696	0.855421686746988
0.45808	0.855421686746988
0.4592	0.855421686746988
0.46032	0.855421686746988
0.46144	0.855421686746988
0.46256	0.855421686746988
0.46368	0.849397590361446
0.4648	0.849397590361446
0.46592	0.849397590361446
0.46704	0.849397590361446
0.46816	0.849397590361446
0.46928	0.849397590361446
0.4704	0.849397590361446
0.47152	0.849397590361446
0.47264	0.849397590361446
0.47376	0.843373493975904
0.47488	0.843373493975904
0.476	0.843373493975904
0.47712	0.843373493975904
0.47824	0.843373493975904
0.47936	0.843373493975904
0.48048	0.843373493975904
0.4816	0.843373493975904
0.48272	0.837349397590361
0.48384	0.837349397590361
0.48496	0.837349397590361
0.48608	0.837349397590361
0.4872	0.837349397590361
0.48832	0.837349397590361
0.48944	0.837349397590361
0.49056	0.837349397590361
0.49168	0.831325301204819
0.4928	0.831325301204819
0.49392	0.831325301204819
0.49504	0.831325301204819
0.49616	0.831325301204819
0.49728	0.831325301204819
0.4984	0.831325301204819
0.49952	0.831325301204819
0.50064	0.831325301204819
0.50176	0.831325301204819
0.50288	0.831325301204819
0.504	0.831325301204819
0.50512	0.825301204819277
0.50624	0.825301204819277
0.50736	0.825301204819277
0.50848	0.825301204819277
0.5096	0.825301204819277
0.51072	0.825301204819277
0.51184	0.825301204819277
0.51296	0.825301204819277
0.51408	0.825301204819277
0.5152	0.825301204819277
0.51632	0.819277108433735
0.51744	0.819277108433735
0.51856	0.819277108433735
0.51968	0.819277108433735
0.5208	0.819277108433735
0.52192	0.819277108433735
0.52304	0.819277108433735
0.52416	0.813253012048193
0.52528	0.813253012048193
0.5264	0.813253012048193
0.52752	0.813253012048193
0.52864	0.813253012048193
0.52976	0.813253012048193
0.53088	0.813253012048193
0.532	0.807228915662651
0.53312	0.807228915662651
0.53424	0.807228915662651
0.53536	0.807228915662651
0.53648	0.807228915662651
0.5376	0.807228915662651
0.53872	0.807228915662651
0.53984	0.801204819277108
0.54096	0.801204819277108
0.54208	0.801204819277108
0.5432	0.801204819277108
0.54432	0.801204819277108
0.54544	0.801204819277108
0.54656	0.801204819277108
0.54768	0.801204819277108
0.5488	0.795180722891566
0.54992	0.795180722891566
0.55104	0.795180722891566
0.55216	0.795180722891566
0.55328	0.795180722891566
0.5544	0.795180722891566
0.55552	0.795180722891566
0.55664	0.795180722891566
0.55776	0.795180722891566
0.55888	0.795180722891566
0.56	0.795180722891566
0.56112	0.795180722891566
0.56224	0.789156626506024
0.56336	0.789156626506024
0.56448	0.789156626506024
0.5656	0.789156626506024
0.56672	0.789156626506024
0.56784	0.789156626506024
0.56896	0.789156626506024
0.57008	0.789156626506024
0.5712	0.783132530120482
0.57232	0.783132530120482
0.57344	0.783132530120482
0.57456	0.783132530120482
0.57568	0.783132530120482
0.5768	0.783132530120482
0.57792	0.783132530120482
0.57904	0.77710843373494
0.58016	0.77710843373494
0.58128	0.77710843373494
0.5824	0.77710843373494
0.58352	0.77710843373494
0.58464	0.77710843373494
0.58576	0.77710843373494
0.58688	0.771084337349398
0.588	0.771084337349398
0.58912	0.771084337349398
0.59024	0.771084337349398
0.59136	0.771084337349398
0.59248	0.771084337349398
0.5936	0.771084337349398
0.59472	0.765060240963855
0.59584	0.765060240963855
0.59696	0.765060240963855
0.59808	0.765060240963855
0.5992	0.765060240963855
0.60032	0.765060240963855
0.60144	0.765060240963855
0.60256	0.765060240963855
0.60368	0.765060240963855
0.6048	0.759036144578313
0.60592	0.759036144578313
0.60704	0.759036144578313
0.60816	0.759036144578313
0.60928	0.759036144578313
0.6104	0.759036144578313
0.61152	0.759036144578313
0.61264	0.759036144578313
0.61376	0.759036144578313
0.61488	0.759036144578313
0.616	0.759036144578313
0.61712	0.753012048192771
0.61824	0.753012048192771
0.61936	0.753012048192771
0.62048	0.753012048192771
0.6216	0.753012048192771
0.62272	0.753012048192771
0.62384	0.753012048192771
0.62496	0.746987951807229
0.62608	0.746987951807229
0.6272	0.746987951807229
0.62832	0.746987951807229
0.62944	0.746987951807229
0.63056	0.746987951807229
0.63168	0.746987951807229
0.6328	0.740963855421687
0.63392	0.740963855421687
0.63504	0.740963855421687
0.63616	0.740963855421687
0.63728	0.740963855421687
0.6384	0.740963855421687
0.63952	0.740963855421687
0.64064	0.734939759036145
0.64176	0.734939759036145
0.64288	0.734939759036145
0.644	0.734939759036145
0.64512	0.734939759036145
0.64624	0.734939759036145
0.64736	0.734939759036145
0.64848	0.734939759036145
0.6496	0.734939759036145
0.65072	0.734939759036145
0.65184	0.728915662650602
0.65296	0.728915662650602
0.65408	0.728915662650602
0.6552	0.728915662650602
0.65632	0.728915662650602
0.65744	0.728915662650602
0.65856	0.728915662650602
0.65968	0.728915662650602
0.6608	0.728915662650602
0.66192	0.72289156626506
0.66304	0.72289156626506
0.66416	0.72289156626506
0.66528	0.72289156626506
0.6664	0.72289156626506
0.66752	0.72289156626506
0.66864	0.72289156626506
0.66976	0.716867469879518
0.67088	0.716867469879518
0.672	0.716867469879518
0.67312	0.716867469879518
0.67424	0.716867469879518
0.67536	0.716867469879518
0.67648	0.716867469879518
0.6776	0.710843373493976
0.67872	0.710843373493976
0.67984	0.710843373493976
0.68096	0.710843373493976
0.68208	0.710843373493976
0.6832	0.710843373493976
0.68432	0.710843373493976
0.68544	0.710843373493976
0.68656	0.704819277108434
0.68768	0.704819277108434
0.6888	0.704819277108434
0.68992	0.704819277108434
0.69104	0.704819277108434
0.69216	0.704819277108434
0.69328	0.704819277108434
0.6944	0.704819277108434
0.69552	0.704819277108434
0.69664	0.704819277108434
0.69776	0.698795180722892
0.69888	0.698795180722892
0.7	0.698795180722892
0.70112	0.698795180722892
0.70224	0.698795180722892
0.70336	0.698795180722892
0.70448	0.698795180722892
0.7056	0.698795180722892
0.70672	0.692771084337349
0.70784	0.692771084337349
0.70896	0.692771084337349
0.71008	0.692771084337349
0.7112	0.692771084337349
0.71232	0.692771084337349
0.71344	0.686746987951807
0.71456	0.686746987951807
0.71568	0.686746987951807
0.7168	0.686746987951807
0.71792	0.686746987951807
0.71904	0.686746987951807
0.72016	0.686746987951807
0.72128	0.680722891566265
0.7224	0.680722891566265
0.72352	0.680722891566265
0.72464	0.680722891566265
0.72576	0.680722891566265
0.72688	0.680722891566265
0.728	0.674698795180723
0.72912	0.674698795180723
0.73024	0.674698795180723
0.73136	0.674698795180723
0.73248	0.674698795180723
0.7336	0.674698795180723
0.73472	0.674698795180723
0.73584	0.668674698795181
0.73696	0.668674698795181
0.73808	0.668674698795181
0.7392	0.668674698795181
0.74032	0.668674698795181
0.74144	0.668674698795181
0.74256	0.668674698795181
0.74368	0.668674698795181
0.7448	0.668674698795181
0.74592	0.668674698795181
0.74704	0.662650602409639
0.74816	0.662650602409639
0.74928	0.662650602409639
0.7504	0.662650602409639
0.75152	0.662650602409639
0.75264	0.662650602409639
0.75376	0.662650602409639
0.75488	0.662650602409639
0.756	0.662650602409639
0.75712	0.662650602409639
0.75824	0.656626506024096
0.75936	0.656626506024096
0.76048	0.656626506024096
0.7616	0.656626506024096
0.76272	0.656626506024096
0.76384	0.656626506024096
0.76496	0.650602409638554
0.76608	0.650602409638554
0.7672	0.650602409638554
0.76832	0.650602409638554
0.76944	0.650602409638554
0.77056	0.650602409638554
0.77168	0.650602409638554
0.7728	0.644578313253012
0.77392	0.644578313253012
0.77504	0.644578313253012
0.77616	0.644578313253012
0.77728	0.644578313253012
0.7784	0.644578313253012
0.77952	0.63855421686747
0.78064	0.63855421686747
0.78176	0.63855421686747
0.78288	0.63855421686747
0.784	0.63855421686747
0.78512	0.63855421686747
0.78624	0.63855421686747
0.78736	0.63855421686747
0.78848	0.63855421686747
0.7896	0.632530120481928
0.79072	0.632530120481928
0.79184	0.632530120481928
0.79296	0.632530120481928
0.79408	0.632530120481928
0.7952	0.632530120481928
0.79632	0.632530120481928
0.79744	0.632530120481928
0.79856	0.632530120481928
0.79968	0.632530120481928
0.8008	0.632530120481928
0.80192	0.626506024096386
0.80304	0.626506024096386
0.80416	0.626506024096386
0.80528	0.626506024096386
0.8064	0.626506024096386
0.80752	0.626506024096386
0.80864	0.626506024096386
0.80976	0.620481927710843
0.81088	0.620481927710843
0.812	0.620481927710843
0.81312	0.620481927710843
0.81424	0.620481927710843
0.81536	0.620481927710843
0.81648	0.620481927710843
0.8176	0.614457831325301
0.81872	0.614457831325301
0.81984	0.614457831325301
0.82096	0.614457831325301
0.82208	0.614457831325301
0.8232	0.614457831325301
0.82432	0.608433734939759
0.82544	0.608433734939759
0.82656	0.608433734939759
0.82768	0.608433734939759
0.8288	0.608433734939759
0.82992	0.608433734939759
0.83104	0.608433734939759
0.83216	0.608433734939759
0.83328	0.608433734939759
0.8344	0.608433734939759
0.83552	0.608433734939759
0.83664	0.602409638554217
0.83776	0.602409638554217
0.83888	0.602409638554217
0.84	0.602409638554217
0.84112	0.602409638554217
0.84224	0.602409638554217
0.84336	0.602409638554217
0.84448	0.602409638554217
0.8456	0.602409638554217
0.84672	0.596385542168675
0.84784	0.596385542168675
0.84896	0.596385542168675
0.85008	0.596385542168675
0.8512	0.596385542168675
0.85232	0.596385542168675
0.85344	0.596385542168675
0.85456	0.590361445783132
0.85568	0.590361445783132
0.8568	0.590361445783132
0.85792	0.590361445783132
0.85904	0.590361445783132
0.86016	0.590361445783132
0.86128	0.590361445783132
0.8624	0.58433734939759
0.86352	0.58433734939759
0.86464	0.58433734939759
0.86576	0.58433734939759
0.86688	0.58433734939759
0.868	0.58433734939759
0.86912	0.58433734939759
0.87024	0.578313253012048
0.87136	0.578313253012048
0.87248	0.578313253012048
0.8736	0.578313253012048
0.87472	0.578313253012048
0.87584	0.578313253012048
0.87696	0.572289156626506
0.87808	0.572289156626506
0.8792	0.572289156626506
0.88032	0.572289156626506
0.88144	0.572289156626506
0.88256	0.572289156626506
0.88368	0.572289156626506
0.8848	0.572289156626506
0.88592	0.572289156626506
0.88704	0.572289156626506
0.88816	0.566265060240964
0.88928	0.566265060240964
0.8904	0.566265060240964
0.89152	0.566265060240964
0.89264	0.566265060240964
0.89376	0.566265060240964
0.89488	0.566265060240964
0.896	0.566265060240964
0.89712	0.566265060240964
0.89824	0.566265060240964
0.89936	0.566265060240964
0.90048	0.560240963855422
0.9016	0.560240963855422
0.90272	0.560240963855422
0.90384	0.560240963855422
0.90496	0.560240963855422
0.90608	0.560240963855422
0.9072	0.560240963855422
0.90832	0.55421686746988
0.90944	0.55421686746988
0.91056	0.55421686746988
0.91168	0.55421686746988
0.9128	0.55421686746988
0.91392	0.55421686746988
0.91504	0.55421686746988
0.91616	0.548192771084337
0.91728	0.548192771084337
0.9184	0.548192771084337
0.91952	0.548192771084337
0.92064	0.548192771084337
0.92176	0.548192771084337
0.92288	0.548192771084337
0.924	0.542168674698795
0.92512	0.542168674698795
0.92624	0.542168674698795
0.92736	0.542168674698795
0.92848	0.542168674698795
0.9296	0.542168674698795
0.93072	0.542168674698795
0.93184	0.536144578313253
0.93296	0.536144578313253
0.93408	0.536144578313253
0.9352	0.536144578313253
0.93632	0.536144578313253
0.93744	0.536144578313253
0.93856	0.536144578313253
0.93968	0.536144578313253
0.9408	0.536144578313253
0.94192	0.536144578313253
0.94304	0.536144578313253
0.94416	0.530120481927711
0.94528	0.530120481927711
0.9464	0.530120481927711
0.94752	0.530120481927711
0.94864	0.530120481927711
0.94976	0.530120481927711
0.95088	0.530120481927711
0.952	0.530120481927711
0.95312	0.530120481927711
0.95424	0.530120481927711
0.95536	0.524096385542169
0.95648	0.524096385542169
0.9576	0.524096385542169
0.95872	0.524096385542169
0.95984	0.524096385542169
0.96096	0.524096385542169
0.96208	0.524096385542169
0.9632	0.518072289156626
0.96432	0.518072289156626
0.96544	0.518072289156626
0.96656	0.518072289156626
0.96768	0.518072289156626
0.9688	0.518072289156626
0.96992	0.518072289156626
0.97104	0.512048192771084
0.97216	0.512048192771084
0.97328	0.512048192771084
0.9744	0.512048192771084
0.97552	0.512048192771084
0.97664	0.512048192771084
0.97776	0.512048192771084
0.97888	0.512048192771084
0.98	0.512048192771084
0.98112	0.506024096385542
0.98224	0.506024096385542
0.98336	0.506024096385542
0.98448	0.506024096385542
0.9856	0.506024096385542
0.98672	0.506024096385542
0.98784	0.506024096385542
0.98896	0.506024096385542
0.99008	0.506024096385542
0.9912	0.506024096385542
0.99232	0.506024096385542
0.99344	0.506024096385542
0.99456	0.5
0.99568	0.5
0.9968	0.5
0.99792	0.5
0.99904	0.5
1.00016	0.5
1.00128	0.5
1.0024	0.5
1.00352	0.5
1.00464	0.493975903614458
1.00576	0.493975903614458
1.00688	0.493975903614458
1.008	0.493975903614458
1.00912	0.493975903614458
1.01024	0.493975903614458
1.01136	0.493975903614458
1.01248	0.487951807228916
1.0136	0.487951807228916
1.01472	0.487951807228916
1.01584	0.487951807228916
1.01696	0.487951807228916
1.01808	0.487951807228916
1.0192	0.487951807228916
1.02032	0.487951807228916
1.02144	0.481927710843373
1.02256	0.481927710843373
1.02368	0.481927710843373
1.0248	0.481927710843373
1.02592	0.481927710843373
1.02704	0.481927710843373
1.02816	0.481927710843373
1.02928	0.481927710843373
1.0304	0.475903614457831
1.03152	0.475903614457831
1.03264	0.475903614457831
1.03376	0.475903614457831
1.03488	0.475903614457831
1.036	0.475903614457831
1.03712	0.475903614457831
1.03824	0.469879518072289
1.03936	0.469879518072289
1.04048	0.469879518072289
1.0416	0.469879518072289
1.04272	0.469879518072289
1.04384	0.469879518072289
1.04496	0.469879518072289
1.04608	0.469879518072289
1.0472	0.469879518072289
1.04832	0.469879518072289
1.04944	0.469879518072289
1.05056	0.469879518072289
1.05168	0.463855421686747
1.0528	0.463855421686747
1.05392	0.463855421686747
1.05504	0.463855421686747
1.05616	0.463855421686747
1.05728	0.463855421686747
1.0584	0.463855421686747
1.05952	0.463855421686747
1.06064	0.463855421686747
1.06176	0.463855421686747
1.06288	0.463855421686747
1.064	0.463855421686747
1.06512	0.457831325301205
1.06624	0.457831325301205
1.06736	0.457831325301205
1.06848	0.457831325301205
1.0696	0.457831325301205
1.07072	0.457831325301205
1.07184	0.457831325301205
1.07296	0.457831325301205
1.07408	0.451807228915663
1.0752	0.451807228915663
1.07632	0.451807228915663
1.07744	0.451807228915663
1.07856	0.451807228915663
1.07968	0.451807228915663
1.0808	0.451807228915663
1.08192	0.451807228915663
1.08304	0.44578313253012
1.08416	0.44578313253012
1.08528	0.44578313253012
1.0864	0.44578313253012
1.08752	0.44578313253012
1.08864	0.44578313253012
1.08976	0.44578313253012
1.09088	0.44578313253012
1.092	0.439759036144578
1.09312	0.439759036144578
1.09424	0.439759036144578
1.09536	0.439759036144578
1.09648	0.439759036144578
1.0976	0.439759036144578
1.09872	0.439759036144578
1.09984	0.439759036144578
1.10096	0.439759036144578
1.10208	0.433734939759036
1.1032	0.433734939759036
1.10432	0.433734939759036
1.10544	0.433734939759036
1.10656	0.433734939759036
1.10768	0.433734939759036
1.1088	0.433734939759036
1.10992	0.433734939759036
1.11104	0.433734939759036
1.11216	0.433734939759036
1.11328	0.433734939759036
1.1144	0.433734939759036
1.11552	0.433734939759036
1.11664	0.427710843373494
1.11776	0.427710843373494
1.11888	0.427710843373494
1.12	0.427710843373494
1.12112	0.427710843373494
1.12224	0.427710843373494
1.12336	0.427710843373494
1.12448	0.427710843373494
1.1256	0.427710843373494
1.12672	0.427710843373494
1.12784	0.427710843373494
1.12896	0.427710843373494
1.13008	0.421686746987952
1.1312	0.421686746987952
1.13232	0.421686746987952
1.13344	0.421686746987952
1.13456	0.421686746987952
1.13568	0.421686746987952
1.1368	0.421686746987952
1.13792	0.421686746987952
1.13904	0.421686746987952
1.14016	0.41566265060241
1.14128	0.41566265060241
1.1424	0.41566265060241
1.14352	0.41566265060241
1.14464	0.41566265060241
1.14576	0.41566265060241
1.14688	0.41566265060241
1.148	0.41566265060241
1.14912	0.41566265060241
1.15024	0.409638554216867
1.15136	0.409638554216867
1.15248	0.409638554216867
1.1536	0.409638554216867
1.15472	0.409638554216867
1.15584	0.409638554216867
1.15696	0.409638554216867
1.15808	0.409638554216867
1.1592	0.409638554216867
1.16032	0.409638554216867
1.16144	0.409638554216867
1.16256	0.403614457831325
1.16368	0.403614457831325
1.1648	0.403614457831325
1.16592	0.403614457831325
1.16704	0.403614457831325
1.16816	0.403614457831325
1.16928	0.403614457831325
1.1704	0.403614457831325
1.17152	0.403614457831325
1.17264	0.403614457831325
1.17376	0.403614457831325
1.17488	0.403614457831325
1.176	0.403614457831325
1.17712	0.403614457831325
1.17824	0.397590361445783
1.17936	0.397590361445783
1.18048	0.397590361445783
1.1816	0.397590361445783
1.18272	0.397590361445783
1.18384	0.397590361445783
1.18496	0.397590361445783
1.18608	0.397590361445783
1.1872	0.397590361445783
1.18832	0.397590361445783
1.18944	0.397590361445783
1.19056	0.397590361445783
1.19168	0.391566265060241
1.1928	0.391566265060241
1.19392	0.391566265060241
1.19504	0.391566265060241
1.19616	0.391566265060241
1.19728	0.391566265060241
1.1984	0.391566265060241
1.19952	0.391566265060241
1.20064	0.391566265060241
1.20176	0.385542168674699
1.20288	0.385542168674699
1.204	0.385542168674699
1.20512	0.385542168674699
1.20624	0.385542168674699
1.20736	0.385542168674699
1.20848	0.385542168674699
1.2096	0.385542168674699
1.21072	0.385542168674699
1.21184	0.385542168674699
1.21296	0.379518072289157
1.21408	0.379518072289157
1.2152	0.379518072289157
1.21632	0.379518072289157
1.21744	0.379518072289157
1.21856	0.379518072289157
1.21968	0.379518072289157
1.2208	0.379518072289157
1.22192	0.379518072289157
1.22304	0.373493975903614
1.22416	0.373493975903614
1.22528	0.373493975903614
1.2264	0.373493975903614
1.22752	0.373493975903614
1.22864	0.373493975903614
1.22976	0.373493975903614
1.23088	0.373493975903614
1.232	0.373493975903614
1.23312	0.373493975903614
1.23424	0.367469879518072
1.23536	0.367469879518072
1.23648	0.367469879518072
1.2376	0.367469879518072
1.23872	0.367469879518072
1.23984	0.367469879518072
1.24096	0.367469879518072
1.24208	0.367469879518072
1.2432	0.367469879518072
1.24432	0.367469879518072
1.24544	0.36144578313253
1.24656	0.36144578313253
1.24768	0.36144578313253
1.2488	0.36144578313253
1.24992	0.36144578313253
1.25104	0.36144578313253
1.25216	0.36144578313253
1.25328	0.36144578313253
1.2544	0.36144578313253
1.25552	0.36144578313253
1.25664	0.36144578313253
1.25776	0.36144578313253
1.25888	0.36144578313253
1.26	0.36144578313253
1.26112	0.355421686746988
1.26224	0.355421686746988
1.26336	0.355421686746988
1.26448	0.355421686746988
1.2656	0.355421686746988
1.26672	0.355421686746988
1.26784	0.355421686746988
1.26896	0.355421686746988
1.27008	0.355421686746988
1.2712	0.355421686746988
1.27232	0.355421686746988
1.27344	0.355421686746988
1.27456	0.355421686746988
1.27568	0.355421686746988
1.2768	0.355421686746988
1.27792	0.349397590361446
1.27904	0.349397590361446
1.28016	0.349397590361446
1.28128	0.349397590361446
1.2824	0.349397590361446
1.28352	0.349397590361446
1.28464	0.349397590361446
1.28576	0.349397590361446
1.28688	0.349397590361446
1.288	0.349397590361446
1.28912	0.349397590361446
1.29024	0.343373493975904
1.29136	0.343373493975904
1.29248	0.343373493975904
1.2936	0.343373493975904
1.29472	0.343373493975904
1.29584	0.343373493975904
1.29696	0.343373493975904
1.29808	0.343373493975904
1.2992	0.343373493975904
1.30032	0.343373493975904
1.30144	0.343373493975904
1.30256	0.337349397590361
1.30368	0.337349397590361
1.3048	0.337349397590361
1.30592	0.337349397590361
1.30704	0.337349397590361
1.30816	0.337349397590361
1.30928	0.337349397590361
1.3104	0.337349397590361
1.31152	0.337349397590361
1.31264	0.337349397590361
1.31376	0.331325301204819
1.31488	0.331325301204819
1.316	0.331325301204819
1.31712	0.331325301204819
1.31824	0.331325301204819
1.31936	0.331325301204819
1.32048	0.331325301204819
1.3216	0.331325301204819
1.32272	0.331325301204819
1.32384	0.331325301204819
1.32496	0.331325301204819
1.32608	0.331325301204819
1.3272	0.331325301204819
1.32832	0.331325301204819
1.32944	0.325301204819277
1.33056	0.325301204819277
1.33168	0.325301204819277
1.3328	0.325301204819277
1.33392	0.325301204819277
1.33504	0.325301204819277
1.33616	0.325301204819277
1.33728	0.325301204819277
1.3384	0.325301204819277
1.33952	0.325301204819277
1.34064	0.325301204819277
1.34176	0.325301204819277
1.34288	0.325301204819277
1.344	0.325301204819277
1.34512	0.325301204819277
1.34624	0.319277108433735
1.34736	0.319277108433735
1.34848	0.319277108433735
1.3496	0.319277108433735
1.35072	0.319277108433735
1.35184	0.319277108433735
1.35296	0.319277108433735
1.35408	0.319277108433735
1.3552	0.319277108433735
1.35632	0.319277108433735
1.35744	0.319277108433735
1.35856	0.313253012048193
1.35968	0.313253012048193
1.3608	0.313253012048193
1.36192	0.313253012048193
1.36304	0.313253012048193
1.36416	0.313253012048193
1.36528	0.313253012048193
1.3664	0.313253012048193
1.36752	0.313253012048193
1.36864	0.313253012048193
1.36976	0.307228915662651
1.37088	0.307228915662651
1.372	0.307228915662651
1.37312	0.307228915662651
1.37424	0.307228915662651
1.37536	0.307228915662651
1.37648	0.307228915662651
1.3776	0.307228915662651
1.37872	0.307228915662651
1.37984	0.307228915662651
1.38096	0.301204819277108
1.38208	0.301204819277108
1.3832	0.301204819277108
1.38432	0.301204819277108
1.38544	0.301204819277108
1.38656	0.301204819277108
1.38768	0.301204819277108
1.3888	0.301204819277108
1.38992	0.301204819277108
1.39104	0.301204819277108
1.39216	0.295180722891566
1.39328	0.295180722891566
1.3944	0.295180722891566
1.39552	0.295180722891566
1.39664	0.295180722891566
1.39776	0.295180722891566
1.39888	0.295180722891566
1.4	0.295180722891566
1.40112	0.295180722891566
1.40224	0.295180722891566
1.40336	0.295180722891566
1.40448	0.289156626506024
1.4056	0.289156626506024
1.40672	0.289156626506024
1.40784	0.289156626506024
1.40896	0.289156626506024
1.41008	0.289156626506024
1.4112	0.289156626506024
1.41232	0.289156626506024
1.41344	0.289156626506024
1.41456	0.289156626506024
1.41568	0.289156626506024
1.4168	0.289156626506024
1.41792	0.289156626506024
1.41904	0.289156626506024
1.42016	0.283132530120482
1.42128	0.283132530120482
1.4224	0.283132530120482
1.42352	0.283132530120482
1.42464	0.283132530120482
1.42576	0.283132530120482
1.42688	0.283132530120482
1.428	0.283132530120482
1.42912	0.283132530120482
1.43024	0.283132530120482
1.43136	0.283132530120482
1.43248	0.283132530120482
1.4336	0.283132530120482
1.43472	0.283132530120482
1.43584	0.27710843373494
1.43696	0.27710843373494
1.43808	0.27710843373494
1.4392	0.27710843373494
1.44032	0.27710843373494
1.44144	0.27710843373494
1.44256	0.27710843373494
1.44368	0.27710843373494
1.4448	0.27710843373494
1.44592	0.27710843373494
1.44704	0.271084337349398
1.44816	0.271084337349398
1.44928	0.271084337349398
1.4504	0.271084337349398
1.45152	0.271084337349398
1.45264	0.271084337349398
1.45376	0.271084337349398
1.45488	0.271084337349398
1.456	0.271084337349398
1.45712	0.271084337349398
1.45824	0.265060240963855
1.45936	0.265060240963855
1.46048	0.265060240963855
1.4616	0.265060240963855
1.46272	0.265060240963855
1.46384	0.265060240963855
1.46496	0.265060240963855
1.46608	0.265060240963855
1.4672	0.265060240963855
1.46832	0.265060240963855
1.46944	0.259036144578313
1.47056	0.259036144578313
1.47168	0.259036144578313
1.4728	0.259036144578313
1.47392	0.259036144578313
1.47504	0.259036144578313
1.47616	0.259036144578313
1.47728	0.259036144578313
1.4784	0.259036144578313
1.47952	0.253012048192771
1.48064	0.253012048192771
1.48176	0.253012048192771
1.48288	0.253012048192771
1.484	0.253012048192771
1.48512	0.253012048192771
1.48624	0.253012048192771
1.48736	0.253012048192771
1.48848	0.253012048192771
1.4896	0.253012048192771
1.49072	0.253012048192771
1.49184	0.253012048192771
1.49296	0.253012048192771
1.49408	0.246987951807229
1.4952	0.246987951807229
1.49632	0.246987951807229
1.49744	0.246987951807229
1.49856	0.246987951807229
1.49968	0.246987951807229
1.5008	0.246987951807229
1.50192	0.246987951807229
1.50304	0.246987951807229
1.50416	0.246987951807229
1.50528	0.246987951807229
1.5064	0.246987951807229
1.50752	0.246987951807229
1.50864	0.246987951807229
1.50976	0.246987951807229
1.51088	0.240963855421687
1.512	0.240963855421687
1.51312	0.240963855421687
1.51424	0.240963855421687
1.51536	0.240963855421687
1.51648	0.240963855421687
1.5176	0.240963855421687
1.51872	0.240963855421687
1.51984	0.240963855421687
1.52096	0.240963855421687
1.52208	0.240963855421687
1.5232	0.234939759036145
1.52432	0.234939759036145
1.52544	0.234939759036145
1.52656	0.234939759036145
1.52768	0.234939759036145
1.5288	0.234939759036145
1.52992	0.234939759036145
1.53104	0.234939759036145
1.53216	0.234939759036145
1.53328	0.234939759036145
1.5344	0.228915662650602
1.53552	0.228915662650602
1.53664	0.228915662650602
1.53776	0.228915662650602
1.53888	0.228915662650602
1.54	0.228915662650602
1.54112	0.228915662650602
1.54224	0.228915662650602
1.54336	0.228915662650602
1.54448	0.22289156626506
1.5456	0.22289156626506
1.54672	0.22289156626506
1.54784	0.22289156626506
1.54896	0.22289156626506
1.55008	0.22289156626506
1.5512	0.22289156626506
1.55232	0.22289156626506
1.55344	0.22289156626506
1.55456	0.22289156626506
1.55568	0.216867469879518
1.5568	0.216867469879518
1.55792	0.216867469879518
1.55904	0.216867469879518
1.56016	0.216867469879518
1.56128	0.216867469879518
1.5624	0.216867469879518
1.56352	0.216867469879518
1.56464	0.216867469879518
1.56576	0.216867469879518
1.56688	0.210843373493976
1.568	0.210843373493976
1.56912	0.210843373493976
1.57024	0.210843373493976
1.57136	0.210843373493976
1.57248	0.210843373493976
1.5736	0.210843373493976
1.57472	0.210843373493976
1.57584	0.210843373493976
1.57696	0.204819277108434
1.57808	0.204819277108434
1.5792	0.204819277108434
1.58032	0.204819277108434
1.58144	0.204819277108434
1.58256	0.204819277108434
1.58368	0.204819277108434
1.5848	0.204819277108434
1.58592	0.204819277108434
1.58704	0.204819277108434
1.58816	0.204819277108434
1.58928	0.204819277108434
1.5904	0.204819277108434
1.59152	0.204819277108434
1.59264	0.204819277108434
1.59376	0.198795180722892
1.59488	0.198795180722892
1.596	0.198795180722892
1.59712	0.198795180722892
1.59824	0.198795180722892
1.59936	0.198795180722892
1.60048	0.198795180722892
1.6016	0.198795180722892
1.60272	0.198795180722892
1.60384	0.198795180722892
1.60496	0.198795180722892
1.60608	0.198795180722892
1.6072	0.198795180722892
1.60832	0.198795180722892
1.60944	0.192771084337349
1.61056	0.192771084337349
1.61168	0.192771084337349
1.6128	0.192771084337349
1.61392	0.192771084337349
1.61504	0.192771084337349
1.61616	0.192771084337349
1.61728	0.192771084337349
1.6184	0.192771084337349
1.61952	0.192771084337349
1.62064	0.186746987951807
1.62176	0.186746987951807
1.62288	0.186746987951807
1.624	0.186746987951807
1.62512	0.186746987951807
1.62624	0.186746987951807
1.62736	0.186746987951807
1.62848	0.186746987951807
1.6296	0.186746987951807
1.63072	0.186746987951807
1.63184	0.180722891566265
1.63296	0.180722891566265
1.63408	0.180722891566265
1.6352	0.180722891566265
1.63632	0.180722891566265
1.63744	0.180722891566265
1.63856	0.180722891566265
1.63968	0.180722891566265
1.6408	0.180722891566265
1.64192	0.180722891566265
1.64304	0.180722891566265
1.64416	0.174698795180723
1.64528	0.174698795180723
1.6464	0.174698795180723
1.64752	0.174698795180723
1.64864	0.174698795180723
1.64976	0.174698795180723
1.65088	0.174698795180723
1.652	0.174698795180723
1.65312	0.174698795180723
1.65424	0.174698795180723
1.65536	0.174698795180723
1.65648	0.174698795180723
1.6576	0.168674698795181
1.65872	0.168674698795181
1.65984	0.168674698795181
1.66096	0.168674698795181
1.66208	0.168674698795181
1.6632	0.168674698795181
1.66432	0.168674698795181
1.66544	0.168674698795181
1.66656	0.168674698795181
1.66768	0.168674698795181
1.6688	0.168674698795181
1.66992	0.168674698795181
1.67104	0.168674698795181
1.67216	0.168674698795181
1.67328	0.162650602409639
1.6744	0.162650602409639
1.67552	0.162650602409639
1.67664	0.162650602409639
1.67776	0.162650602409639
1.67888	0.162650602409639
1.68	0.162650602409639
1.68112	0.162650602409639
1.68224	0.162650602409639
1.68336	0.162650602409639
1.68448	0.162650602409639
1.6856	0.162650602409639
1.68672	0.162650602409639
1.68784	0.162650602409639
1.68896	0.156626506024096
1.69008	0.156626506024096
1.6912	0.156626506024096
1.69232	0.156626506024096
1.69344	0.156626506024096
1.69456	0.156626506024096
1.69568	0.156626506024096
1.6968	0.156626506024096
1.69792	0.156626506024096
1.69904	0.156626506024096
1.70016	0.156626506024096
1.70128	0.156626506024096
1.7024	0.156626506024096
1.70352	0.156626506024096
1.70464	0.156626506024096
1.70576	0.156626506024096
1.70688	0.150602409638554
1.708	0.150602409638554
1.70912	0.150602409638554
1.71024	0.150602409638554
1.71136	0.150602409638554
1.71248	0.150602409638554
1.7136	0.150602409638554
1.71472	0.150602409638554
1.71584	0.150602409638554
1.71696	0.150602409638554
1.71808	0.150602409638554
1.7192	0.150602409638554
1.72032	0.144578313253012
1.72144	0.144578313253012
1.72256	0.144578313253012
1.72368	0.144578313253012
1.7248	0.144578313253012
1.72592	0.144578313253012
1.72704	0.144578313253012
1.72816	0.144578313253012
1.72928	0.144578313253012
1.7304	0.144578313253012
1.73152	0.144578313253012
1.73264	0.144578313253012
1.73376	0.144578313253012
1.73488	0.144578313253012
1.736	0.13855421686747
1.73712	0.13855421686747
1.73824	0.13855421686747
1.73936	0.13855421686747
1.74048	0.13855421686747
1.7416	0.13855421686747
1.74272	0.13855421686747
1.74384	0.13855421686747
1.74496	0.13855421686747
1.74608	0.13855421686747
1.7472	0.13855421686747
1.74832	0.13855421686747
1.74944	0.13855421686747
1.75056	0.13855421686747
1.75168	0.132530120481928
1.7528	0.132530120481928
1.75392	0.132530120481928
1.75504	0.132530120481928
1.75616	0.132530120481928
1.75728	0.132530120481928
1.7584	0.132530120481928
1.75952	0.132530120481928
1.76064	0.132530120481928
1.76176	0.132530120481928
1.76288	0.132530120481928
1.764	0.132530120481928
1.76512	0.132530120481928
1.76624	0.132530120481928
1.76736	0.132530120481928
1.76848	0.132530120481928
1.7696	0.132530120481928
1.77072	0.132530120481928
1.77184	0.132530120481928
1.77296	0.132530120481928
1.77408	0.132530120481928
1.7752	0.132530120481928
1.77632	0.132530120481928
1.77744	0.126506024096386
1.77856	0.126506024096386
1.77968	0.126506024096386
1.7808	0.126506024096386
1.78192	0.126506024096386
1.78304	0.126506024096386
1.78416	0.126506024096386
1.78528	0.126506024096386
1.7864	0.126506024096386
1.78752	0.126506024096386
1.78864	0.126506024096386
1.78976	0.126506024096386
1.79088	0.126506024096386
1.792	0.126506024096386
1.79312	0.126506024096386
1.79424	0.126506024096386
1.79536	0.126506024096386
1.79648	0.126506024096386
1.7976	0.126506024096386
1.79872	0.126506024096386
1.79984	0.126506024096386
1.80096	0.126506024096386
1.80208	0.126506024096386
1.8032	0.126506024096386
1.80432	0.126506024096386
1.80544	0.126506024096386
1.80656	0.126506024096386
1.80768	0.126506024096386
1.8088	0.126506024096386
1.80992	0.126506024096386
1.81104	0.120481927710843
1.81216	0.120481927710843
1.81328	0.120481927710843
1.8144	0.120481927710843
1.81552	0.120481927710843
1.81664	0.120481927710843
1.81776	0.120481927710843
1.81888	0.120481927710843
1.82	0.120481927710843
1.82112	0.120481927710843
1.82224	0.120481927710843
1.82336	0.120481927710843
1.82448	0.120481927710843
1.8256	0.120481927710843
1.82672	0.120481927710843
1.82784	0.120481927710843
1.82896	0.120481927710843
1.83008	0.120481927710843
1.8312	0.120481927710843
1.83232	0.120481927710843
1.83344	0.120481927710843
1.83456	0.120481927710843
1.83568	0.120481927710843
1.8368	0.120481927710843