This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: The issue of tampering with the value of the bar memory allocated by PCIe on sdk0902

Part Number: TDA4VH-Q1

Tool/software:

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1360433/tda4vh-q1-how-to-modify-pcie-shared-memory-size-to-1gb

According to the patch "0001-Change-PCIe1-memory-space-to-PCIE1_DAT1.patch" used in the above link, there is no problem with testing on SDK0805. However, when testing on sdk0902, there may be issues with certain memory points being modified on the bar, as shown in the following figure. Writing a value of 0xB0B0B0B0 to memory point 0x4124406005 on a certain bar on the RC end will cause a change in value after one or two seconds. Please help confirm if this patch is also used on SDK0902?