Tool/software:
I am using the following:
it runs on EVB well
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I am using the following:
I have this :
administrator@administrator-HP-EliteBook-840-G8-Notebook-PC:~/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/board-support/linux-4.19.94+gitAUTOINC+be5389fd85-gbe5389fd85/arch/arm/boot/dts$ ls -l am57xx*
-rw-r--r-- 1 administrator administrator 13329 Apr 19 2020 am57xx-beagle-x15-common.dtsi
-rw-rw-r-- 1 administrator administrator 90792 Jul 8 18:54 am57xx-beagle-x15.dtb
-rw-r--r-- 1 administrator administrator 1104 Apr 19 2020 am57xx-beagle-x15.dts
-rw-rw-r-- 1 administrator administrator 90328 Jul 8 18:54 am57xx-beagle-x15-revb1.dtb
-rw-r--r-- 1 administrator administrator 1024 Apr 19 2020 am57xx-beagle-x15-revb1.dts
-rw-rw-r-- 1 administrator administrator 90766 Jul 8 18:54 am57xx-beagle-x15-revc.dtb
-rw-r--r-- 1 administrator administrator 926 Apr 19 2020 am57xx-beagle-x15-revc.dts
-rw-r--r-- 1 administrator administrator 16784 Apr 19 2020 am57xx-cl-som-am57x.dts
-rw-r--r-- 1 administrator administrator 395 Apr 19 2020 am57xx-commercial-grade.dtsi
-rw-rw-r-- 1 administrator administrator 135382 Jul 8 18:55 am57xx-evm-cam-mt9t111.dtb
-rw-rw-r-- 1 administrator administrator 135669 Jul 8 18:55 am57xx-evm-cam-ov10635.dtb
-rw-rw-r-- 1 administrator administrator 780 Apr 19 2020 am57xx-evm-cmem-am571x.dtsi
-rw-rw-r-- 1 administrator administrator 698 Apr 19 2020 am57xx-evm-cmem-am5729-beagleboneai.dtsi
-rw-rw-r-- 1 administrator administrator 1006 Apr 19 2020 am57xx-evm-cmem-am572idk.dtsi
-rw-rw-r-- 1 administrator administrator 1006 Apr 19 2020 am57xx-evm-cmem-am574x.dtsi
-rw-rw-r-- 1 administrator administrator 1006 Apr 19 2020 am57xx-evm-cmem.dtsi
-rw-rw-r-- 1 administrator administrator 134744 Jul 8 18:54 am57xx-evm.dtb
-rw-rw-r-- 1 administrator administrator 135132 Jul 8 18:55 am57xx-evm-jailhouse.dtb
-rw-rw-r-- 1 administrator administrator 135368 Jul 8 18:55 am57xx-evm-reva3-cam-mt9t111.dtb
-rw-rw-r-- 1 administrator administrator 135655 Jul 8 18:55 am57xx-evm-reva3-cam-ov10635.dtb
-rw-rw-r-- 1 administrator administrator 134730 Jul 8 18:55 am57xx-evm-reva3.dtb
-rw-rw-r-- 1 administrator administrator 135118 Jul 8 18:55 am57xx-evm-reva3-jailhouse.dtb
-rw-r--r-- 1 administrator administrator 14012 Apr 19 2020 am57xx-idk-common.dtsi
-rw-r--r-- 1 administrator administrator 400 Apr 19 2020 am57xx-industrial-grade.dtsi
-rw-r--r-- 1 administrator administrator 8054 Apr 19 2020 am57xx-pru-uio.dtsi
-rw-r--r-- 1 administrator administrator 4202 Apr 19 2020 am57xx-sbc-am57x.dts
administrator@administrator-HP-EliteBook-840-G8-Notebook-PC:~/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/board-support/linux-4.19.94+gitAUTOINC+be5389fd85-gbe5389fd85/arch/arm/boot/dts$
by looking at board uboot I can see (I am working with the default sd card) am57xx-evm-reva3.dtb is used
however there is no am57xx-evm-reva3.dts
notice that in sdk: ti-processor-sdk-linux-am57xx-evm-08_02_01_00 , this dts does exist
but I am working with: /06.03.00.106
I must work with this version and can not move version
please advice (I think you simplly forgot to release it, since it's clear you have the source and you just released the dtb)
thank you
Hello Ilan,
I believe the file you are looking for is the am57xx-evm-reva3.dtso, which can be found in the following directory:
For more information on how it works please see https://docs.kernel.org/devicetree/overlay-notes.html
Best,
Josue