This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: What is the range of CSITX node send resolution?

Part Number: TDA4VM

Tool/software:

Dear experts,

 I used CSITX node to send 1024x512 resolution images, the images can be sent and received normally, 1080P resolution also works. But when I sent 640x512 resolution images, the images I received were always abnormal . I added display node to the sender's graph. DSS module shows the sent picture is normal, what is the reason?

Regards,

xin

  • Hi Xin,

    If you are seeing image using DSS correctly, that means that the input to the csitx is fine.

    And if you are getting some data on the other side (i.e. the csi receiver side) then your csitx is sending the data fine with certain laneband speed.

    So please check you have configured the receiver side correctly.

    Regards,

    Nikhil