Other Parts Discussed in Thread: TMS320C5515
Hi all,
I received the USB boot tool from TI recently. I have done the required changes on EVM5515 and the USB boot is working fine on the EVM5515 board. We have a prototype board with C5515 processor and the board is having similar connections for the USB module. I have provided external power-supply of 1.3V to our prototype and our HID drivers are working fine with this change. So I think the external supply is also proper. But the USB booting is not working on our prototype. The device is emulated as "unknown device" where as C5515 EVM is emulated as "TMSC5505" while USB boot. The only change we are seeing is CPU silicon revision.
The CPU name on EVM5515: TMX320C5515 AZCHI2 01A9PLW
The CPU name on our prototype: TMS320C5515 AZCHI2 04AH08W
"TMX" and "TMS" CPU silicon will have any difference or the ROM boot-loader is different in both? Does any body had similar issue? Any other suggestions?