Hi,
I tried to set up 64 bit gp timer as "32-bit timer chained mode for continuous operation with period reload" on C6747, but so far timer doesn't start counting.
I could get expected result with "32-bit timer chained mode for continuous operation " and "the 32-bit timer unchained mode with no prescaler for continuous operation with period reload."
So I concern that, page. 14 of below documents said "32-bit timer chained mode for continuous operation with period reload (Timer 3 only)"
http://www.ti.com/lit/ug/sprufm5d/sprufm5d.pdf,
What does this (Timer 3 only) ? Does it mean, it is available only for the device, which has over more than 2 gp timers (like, C6748)?
best regards,
Hirofumi Fujita