Hi Champs,
I'm checking a "hw_dbg0" pin of AM3517 ZCN Pkg now, but I have one question about the difference of description between the datasheet(SPRS550C) and TRM(SPRUGR0B).
In datasheet, Table 2-1(P.23), hw_dbg0 is assigned to AD2 and mode is 5.
Also, hw_dbg0 is assigned to both AD2 and AD17 in Table 2-3(P.53 and 55).
On the other hand, in TRM, Table 6-5(P.629 and 632), hw_dbg0 is assigned both CONTROL_PADCONF_CCDC_PCLK[15:0] mode5 and CONTROL_PADCONF_SYS_NIRQ[31:16] mode7. However, mode0-6 of CONTROL_PADCONF_SYS_NIRQ[31:16] does not correspond to AD17 description in the datasheet.
Which one is the correct assignment for hw_dbg0?
Best regards,
Ayumi