Other Parts Discussed in Thread: TPS65920, TPS65950, SYSCONFIG
Hi,
On our own 3730 board (with TPS65920) as well as on BeagleBoard xM (TPS65950), configuring the MUSB controller in Linux to peripheral mode (i.e. not OTG mode) and using a built-in gadget driver, the gadget device sometimes does not appear after a software reboot.
This is using the latest Arago, but I've seen it with Angstrom 2008.1 and 2010.x too.
Configuring the MUSB controller in u-boot as a device and only booting as far as u-boot before a software reset, the device always appears. To me this suggests a MUSB driver issue in Linux (as opposed to, say, PHY initialization).
I checked with a USB analyzer what happens on the bus: when it doesn't
show up there is a reset on the bus when we reboot, but it doesn't
re-enter full speed mode. No SOFs are sent either.
I did a rudimentary check of the OTG registers in the TPS chip (over
i2c) but saw nothing out of the ordinary.
I set musb_debug = 5 in musb_core.c, but no errors are reported.
Anyone else seen this?
Thanks,
Orjan