This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The Source Code for C5515 Programmer is Available



The source code for the C5515 EVM Programmer is available for download via:

CCS3.3: http://code.google.com/p/c5505-ezdsp/downloads/detail?name=programmer_c5515evm.zip

CCS4.x: http://code.google.com/p/c5505-ezdsp/downloads/detail?name=programmer_c5515evm_ccs4.zip

as a reference for your development.

[EDIT - Added CCS4 link]

  • I have imported this project in to CCS4 as a legacy CCSv3.3 project but when I try to build I get unresolved symbol errors at link time:

    Severity and Description    Path    Resource    Location    Creation Time    Id
    unresolved symbol _vATA_cdRoot, first referenced in C:/wip/C5515EVM/programmer_c5515evm/Debug/mmc_sd.obj        programmer    line 0    1318356932040    763
    unresolved symbol _vATA_close, first referenced in C:/wip/C5515EVM/programmer_c5515evm/Debug/mmc_sd.obj        programmer    line 0    1318356932040    764
    unresolved symbol _vATA_create, first referenced in C:/wip/C5515EVM/programmer_c5515evm/Debug/mmc_sd.obj        programmer    line 0    1318356932040    765
    unresolved symbol _vATA_delete, first referenced in C:/wip/C5515EVM/programmer_c5515evm/Debug/mmc_sd.obj        programmer    line 0    1318356932040    766
    unresolved symbol _vATA_fileInit, first referenced in C:/wip/C5515EVM/programmer_c5515evm/Debug/mmc_sd.obj        programmer    line 0    1318356932040    767
    unresolved symbol _vATA_findNext, first referenced in C:/wip/C5515EVM/programmer_c5515evm/Debug/mmc_sd.obj        programmer    line 0    1318356932040    768
    unresolved symbol _vATA_isDir, first referenced in C:/wip/C5515EVM/programmer_c5515evm/Debug/mmc_sd.obj        programmer    line 0    1318356932040    769
    unresolved symbol _vATA_read, first referenced in C:/wip/C5515EVM/programmer_c5515evm/Debug/mmc_sd.obj        programmer    line 0    1318356932040    770
    unresolved symbol _vATA_seek, first referenced in C:/wip/C5515EVM/programmer_c5515evm/Debug/mmc_sd.obj        programmer    line 0    1318356932040    771
    unresolved symbol _vATA_setFileName, first referenced in C:/wip/C5515EVM/programmer_c5515evm/Debug/mmc_sd.obj        programmer    line 0    1318356932040    772
    unresolved symbol _vATA_systemInit, first referenced in C:/wip/C5515EVM/programmer_c5515evm/Debug/mmc_sd.obj        programmer    line 0    1318356932056    773
    unresolved symbol _vATA_write, first referenced in C:/wip/C5515EVM/programmer_c5515evm/Debug/mmc_sd.obj        programmer    line 0    1318356932056    774

     

  • All,

    We have replaced theCCS3.3 version with a CCS4 version. Please download again.

    http://code.google.com/p/c5505-ezdsp/downloads/detail?name=programmer_c5515evm_ccs4.zip

    Regards.

     

  • Steve,

    Is there any chance we could also get the source code that generated the  programmer_c5515_eZdsp.out file (http://processors.wiki.ti.com/index.php/C5515_Boot-Image_Programmer)? The EVM programmer above is very different and does not work for the ezdsp.

  • Mike,

    The total project is not ready for generate release. If you agree to use it as-is without any support, I could send to you directly via your personal email.

    Regards.