Other Parts Discussed in Thread: TPS65219,
Tool/software:
I’m working on a custom board based on the am623 processor. It is running a U-boot 2023.10 and Linux kernel 6.1.69-rt21. The thing is that its not able to reboot and I would not like to reset only the eMMC to do so. I'd like to reset all system. The used PMIC is TPS65219. I'm attaching the kernel messages that appear when I run the reboot command.
Requesting system reboot
[ 69.223434] watchdog: watchdog0: watchdog did not stop!
[ 71.273368] ti-sci 44043000.system-controller: Mbox timedout in resp(caller: sci_clk_recalc_rate+0x48/0xa0)
[ 71.283128] ti-sci 44043000.system-controller: Mbox send fail -110
[ 71.289297] ti-sci-clk 44043000.system-controller:clock-controller: recalc-rate failed for dev=135, clk=0, ret=-110
[ 71.299738] ti-sci 44043000.system-controller: Message for 0 is not expected!
[ 71.384445] reboot: Restarting system
Any help is appreciated.