Other Parts Discussed in Thread: TVP5158, TVP5151
We have the DM368 DVR RDK, the instructions state when we should load the kernal named "uImage_DM368_DVR", unfortunately the /bin folder only has a file named uImage_DM365_DVR. I built the kernel, but it also generates a file of the incorrect name. I suspect I may have the "target" set incorrectly. Is this really an issue, do I need to set the target correctly? How do I do this in the RDK? I do not see any compile fields that can be set to DM368.
In the interest of being diligent, I tried loading this kernel file, but I get a kernel panic during boot:
layer=c3bee800,layer->video_dev=c3bee960
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
i2c /dev entries driver
MDIN200 default input NTSC
Unable to handle kernel NULL pointer dereference at virtual address 00000008
pgd = c0004000
[00000008] *pgd=00000000
Internal error: Oops: 5 [#1]
Modules linked in:
CPU: 0
PC is at mdin200_i2c_read_reg+0x10/0x9c
LR is at mdin200_probe+0x40/0xf74
pc : [<c02f23fc>] lr : [<c02f2e30>] Not tainted
sp : c05a1c50 ip : c05a1c90 fp : c05a1c8c
r10: 00000000 r9 : c045dcf8 r8 : c0460108
r7 : c0460004 r6 : 00000000 r5 : c04600a0 r4 : c05a1dee
r3 : 00000080 r2 : c05a1dee r1 : 00000004 r0 : 00000000
Flags: nZCv IRQs on FIQs on Mode SVC_32 Segment kernel
Control: 5317F
Table: 80004000 DAC: 00000017
Process swapper (pid: 1, stack limit = 0xc05a0258)
Stack: (0xc05a1c50 to 0xc05a2000)
1c40: c00fdba4 c05a1dee c04600a0 00000000
1c60: c0460004 c0460108 c045dcf8 00000000 c05a1c8c c05a1dee c04600a0 00000000
1c80: c05a1e1c c05a1c90 c02f2e30 c02f23fc c0460098 00000000 c05a1cc4 c05a1ca8
1ca0: c00efba4 c010afe4 c05a0000 ffffffff fbc48000 c044f048 c03dbed8 c05a1d28
1cc0: c05a1d0c c05a1cd0 c04c7280 c05b4640 c05a1cf4 c05a1ce0 c00ff0b8 c00fefcc
1ce0: c05b4640 c04c7280 c05a1d14 c05a1cf8 c00ff158 c00ff0a0 00000001 c05b4640
1d00: c04c7280 00000007 c05a1d44 c05a0000 c058dbc0 00000017 c05a1d3c c05a1d28
1d20: c01151f4 c0114610 c05d201c c058dbc0 c05a1d7c c05a1d40 c03dbc6c c03de130
1d40: c01001ac c00fffd4 00000001 c058dcd0 c00feb44 c05a0000 c058dbc0 c05a0000
1d60: c05a1e2c c0458d54 00000000 c3bd4ca0 c05a1d94 c05a1d80 c03dbed8 c03db570
1d80: c010043c 00000004 c05a1dcc c05a1d98 c03dc228 c03dbe2c c05a1dbc 00000001
1da0: c058dbc0 c0100190 00100100 00200200 00000000 c05a1e84 c05a1ddc c05a1e2c
1dc0: c05a1e64 c05a1dd0 c0117518 c03dc178 c05a1df4 c05be640 c05f59e0 00000000
1de0: c05a1de0 c05a1de0 c0117530 00001e0c c05966e0 00000000 c04600a0 00000000
1e00: c0460004 c0460108 c045dcf8 00000000 c05a1e2c c05a1e20 c02d14b8 c02f2e00
1e20: c05a1e4c c05a1e30 c02cfae8 c02d14a8 00000000 c02cfb38 c04600a0 c05a1e64
1e40: c05a1e5c c05a1e50 c02cfb48 c02cfa7c c05a1e8c c05a1e60 c02cf314 c02cfb48
1e60: c028ed60 c045df30 c045df30 c0460064 c0460170 c04600a0 c0460144 00000000
1e80: c05a1ea4 c05a1e90 c02cfbac c02cf2d4 c02cf2b0 c045de20 c05a1ebc c05a1ea8
1ea0: c02ceff4 c02cfb5c 00000000 c04600a0 c05a1ef4 c05a1ec0 c02cdff4 c02cefe4
1ec0: c0418874 00000000 c05a1fa0 00000000 c0460098 00000000 c0460144 c044e094
1ee0: 00000000 c044e0b0 c05a1f24 c05a1ef8 c02d1860 c02cdda0 00000000 c04600a0
1f00: c0460098 00000000 c04e7758 00000000 c05a1fa0 c0030c40 c05a1f3c c05a1f28
1f20: c02d18d8 c02d1768 c02d16e0 c040cdfc c05a1f9c c05a1f40 c0027d94 c02d18c4
1f40: c041832c c040cdfc 00000001 00000001 00000001 000002e0 000001e0 00007530
1f60: 000003e9 00000079 00000000 00000010 00000000 00000000 00000000 00000000
1f80: c0027c6c 00000000 c0030abc c05a0000 c05a1ff4 c05a1fa0 c00ee0c0 c0027ce8
1fa0: 00000000 c05a1fb0 c00eee88 c00f1208 00000000 00000000 c00ee028 c0107f24
1fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
1fe0: 00000000 00000000 00000000 c05a1ff8 c0107f24 c00ee038 e5933008 e3530000
Backtrace:
[<c02f23ec>] (mdin200_i2c_read_reg+0x0/0x9c) from [<c02f2e30>] (mdin200_probe+0x40/0xf74)
r6 = 00000000 r5 = C04600A0 r4 = C05A1DEE
[<c02f2df0>] (mdin200_probe+0x0/0xf74) from [<c02d14b8>] (platform_drv_probe+0x20/0x24)
[<c02d1498>] (platform_drv_probe+0x0/0x24) from [<c02cfae8>] (driver_probe_device+0x7c/0xcc)
[<c02cfa6c>] (driver_probe_device+0x0/0xcc) from [<c02cfb48>] (__device_attach+0x10/0x14)
r7 = C05A1E64 r6 = C04600A0 r5 = C02CFB38 r4 = 00000000
[<c02cfb38>] (__device_attach+0x0/0x14) from [<c02cf314>] (bus_for_each_drv+0x50/0x8c)
[<c02cf2c4>] (bus_for_each_drv+0x0/0x8c) from [<c02cfbac>] (device_attach+0x60/0x8c)
r7 = 00000000 r6 = C0460144 r5 = C04600A0 r4 = C0460170
[<c02cfb4c>] (device_attach+0x0/0x8c) from [<c02ceff4>] (bus_attach_device+0x20/0x30)
r4 = C045DE20
[<c02cefd4>] (bus_attach_device+0x0/0x30) from [<c02cdff4>] (device_add+0x264/0x3b8)
r5 = C04600A0 r4 = 00000000
[<c02cdd90>] (device_add+0x0/0x3b8) from [<c02d1860>] (platform_device_add+0x108/0x15c)
[<c02d1758>] (platform_device_add+0x0/0x15c) from [<c02d18d8>] (platform_device_register+0x24/0x28)
[<c02d18b4>] (platform_device_register+0x0/0x28) from [<c0027d94>] (mdin200_i2c_init+0xbc/0x134)
r4 = C040CDFC
[<c0027cd8>] (mdin200_i2c_init+0x0/0x134) from [<c00ee0c0>] (init+0x98/0x26c)
r6 = C05A0000 r5 = C0030ABC r4 = 00000000
[<c00ee028>] (init+0x0/0x26c) from [<c0107f24>] (do_exit+0x0/0xa24)
Code: e1a0c00d e92dd870 e24cb004 e24dd024 (e5903008)
<0>Kernel panic - not syncing: Attempted to kill init!