This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Running example codes on DM6437



Hi everyone,

I am trying to run the example codes that come with the DM6437 board. 

normally when you connect the board it will run the default program which acquire video and audio data and display/play it back.

When I run the example code ...... (videopreview.pjt) ...... which suppose to render video data from camera and display it back

however when I compile the code and connect it to CCS to board the widow start shaking and now video data is rendered .. ( I can only see the previous image).

can anyone tell me why this is happening and why I can not see the video streaming.