This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cannot run syslink samples on the DM816X EVM



I have been trying for a long time to run any of the sample programs provided with the syslink package on a Spectrum Digital 816X EVM.

I can build the samples, but when I attempt to run them I get errors like the following:

root@dm816x-evm:~/TI816X/ti/syslink-examples/TI816X/ringio# ./run_ringio_debug.sh
======== Running app using slaveloader ========
RingIOApp sampleAssertion at Line no: 302 in /swcoe/sdk/cm/netra/arago-tmp/work/dm816x-evm-none-linux-gnueabi/ti-syslink-02_0
0_00_68-r3i/syslink_02_00_00_68_beta1/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/Linux/IpcDrv.
c: (status >= 0) : failed application
Run for all supported proc IDs
Entered RingIOApp_startup
Warning! Unsupported procID specified for running the sample application! proc ID: [1]
Warning! Unsupported procID specified for running the sample application! proc ID: [2]
Error in Ipc_control Ipc_CONTROLCMD_LOADCALLBACK [0xffffffff]
Leaving RingIOApp_startup() (0xffffffff)
======== Running app using agruments ========
RingIOApp sample application
Entered RingIOApp_startup
Loading and starting procId [0] with [./ringio_ti81xx_dsp.xe674]
SlaveLoader_startup status [-2]
Leaving RingIOApp_startup() (0xfffffffe)
root@dm816x-evm:~/TI816X/ti/syslink-examples/TI816X/ringio#

The settings used to build Syslink were:

peterr@ubuntu:~/ti-ezsdk_dm816x-evm_5_01_01_80/syslink_2_00_03_82$ make .show-products
DEPOT                    = /home/peterr/ti-ezsdk_dm816x-evm_5_01_01_80
DEVICE                   = TI816X
GPPOS                    = Linux
SDK                      = EZSDK
SYSLINK_BUILD_DEBUG      = 1
SYSLINK_BUILD_OPTIMIZE   = 0
SYSLINK_TRACE_ENABLE     = 1
LOADER                   =
SYSLINK_INSTALL_DIR      = /home/peterr/ti-ezsdk_dm816x-evm_5_01_01_80/syslink_2_00_03_82
IPC_INSTALL_DIR          = /home/peterr/ti-ezsdk_dm816x-evm_5_01_01_80/ipc_1_23_01_26
BIOS_INSTALL_DIR         = /home/peterr/ti-ezsdk_dm816x-evm_5_01_01_80/bios_6_32_01_38
XDC_INSTALL_DIR          = /home/peterr/ti-ezsdk_dm816x-evm_5_01_01_80/xdctools_3_22_01_21
LINUXKERNEL              = /home/peterr/ti-ezsdk_dm816x-evm_5_01_01_80/psp/linux-2.6.37-psp04.00.00.10
CGT_ARM_PREFIX           = /home/peterr/CodeSourcery/Sourcery_G++_Lite/bin/arm-none-linux-gnueabi-
CGT_C64P_INSTALL_DIR     =
CGT_C674_ELF_INSTALL_DIR = /home/peterr/ti-ezsdk_dm816x-evm_5_01_01_80/cgt6x_7_2_2
CGT_M3_ELF_INSTALL_DIR   =
CGT_A8_ELF_INSTALL_DIR   =
EXEC_DIR                 = /home/peterr/targetfs/home/root/TI816X
peterr@ubuntu:~/ti-ezsdk_dm816x-evm_5_01_01_80/syslink_2_00_03_82$

Following suggestions elsewhere I have tried unsuccessfully to update syslink.ko as described in the installation guide.

The command: rmmod syslink results in the error:

ERROR: Module syslink is in use by vpss.

I have searched in vain for a way to stop vpss. The possibility of rmmod failing is not mentioned in the syslink install guide.

I cannot see any process that suggests it is related to vpss. Here is the list:

root@dm816x-evm:~# ps
  PID USER       VSZ STAT COMMAND
    1 root      1708 S    init [5] 
    2 root         0 SW   [kthreadd]
    3 root         0 SW   [ksoftirqd/0]
    4 root         0 SW   [kworker/0:0]
    6 root         0 SW<  [khelper]
    7 root         0 SW   [irq/72-serial i]
    8 root         0 SW   [irq/73-serial i]
    9 root         0 SW   [irq/74-serial i]
   10 root         0 SW   [sync_supers]
   11 root         0 SW   [bdi-default]
   12 root         0 SW<  [kblockd]
   13 root         0 SW<  [omap2_mcspi]
   14 root         0 SW   [khubd]
   15 root         0 SW   [kseriod]
   16 root         0 SW<  [kmmcd]
   17 root         0 SW<  [musb-hdrc.0]
   18 root         0 SW<  [musb-hdrc.1]
   19 root         0 SW<  [rpciod]
   21 root         0 SW   [kswapd0]
   22 root         0 SW<  [aio]
   23 root         0 SW<  [nfsiod]
   24 root         0 SW   [scsi_eh_0]
   25 root         0 SW   [scsi_eh_1]
   26 root         0 SW   [kworker/u:1]
   28 root         0 SW   [kworker/u:3]
   29 root         0 SW   [mtdblock0]
   30 root         0 SW   [mtdblock1]
   31 root         0 SW   [mtdblock2]
   32 root         0 SW   [mtdblock3]
   33 root         0 SW   [mtdblock4]
   34 root         0 SW   [mtdblock5]
   35 root         0 SW   [mtdblock6]
   36 root         0 SW   [mtdblock7]
   37 root         0 SW   [mtdblock8]
   42 root         0 SW<  [usbhid_resumer]
   43 root         0 SW   [mmcqd/0]
   44 root         0 SW   [kworker/0:2]
   79 root      1956 S <  /sbin/udevd -d
  841 root         0 SW   [flush-0:14]
 1023 messageb  3324 S    /usr/bin/dbus-daemon --system
 1043 root         0 SW   [kjournald]
 1046 root         0 SW   [kjournald]
 1073 root         0 DW<  [kernelThread_0]
 1078 root      2936 S    /usr/sbin/telnetd
 1086 root         0 SW   [flush-179:0]
 1113 root      3000 S    /sbin/syslogd -n -C64 -m 20
 1115 root      2936 S    /sbin/klogd -n
 1120 root      2172 S    /usr/sbin/thttpd -d /srv/www -u root -c /cgi-bin/*
 1142 root         0 SW<  [pvr_timer]
 1175 root         0 SW<  [pvr_workqueue]
 1181 root      2516 S    login -- root    
 1182 root      1968 S    /sbin/getty 38400 tty1
 1183 root      3128 S    -sh
 1188 root      3128 R    ps

How do I update syslink.ko?