Dear All:
We encounter a big problem about system_server rise its cpu loading up unexpectedly.
Our IPNC version is V2.0 and settings :
|
Stream |
audio |
Alarm (aplay) |
Alarm duration |
Alarm trigger |
Storage |
|
3 |
ON |
ON |
Non STOP |
Motion or external Input |
Not necessary |
And after about 14 hours, the aplay fucntion will stop and disappear, even though we re-enable the alarm.
We use "top" cmd to monitor the IPCAM status and surprisingly find out system server rise its cpu loading up to about 30%.
But we still can type #aplay -f U8 alarm_1_8K.wav -r 8000 and it could work.
And we list below results for system_server and the other services.
>> system_server around 10% => normal status
>> system_server up to about 20% => aplay and storage functions don't work.
>> system_server up to about 50% => boa server and Upnp failed to use. but VLC could still receive the streaming.
>> system_server large than 90% => system crash....
However, we change our IP environment to Static IP mode, the system and services are health during 3-4 day long-term testing.
And the result is same as the Appro IPCAM in version 2.0.
Hence, had anyone met the same problem? Or any idea to solve the strange phenomenon?
I really appreciate and thanks for your kindly help.