Part Number: AM6422
Tool/software:
Dear Experts,
Currently I am struggeling to understand our requirements for power up and power down sequencing.
Our Power down Sequencing states: VDD_CORE should be ramped down parallel or later than

the 0.85 V supply lines.
Considering the power up there it is also allowed for VDD_CORE to ramp up/down before or after VDDS_DDR.
So, why is this not allowed during power down?
I would like to understand the exact requirements here and were they orginate from.
Especially knowing that the PMIC that is intended to use (TPS6521903) is switching of the 3.3 V load switch at the same time as 0V75 ramps down.

When 3V3 have more capacities on rail this will discharge slower especially when considering that 0.75 is activly discharged.
Regards,
Alex