Tool/software:
Hi Ti ,
Working on AM62X , 09_00_00_03 build . using ubuntu 24 version host.
while compiling Yocto build getting permission issues and exiting .
Kindly help me on this as it is critical to us .
Logs:
OTE: Deferring mc:k3r5:virtual:native:/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-support/re2c/re2c_3.0.bb:do_deploy_source_date_epoch after virtual:native:/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-support/re2c/re2c_3.0.bb:do_deploy_source_date_epoch NOTE: Deferring mc:k3r5:virtual:native:/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-support/re2c/re2c_3.0.bb:do_populate_lic after virtual:native:/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-support/re2c/re2c_3.0.bb:do_populate_lic NOTE: Deferring mc:k3r5:virtual:native:/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-support/re2c/re2c_3.0.bb:do_populate_sysroot after virtual:native:/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-support/re2c/re2c_3.0.bb:do_populate_sysroot NOTE: Deferring mc:k3r5:virtual:native:/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-support/sqlite/sqlite3_3.38.5.bb:do_deploy_source_date_epoch after virtual:native:/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-support/sqlite/sqlite3_3.38.5.bb:do_deploy_source_date_epoch NOTE: Deferring mc:k3r5:virtual:native:/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-support/sqlite/sqlite3_3.38.5.bb:do_populate_lic after virtual:native:/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-support/sqlite/sqlite3_3.38.5.bb:do_populate_lic NOTE: Deferring mc:k3r5:virtual:native:/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-support/sqlite/sqlite3_3.38.5.bb:do_populate_sysroot after virtual:native:/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-support/sqlite/sqlite3_3.38.5.bb:do_populate_sysroot Sstate summary: Wanted 2454 Local 0 Mirrors 0 Missed 2454 Current 0 (0% match, 0% complete) NOTE: Executing Tasks ERROR: PermissionError: [Errno 1] Operation not permitted During handling of the above exception, another exception occurred: Traceback (most recent call last): File "/home/test/project/ototrak/Yocto_WS/tisdk/sources/bitbake/bin/bitbake-worker", line 268, in child bb.utils.disable_network(uid, gid) File "/home/test/project/ototrak/Yocto_WS/tisdk/sources/bitbake/lib/bb/utils.py", line 1653, in disable_network with open("/proc/self/uid_map", "w") as f: PermissionError: [Errno 1] Operation not permitted ERROR: PermissionError: [Errno 1] Operation not permitted During handling of the above exception, another exception occurred: Traceback (most recent call last): File "/home/test/project/ototrak/Yocto_WS/tisdk/sources/bitbake/bin/bitbake-worker", line 268, in child bb.utils.disable_network(uid, gid) File "/home/test/project/ototrak/Yocto_WS/tisdk/sources/bitbake/lib/bb/utils.py", line 1653, in disable_network with open("/proc/self/uid_map", "w") as f: PermissionError: [Errno 1] Operation not permitted ERROR: Task (/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-devtools/quilt/quilt-native_0.67.bb:do_unpack) failed with exit code '1' ERROR: PermissionError: [Errno 1] Operation not permitted During handling of the above exception, another exception occurred: Traceback (most recent call last): File "/home/test/project/ototrak/Yocto_WS/tisdk/sources/bitbake/bin/bitbake-worker", line 268, in child bb.utils.disable_network(uid, gid) File "/home/test/project/ototrak/Yocto_WS/tisdk/sources/bitbake/lib/bb/utils.py", line 1653, in disable_network with open("/proc/self/uid_map", "w") as f: PermissionError: [Errno 1] Operation not permitted ERROR: PermissionError: [Errno 1] Operation not permitted During handling of the above exception, another exception occurred: Traceback (most recent call last): File "/home/test/project/ototrak/Yocto_WS/tisdk/sources/bitbake/bin/bitbake-worker", line 268, in child bb.utils.disable_network(uid, gid) File "/home/test/project/ototrak/Yocto_WS/tisdk/sources/bitbake/lib/bb/utils.py", line 1653, in disable_network with open("/proc/self/uid_map", "w") as f: PermissionError: [Errno 1] Operation not permitted ERROR: Task (/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-extended/texinfo-dummy-native/texinfo-dummy-native.bb:do_unpack) failed with exit code '1' ERROR: Task (/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-devtools/quilt/quilt-native_0.67.bb:do_prepare_recipe_sysroot) failed with exit code '1' ERROR: Task (/home/test/project/ototrak/Yocto_WS/tisdk/sources/oe-core/meta/recipes-core/gettext/gettext-minimal-native_0.21.bb:do_unpack) failed with exit code '1' ERROR: PermissionError: [Errno 1] Operation not permitted During handling of the above exception, another exception occurred: Traceback (most recent call last): File "/home/test/project/ototrak/Yocto_WS/tisdk/sources/bitbake/bin/bitbake-worker", line 268, in child bb.utils.disable_network(uid, gid) File "/home/test/project/ototrak/Yocto_WS/tisdk/sources/bitbake/lib/bb/utils.py", line 1653, in disable_network with open("/proc/self/uid_map", "w") as f: PermissionError: [Errno 1] Operation not permitted ERROR: PermissionError: [Errno 1] Operation not permitted During handling of the above exception, another exception occurred: Traceback (most recent call last): File "/home/test/project/ototrak/Yocto_WS/tisdk/sources/bitbake/bin/bitbake-worker", line 268, in child bb.utils.disable_network(uid, gid) File "/home/test/project/ototrak/Yocto_WS/tisdk/sources/bitbake/lib/bb/utils.py", line 1653, in disable_network with open("/proc/self/uid_map", "w") as f: PermissionError: [Errno 1] Operation not permitted
Thanks,Naresh